Source code for bosdyn.client.log_annotation

# Copyright (c) 2021 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

"""Client for the log-annotation service (DEPRECATED).

The log-annotation service is deprecated and will be removed in a later release.
Instead, please use the data_buffer service going forward.
"""
from __future__ import print_function

import logging
import random
import string
import struct
import sys
import threading
import time
import traceback

from deprecated import deprecated
from six.moves.queue import Queue

from bosdyn import util as core_util
from bosdyn.client.exceptions import Error, RpcError, ServerError
from bosdyn.client.common import BaseClient, common_header_errors
from bosdyn.client import time_sync
import bosdyn.api.log_annotation_pb2 as log_annotation_protos
import bosdyn.api.log_annotation_service_pb2_grpc as log_annotation_service


[docs]class InvalidArgument(Error): """A given argument could not be used."""
[docs]@deprecated(reason='The log-annotation client and service have been replaced by data_buffer.', version='2.1.0', action="always") class LogAnnotationClient(BaseClient): """A client for adding annotations to robot logs.""" default_service_name = 'log-annotation' service_type = 'bosdyn.api.LogAnnotationService' def __init__(self): super(LogAnnotationClient, self).__init__(log_annotation_service.LogAnnotationServiceStub) self.log_tick_schemas = {} self._timesync_endpoint = None
[docs] def update_from(self, other): super(LogAnnotationClient, self).update_from(other) # Grab a timesync endpoint if it is available. try: self._timesync_endpoint = other.time_sync.endpoint except AttributeError: pass # other doesn't have a time_sync accessor
[docs] def add_text_messages(self, text_messages, **kwargs): """Log text messages to the robot. Args: text_messages: Sequence of LogAnnotationTextMessage protos. Raises: RpcError: Problem communicating with the robot. """ return self._do_add_text_messages(self.call, text_messages, **kwargs)
[docs] def add_text_messages_async(self, text_messages, **kwargs): """Async version of add_text_messages.""" return self._do_add_text_messages(self.call_async, text_messages, **kwargs)
def _do_add_text_messages(self, func, text_messages, **kwargs): request = log_annotation_protos.AddLogAnnotationRequest() for in_text_msg in text_messages: request.annotations.text_messages.add().CopyFrom(in_text_msg) return func(self._stub.AddLogAnnotation, request, value_from_response=None, error_from_response=common_header_errors, **kwargs)
[docs] def add_operator_comment(self, msg, robot_timestamp=None, **kwargs): """Add an operator comment to the robot log. Args: msg: Text of user comment to log. robot_timestamp: Time (google.protobuf.Timestamp) of messages, in *robot time*. If not set, timestamp will be when the robot receives the message. Raises: RpcError: Problem communicating with the robot. """ return self._do_add_operator_comment(self.call, msg, robot_timestamp, **kwargs)
[docs] def add_operator_comment_async(self, msg, robot_timestamp=None, **kwargs): """Async version of add_operator_comment.""" return self._do_add_operator_comment(self.call_async, msg, robot_timestamp, **kwargs)
def _do_add_operator_comment(self, func, msg, robot_timestamp=None, **kwargs): request = log_annotation_protos.AddLogAnnotationRequest() robot_timestamp = robot_timestamp or self._now_in_robot_basis(msg_type="Operator Comment") request.annotations.operator_messages.add(message=msg, timestamp=robot_timestamp) return func(self._stub.AddLogAnnotation, request, value_from_response=None, error_from_response=common_header_errors, **kwargs)
[docs] def add_log_blob(self, data, type_id, channel=None, robot_timestamp=None, **kwargs): """Log blob messages to the robot. Args: data: Binary data of one blob. type_id: Type of binary data of blob. robot_timestamp: Time (google.protobuf.Timestamp) of messages, in *robot time*. If not set, timestamp will be when the robot receives the message. Raises: RpcError: Problem communicating with the robot. """ return self._do_add_log_blob(self.call, data, type_id, channel, robot_timestamp, **kwargs)
[docs] def add_log_blob_async(self, data, type_id, channel=None, robot_timestamp=None, **kwargs): """Async version of add_log_blob.""" return self._do_add_log_blob(self.call_async, data, type_id, channel, robot_timestamp, **kwargs)
def _do_add_log_blob(self, func, data, type_id, channel, robot_timestamp, **kwargs): request = log_annotation_protos.AddLogAnnotationRequest() if not channel: channel = type_id robot_timestamp = robot_timestamp or self._now_in_robot_basis(msg_type=type_id) request.annotations.blob_data.add(timestamp=robot_timestamp, channel=channel, type_id=type_id, data=data) return func(self._stub.AddLogAnnotation, request, value_from_response=None, error_from_response=common_header_errors, **kwargs)
[docs] def add_log_protobuf(self, proto, robot_timestamp=None): return self._do_add_log_protobuf(self.add_log_blob, proto, robot_timestamp)
[docs] def add_log_protobuf_async(self, proto, robot_timestamp=None): return self._do_add_log_protobuf(self.add_log_blob_async, proto, robot_timestamp)
def _do_add_log_protobuf(self, func, proto, robot_timestamp): binary_data = proto.SerializeToString() robot_timestamp = robot_timestamp or self._now_in_robot_basis(proto=proto) return func(data=binary_data, type_id=proto.DESCRIPTOR.full_name, channel=proto.DESCRIPTOR.full_name, robot_timestamp=robot_timestamp) def _now_in_robot_basis(self, msg_type=None, proto=None): """Get current time in robot clock basis if possible, None otherwise.""" if self._timesync_endpoint: try: converter = self._timesync_endpoint.get_robot_time_converter() except time_sync.NotEstablishedError: # No timesync. That's OK -- the receiving host will provide the timestamp. self.logger.debug( 'Could not timestamp message of type %s', (msg_type if msg_type is not None else (proto.DESCRIPTOR.full_name if proto is not None else 'Unknown'))) else: return converter.robot_timestamp_from_local_secs(time.time()) return None
[docs]@deprecated(reason='The log-annotation client and service have been replaced by data_buffer.', version='2.1.0', action="always") class LogAnnotationHandler(logging.Handler): """A logging system Handler that will publish text to a bosdyn.api.LogAnnotationService. Args: service: Name of the service. See LogAnnotationTextMessage. log_client: API client that will send log messages. level: Python logging level. Defaults to NOTSET. time_sync_endpoint: A TimeSyncEndpoint, already synchronized to the remote clock. rpc_timeout: Timeout on RPCs made by log_client. msg_num_limit: If number of messages reaches this number, send data with log_client. msg_age_limit: If messages have been sitting locally for this many seconds, send data with log_client. Raises: log_annotation.InvalidArgument: The TimeSyncEndpoint is not valid. """ def __init__(self, service, log_client, level=logging.NOTSET, time_sync_endpoint=None, rpc_timeout=1, msg_num_limit=10, msg_age_limit=1): logging.Handler.__init__(self, level=level) self.msg_age_limit = msg_age_limit self.msg_num_limit = msg_num_limit self.rpc_timeout = rpc_timeout self.service = service self.time_sync_endpoint = time_sync_endpoint if self.time_sync_endpoint and not self.time_sync_endpoint.has_established_time_sync: raise InvalidArgument('time_sync_endpoint must have already established timesync!') # If we have this many unsent messages in the queue after a failure to send, # "dump" the messages to stdout. self._dump_msg_count = 20 # Internal tracking of errors. self._num_failed_sends = 0 self._num_failed_sends_sequential = 0 # If we have this many failed sends in a row, stop the send thread. self._limit_failed_sends_sequential = 5 # Event to trigger immediate flush of messages to the log client. self._flush_event = threading.Event() # How long to wait for flush events. Dictates non-flush update rate. self._flush_event_wait_time = 0.1 # Last time "emit" was called. self._last_emit_time = 0 self._log_client = log_client self._lock = threading.Lock() self._msg_queue = [] self._send_thread = threading.Thread(target=self._run_send_thread) # Set to stop the message send thread. self._shutdown_event = threading.Event() # This apparently needs to be a daemon thread to play nicely with python's Handler shutdown # procedure. self._send_thread.daemon = True self._send_thread.start() def __enter__(self): """Optionally use this as a ContextManager to be more cautious about sending messages.""" return self def __exit__(self, exc_type, exc_val, exc_tb): """To ensure all messages have been sent to the best of our ability, call close().""" self.close()
[docs] def emit(self, record): msg = self.record_to_msg(record) with self._lock: self._msg_queue.append(msg) self._last_emit_time = time.time()
[docs] def flush(self): self._flush_event.set()
[docs] def close(self): self._shutdown_event.set() self._send_thread.join() # One last attempt to send any messages. if self._msg_queue: try: self._log_client.add_text_messages(self._msg_queue, timeout=self.rpc_timeout) # Catch all client library errors. except Error: self._num_failed_sends += 1 with self._lock: self._dump_msg_queue() logging.Handler.close(self)
[docs] def is_thread_alive(self): return self._send_thread.is_alive()
[docs] def restart(self, log_client): """Restart the send thread. Raises: AssertionError if send thread is still alive. """ assert not self.is_thread_alive() self._num_failed_sends_sequential = 0 self._log_client = log_client self._send_thread = threading.Thread(target=self._run_send_thread) self._send_thread.daemon = True self._send_thread.start()
def _dump_msg_queue(self): """Pop all of the message queue, using fallback_log to try and capture them. Should be called with the lock held. """ self.fallback_log('Dumping {} messages!'.format(len(self._msg_queue))) for msg in self._msg_queue: self.fallback_log(msg) del self._msg_queue[:]
[docs] def fallback_log(self, msg): print(msg, file=sys.stderr)
def _run_send_thread(self): while (self._num_failed_sends_sequential < self._limit_failed_sends_sequential and not self._shutdown_event.is_set()): flush = self._flush_event.wait(self._flush_event_wait_time) msg_age = time.time() - self._last_emit_time with self._lock: num_msgs = len(self._msg_queue) to_send = self._msg_queue[:num_msgs] send_now = num_msgs >= 1 and (flush or msg_age >= self.msg_age_limit or num_msgs >= self.msg_num_limit) if send_now: self._flush_event.clear() send_errors = 0 error_limit = 2 sent = False while send_errors < error_limit and not self._shutdown_event.is_set(): try: self._log_client.add_text_messages(to_send, timeout=self.rpc_timeout) except (RpcError, ServerError): self.fallback_log('Error:\n{}'.format(traceback.format_exc())) send_errors += 1 except: # Catch all other exceptions and log them. self.fallback_log('Unexpected exception!\n{}'.format( traceback.format_exc())) break else: sent = True break # Default to possibly dumping messages. maybe_dump = True if sent: # We successfully sent logs to the log service! Delete relevant local cache. with self._lock: del self._msg_queue[:num_msgs] maybe_dump = False self._num_failed_sends_sequential = 0 elif send_errors >= error_limit: self._num_failed_sends += 1 self._num_failed_sends_sequential += 1 elif self._shutdown_event.is_set(): # Don't dump if we're shutting down; we'll clear the messages in close(). maybe_dump = False else: # We can hit this state if # 1) We break out of the above loop without setting sent = True # 2) There is a logic bug in the above handling code / while loop. function_name = traceback.extract_stack()[-1][2] self.fallback_log('Unexpected condition in {}.{}!'.format( self.__class__.__name__, function_name)) # If we decided we may need to dump the message queue... if maybe_dump: with self._lock: if len(self._msg_queue) >= self._dump_msg_count: self._dump_msg_queue()
[docs] def record_to_msg(self, record): level = self.record_level_to_proto_level(record.levelno) msg = log_annotation_protos.LogAnnotationTextMessage(service=self.service, level=level) msg.message = self.format(record) if self.time_sync_endpoint is not None: try: msg.timestamp.CopyFrom( self.time_sync_endpoint.robot_timestamp_from_local_secs(time.time())) except time_sync.NotEstablishedError: msg.message = '(No time sync!): ' + msg.message msg.timestamp.CopyFrom(core_util.now_timestamp()) else: msg.timestamp.CopyFrom(core_util.now_timestamp()) return msg
[docs] @staticmethod def record_level_to_proto_level(record_level): if record_level >= logging.ERROR: return log_annotation_protos.LogAnnotationTextMessage.LEVEL_ERROR elif record_level >= logging.WARNING: return log_annotation_protos.LogAnnotationTextMessage.LEVEL_WARN elif record_level >= logging.INFO: return log_annotation_protos.LogAnnotationTextMessage.LEVEL_INFO return log_annotation_protos.LogAnnotationTextMessage.LEVEL_DEBUG