# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

import argparse
import io
import logging
import os
import queue
import sys
import threading
import time
from concurrent import futures

import cv2
import grpc
import numpy as np
import tensorflow as tf
from google.protobuf import wrappers_pb2
from object_detection.utils import label_map_util
from PIL import Image

import bosdyn.client
import bosdyn.client.util
from bosdyn.api import (header_pb2, image_pb2, network_compute_bridge_pb2,
                        network_compute_bridge_service_pb2_grpc)

kServiceAuthority = "fetch-tutorial-worker.spot.robot"


class TensorFlowObjectDetectionModel:

    def __init__(self, model_path, label_path):
        self.detect_fn = tf.saved_model.load(model_path)
        self.category_index = label_map_util.create_category_index_from_labelmap(
            label_path, use_display_name=True)
        self.name = os.path.basename(os.path.dirname(model_path))

    def predict(self, image):
        input_tensor = tf.convert_to_tensor(image)
        input_tensor = input_tensor[tf.newaxis, ...]
        detections = self.detect_fn(input_tensor)

        return detections


def process_thread(args, request_queue, response_queue):
    # Load the model(s)
    models = {}
    for model in args.model:
        this_model = TensorFlowObjectDetectionModel(model[0], model[1])
        models[this_model.name] = this_model

    print('')
    print('Service ' + args.name + ' running on port: ' + str(args.port))

    print('Loaded models:')
    for model_name in models:
        print('    ' + model_name)

    while True:
        request = request_queue.get()

        if isinstance(request, network_compute_bridge_pb2.ListAvailableModelsRequest):
            out_proto = network_compute_bridge_pb2.ListAvailableModelsResponse()
            for model_name in models:
                out_proto.models.data.append(
                    network_compute_bridge_pb2.ModelData(model_name=model_name))
            response_queue.put(out_proto)
            continue
        else:
            out_proto = network_compute_bridge_pb2.NetworkComputeResponse()

        # Find the model
        if request.input_data.model_name not in models:
            err_str = 'Cannot find model "' + request.input_data.model_name + '" in loaded models.'
            print(err_str)

            # Set the error in the header.
            out_proto.header.error.code = header_pb2.CommonError.CODE_INVALID_REQUEST
            out_proto.header.error.message = err_str
            response_queue.put(out_proto)
            continue

        model = models[request.input_data.model_name]

        # Unpack the incoming image.
        if request.input_data.image.format == image_pb2.Image.FORMAT_RAW:
            pil_image = Image.open(io.BytesIO(request.input_data.image.data))
            if request.input_data.image.pixel_format == image_pb2.Image.PIXEL_FORMAT_GREYSCALE_U8:
                # If the input image is grayscale, convert it to RGB.
                image = cv2.cvtColor(pil_image, cv2.COLOR_GRAY2RGB)

            elif request.input_data.image.pixel_format == image_pb2.Image.PIXEL_FORMAT_RGB_U8:
                # Already an RGB image.
                image = pil_image

            else:
                print('Error: image input in unsupported pixel format: ',
                      request.input_data.image.pixel_format)
                response_queue.put(out_proto)
                continue

        elif request.input_data.image.format == image_pb2.Image.FORMAT_JPEG:
            dtype = np.uint8
            jpg = np.frombuffer(request.input_data.image.data, dtype=dtype)
            image = cv2.imdecode(jpg, -1)

            if len(image.shape) < 3:
                # If the input image is grayscale, convert it to RGB.
                image = cv2.cvtColor(image, cv2.COLOR_GRAY2RGB)

        image_width = image.shape[0]
        image_height = image.shape[1]

        detections = model.predict(image)

        num_objects = 0

        # All outputs are batches of tensors.
        # Convert to numpy arrays, and take index [0] to remove the batch dimension.
        # We're only interested in the first num_detections.
        num_detections = int(detections.pop('num_detections'))
        detections = {key: value[0, :num_detections].numpy() for key, value in detections.items()}

        boxes = detections['detection_boxes']
        classes = detections['detection_classes']
        scores = detections['detection_scores']

        for i in range(boxes.shape[0]):
            if scores[i] < request.input_data.min_confidence:
                continue

            box = tuple(boxes[i].tolist())

            # Boxes come in with normalized coordinates.  Convert to pixel values.
            box = [
                box[0] * image_width, box[1] * image_height, box[2] * image_width,
                box[3] * image_height
            ]

            score = scores[i]

            if classes[i] in model.category_index.keys():
                label = model.category_index[classes[i]]['name']
            else:
                label = 'N/A'

            num_objects += 1

            print('Found object with label: "' + label + '" and score: ' + str(score))

            point1 = np.array([box[1], box[0]])
            point2 = np.array([box[3], box[0]])
            point3 = np.array([box[3], box[2]])
            point4 = np.array([box[1], box[2]])

            # Add data to the output proto.
            out_obj = out_proto.object_in_image.add()
            out_obj.name = "obj" + str(num_objects) + "_label_" + label

            vertex1 = out_obj.image_properties.coordinates.vertexes.add()
            vertex1.x = point1[0]
            vertex1.y = point1[1]

            vertex2 = out_obj.image_properties.coordinates.vertexes.add()
            vertex2.x = point2[0]
            vertex2.y = point2[1]

            vertex3 = out_obj.image_properties.coordinates.vertexes.add()
            vertex3.x = point3[0]
            vertex3.y = point3[1]

            vertex4 = out_obj.image_properties.coordinates.vertexes.add()
            vertex4.x = point4[0]
            vertex4.y = point4[1]

            # Pack the confidence value.
            confidence = wrappers_pb2.FloatValue(value=score)
            out_obj.additional_properties.Pack(confidence)

            if not args.no_debug:
                polygon = np.array([point1, point2, point3, point4], np.int32)
                polygon = polygon.reshape((-1, 1, 2))
                cv2.polylines(image, [polygon], True, (0, 255, 0), 2)

                caption = "{}: {:.3f}".format(label, score)
                left_x = min(point1[0], min(point2[0], min(point3[0], point4[0])))
                top_y = min(point1[1], min(point2[1], min(point3[1], point4[1])))
                cv2.putText(image, caption, (int(left_x), int(top_y)), cv2.FONT_HERSHEY_SIMPLEX,
                            0.5, (0, 255, 0), 2)

        print('Found ' + str(num_objects) + ' object(s)')

        if not args.no_debug:
            debug_image_filename = 'network_compute_server_output.jpg'
            cv2.imwrite(debug_image_filename, image)
            print('Wrote debug image output to: "' + debug_image_filename + '"')

        response_queue.put(out_proto)


class NetworkComputeBridgeWorkerServicer(
        network_compute_bridge_service_pb2_grpc.NetworkComputeBridgeWorkerServicer):

    def __init__(self, thread_input_queue, thread_output_queue):
        super(NetworkComputeBridgeWorkerServicer, self).__init__()

        self.thread_input_queue = thread_input_queue
        self.thread_output_queue = thread_output_queue

    def NetworkCompute(self, request, context):
        print('Got NetworkCompute request')
        self.thread_input_queue.put(request)
        out_proto = self.thread_output_queue.get()
        return out_proto

    def ListAvailableModels(self, request, context):
        print('Got ListAvailableModels request')
        self.thread_input_queue.put(request)
        out_proto = self.thread_output_queue.get()
        return out_proto


def register_with_robot(options):
    """ Registers this worker with the robot's Directory."""
    ip = bosdyn.client.common.get_self_ip(options.hostname)
    print('Detected IP address as: ' + ip)

    sdk = bosdyn.client.create_standard_sdk("tensorflow_server")

    robot = sdk.create_robot(options.hostname)

    # Authenticate robot before being able to use it
    if options.payload_credentials_file:
        robot.authenticate_from_payload_credentials(
            *bosdyn.client.util.get_guid_and_secret(options))
    else:
        bosdyn.client.util.authenticate(robot)

    directory_client = robot.ensure_client(
        bosdyn.client.directory.DirectoryClient.default_service_name)
    directory_registration_client = robot.ensure_client(
        bosdyn.client.directory_registration.DirectoryRegistrationClient.default_service_name)

    # Check to see if a service is already registered with our name
    services = directory_client.list()
    for s in services:
        if s.name == options.name:
            print("WARNING: existing service with name, \"" + options.name + "\", removing it.")
            directory_registration_client.unregister(options.name)
            break

    # Register service
    print('Attempting to register ' + ip + ':' + options.port + ' onto ' + options.hostname +
          ' directory...')
    directory_registration_client.register(options.name, "bosdyn.api.NetworkComputeBridgeWorker",
                                           kServiceAuthority, ip, int(options.port))


def main(argv):
    default_port = '50051'

    parser = argparse.ArgumentParser()
    parser.add_argument(
        '-m', '--model', help=
        '[MODEL_DIR] [LABELS_FILE.pbtxt]: Path to a model\'s directory and path to its labels .pbtxt file',
        action='append', nargs=2, required=True)
    parser.add_argument('-p', '--port', help='Server\'s port number, default: ' + default_port,
                        default=default_port)
    parser.add_argument('-d', '--no-debug', help='Disable writing debug images.',
                        action='store_true')
    parser.add_argument('-n', '--name', help='Service name', default='fetch-server')
    bosdyn.client.util.add_payload_credentials_arguments(parser, required=False)
    bosdyn.client.util.add_base_arguments(parser)

    options = parser.parse_args(argv)

    print(options.model)

    for model in options.model:
        if not os.path.isdir(model[0]):
            print('Error: model directory (' + model[0] + ') not found or is not a directory.')
            sys.exit(1)

    # Perform registration.
    register_with_robot(options)

    # Thread-safe queues for communication between the GRPC endpoint and the ML thread.
    request_queue = queue.Queue()
    response_queue = queue.Queue()

    # Start server thread
    thread = threading.Thread(target=process_thread, args=([options, request_queue,
                                                            response_queue]))
    thread.start()

    # Set up GRPC endpoint
    server = grpc.server(futures.ThreadPoolExecutor(max_workers=10))
    network_compute_bridge_service_pb2_grpc.add_NetworkComputeBridgeWorkerServicer_to_server(
        NetworkComputeBridgeWorkerServicer(request_queue, response_queue), server)
    server.add_insecure_port('[::]:' + options.port)
    server.start()

    print('Running...')
    thread.join()

    return True


if __name__ == '__main__':
    logging.basicConfig()
    if not main(sys.argv[1:]):
        sys.exit(1)