# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

import argparse
import math
import sys
import time

import cv2
import numpy as np
from google.protobuf import wrappers_pb2

import bosdyn.client
import bosdyn.client.util
from bosdyn.api import (basic_command_pb2, geometry_pb2, image_pb2, manipulation_api_pb2,
                        network_compute_bridge_pb2)
from bosdyn.client import frame_helpers, math_helpers
from bosdyn.client.lease import LeaseClient, LeaseKeepAlive
from bosdyn.client.manipulation_api_client import ManipulationApiClient
from bosdyn.client.network_compute_bridge_client import (ExternalServerError,
                                                         NetworkComputeBridgeClient)
from bosdyn.client.robot_command import (RobotCommandBuilder, RobotCommandClient,
                                         block_for_trajectory_cmd, block_until_arm_arrives)
from bosdyn.client.robot_state import RobotStateClient

kImageSources = [
    'frontleft_fisheye_image', 'frontright_fisheye_image', 'left_fisheye_image',
    'right_fisheye_image', 'back_fisheye_image'
]


def get_obj_and_img(network_compute_client, server, model, confidence, image_sources, label):

    for source in image_sources:
        # Build a network compute request for this image source.
        image_source_and_service = network_compute_bridge_pb2.ImageSourceAndService(
            image_source=source)

        # Input data:
        #   model name
        #   minimum confidence (between 0 and 1)
        #   if we should automatically rotate the image
        input_data = network_compute_bridge_pb2.NetworkComputeInputData(
            image_source_and_service=image_source_and_service, model_name=model,
            min_confidence=confidence, rotate_image=network_compute_bridge_pb2.
            NetworkComputeInputData.ROTATE_IMAGE_ALIGN_HORIZONTAL)

        # Server data: the service name
        server_data = network_compute_bridge_pb2.NetworkComputeServerConfiguration(
            service_name=server)

        # Pack and send the request.
        process_img_req = network_compute_bridge_pb2.NetworkComputeRequest(
            input_data=input_data, server_config=server_data)

        try:
            resp = network_compute_client.network_compute_bridge_command(process_img_req)
        except ExternalServerError:
            # This sometimes happens if the NCB is unreachable due to intermittent wifi failures.
            print('Error connecting to network compute bridge. This may be temporary.')
            return None, None, None

        best_obj = None
        highest_conf = 0.0
        best_vision_tform_obj = None

        img = get_bounding_box_image(resp)
        image_full = resp.image_response

        # Show the image
        cv2.imshow("Fetch", img)
        cv2.waitKey(15)

        if len(resp.object_in_image) > 0:
            for obj in resp.object_in_image:
                # Get the label
                obj_label = obj.name.split('_label_')[-1]
                if obj_label != label:
                    continue
                conf_msg = wrappers_pb2.FloatValue()
                obj.additional_properties.Unpack(conf_msg)
                conf = conf_msg.value

                try:
                    vision_tform_obj = frame_helpers.get_a_tform_b(
                        obj.transforms_snapshot, frame_helpers.VISION_FRAME_NAME,
                        obj.image_properties.frame_name_image_coordinates)
                except bosdyn.client.frame_helpers.ValidateFrameTreeError:
                    # No depth data available.
                    vision_tform_obj = None

                if conf > highest_conf and vision_tform_obj is not None:
                    highest_conf = conf
                    best_obj = obj
                    best_vision_tform_obj = vision_tform_obj

        if best_obj is not None:
            return best_obj, image_full, best_vision_tform_obj

    return None, None, None


def get_bounding_box_image(response):
    dtype = np.uint8
    img = np.fromstring(response.image_response.shot.image.data, dtype=dtype)
    if response.image_response.shot.image.format == image_pb2.Image.FORMAT_RAW:
        img = img.reshape(response.image_response.shot.image.rows,
                          response.image_response.shot.image.cols)
    else:
        img = cv2.imdecode(img, -1)

    # Convert to BGR so we can draw colors
    img = cv2.cvtColor(img, cv2.COLOR_GRAY2BGR)

    # Draw bounding boxes in the image for all the detections.
    for obj in response.object_in_image:
        conf_msg = wrappers_pb2.FloatValue()
        obj.additional_properties.Unpack(conf_msg)
        confidence = conf_msg.value

        polygon = []
        min_x = float('inf')
        min_y = float('inf')
        for v in obj.image_properties.coordinates.vertexes:
            polygon.append([v.x, v.y])
            min_x = min(min_x, v.x)
            min_y = min(min_y, v.y)

        polygon = np.array(polygon, np.int32)
        polygon = polygon.reshape((-1, 1, 2))
        cv2.polylines(img, [polygon], True, (0, 255, 0), 2)

        caption = "{} {:.3f}".format(obj.name, confidence)
        cv2.putText(img, caption, (int(min_x), int(min_y)), cv2.FONT_HERSHEY_SIMPLEX, 0.5,
                    (0, 255, 0), 2)

    return img


def find_center_px(polygon):
    min_x = math.inf
    min_y = math.inf
    max_x = -math.inf
    max_y = -math.inf
    for vert in polygon.vertexes:
        if vert.x < min_x:
            min_x = vert.x
        if vert.y < min_y:
            min_y = vert.y
        if vert.x > max_x:
            max_x = vert.x
        if vert.y > max_y:
            max_y = vert.y
    x = math.fabs(max_x - min_x) / 2.0 + min_x
    y = math.fabs(max_y - min_y) / 2.0 + min_y
    return (x, y)


def main(argv):
    parser = argparse.ArgumentParser()
    bosdyn.client.util.add_base_arguments(parser)
    parser.add_argument('-s', '--ml-service',
                        help='Service name of external machine learning server.', required=True)
    parser.add_argument('-m', '--model', help='Model name running on the external server.',
                        required=True)
    parser.add_argument('-p', '--person-model',
                        help='Person detection model name running on the external server.')
    parser.add_argument('-c', '--confidence-dogtoy',
                        help='Minimum confidence to return an object for the dogoy (0.0 to 1.0)',
                        default=0.5, type=float)
    parser.add_argument('-e', '--confidence-person',
                        help='Minimum confidence for person detection (0.0 to 1.0)', default=0.6,
                        type=float)
    options = parser.parse_args(argv)

    cv2.namedWindow("Fetch")
    cv2.waitKey(500)

    sdk = bosdyn.client.create_standard_sdk('SpotFetchClient')
    sdk.register_service_client(NetworkComputeBridgeClient)
    robot = sdk.create_robot(options.hostname)
    bosdyn.client.util.authenticate(robot)

    # Time sync is necessary so that time-based filter requests can be converted
    robot.time_sync.wait_for_sync()

    network_compute_client = robot.ensure_client(NetworkComputeBridgeClient.default_service_name)
    robot_state_client = robot.ensure_client(RobotStateClient.default_service_name)
    command_client = robot.ensure_client(RobotCommandClient.default_service_name)
    lease_client = robot.ensure_client(LeaseClient.default_service_name)
    manipulation_api_client = robot.ensure_client(ManipulationApiClient.default_service_name)

    # This script assumes the robot is already standing via the tablet.  We'll take over from the
    # tablet.
    lease_client.take()
    with bosdyn.client.lease.LeaseKeepAlive(lease_client, must_acquire=True, return_at_exit=True):
        # Store the position of the hand at the last toy drop point.
        vision_tform_hand_at_drop = None

        while True:
            holding_toy = False
            while not holding_toy:
                # Capture an image and run ML on it.
                dogtoy, image, vision_tform_dogtoy = get_obj_and_img(
                    network_compute_client, options.ml_service, options.model,
                    options.confidence_dogtoy, kImageSources, 'dogtoy')

                if dogtoy is None:
                    # Didn't find anything, keep searching.
                    continue

                # If we have already dropped the toy off, make sure it has moved a sufficient amount before
                # picking it up again
                if vision_tform_hand_at_drop is not None and pose_dist(
                        vision_tform_hand_at_drop, vision_tform_dogtoy) < 0.5:
                    print('Found dogtoy, but it hasn\'t moved.  Waiting...')
                    time.sleep(1)
                    continue

                print('Found dogtoy...')

                # Got a dogtoy.  Request pick up.

                # Stow the arm in case it is deployed
                stow_cmd = RobotCommandBuilder.arm_stow_command()
                command_client.robot_command(stow_cmd)

                # Walk to the object.
                walk_rt_vision, heading_rt_vision = compute_stand_location_and_yaw(
                    vision_tform_dogtoy, robot_state_client, distance_margin=1.0)

                se2_pose = geometry_pb2.SE2Pose(
                    position=geometry_pb2.Vec2(x=walk_rt_vision[0], y=walk_rt_vision[1]),
                    angle=heading_rt_vision)
                move_cmd = RobotCommandBuilder.synchro_se2_trajectory_command(
                    se2_pose, frame_name=frame_helpers.VISION_FRAME_NAME,
                    params=get_walking_params(0.5, 0.5))
                end_time = 5.0
                cmd_id = command_client.robot_command(command=move_cmd,
                                                      end_time_secs=time.time() + end_time)

                # Wait until the robot reports that it is at the goal.
                block_for_trajectory_cmd(command_client, cmd_id, timeout_sec=5)

                # The ML result is a bounding box.  Find the center.
                (center_px_x, center_px_y) = find_center_px(dogtoy.image_properties.coordinates)

                # Request Pick Up on that pixel.
                pick_vec = geometry_pb2.Vec2(x=center_px_x, y=center_px_y)
                grasp = manipulation_api_pb2.PickObjectInImage(
                    pixel_xy=pick_vec,
                    transforms_snapshot_for_camera=image.shot.transforms_snapshot,
                    frame_name_image_sensor=image.shot.frame_name_image_sensor,
                    camera_model=image.source.pinhole)

                # We can specify where in the gripper we want to grasp. About halfway is generally good for
                # small objects like this. For a bigger object like a shoe, 0 is better (use the entire
                # gripper)
                grasp.grasp_params.grasp_palm_to_fingertip = 0.6

                # Tell the grasping system that we want a top-down grasp.

                # Add a constraint that requests that the x-axis of the gripper is pointing in the
                # negative-z direction in the vision frame.

                # The axis on the gripper is the x-axis.
                axis_on_gripper_ewrt_gripper = geometry_pb2.Vec3(x=1, y=0, z=0)

                # The axis in the vision frame is the negative z-axis
                axis_to_align_with_ewrt_vision = geometry_pb2.Vec3(x=0, y=0, z=-1)

                # Add the vector constraint to our proto.
                constraint = grasp.grasp_params.allowable_orientation.add()
                constraint.vector_alignment_with_tolerance.axis_on_gripper_ewrt_gripper.CopyFrom(
                    axis_on_gripper_ewrt_gripper)
                constraint.vector_alignment_with_tolerance.axis_to_align_with_ewrt_frame.CopyFrom(
                    axis_to_align_with_ewrt_vision)

                # We'll take anything within about 15 degrees for top-down or horizontal grasps.
                constraint.vector_alignment_with_tolerance.threshold_radians = 0.25

                # Specify the frame we're using.
                grasp.grasp_params.grasp_params_frame_name = frame_helpers.VISION_FRAME_NAME

                # Build the proto
                grasp_request = manipulation_api_pb2.ManipulationApiRequest(
                    pick_object_in_image=grasp)

                # Send the request
                print('Sending grasp request...')
                cmd_response = manipulation_api_client.manipulation_api_command(
                    manipulation_api_request=grasp_request)

                # Wait for the grasp to finish
                grasp_done = False
                failed = False
                time_start = time.time()
                while not grasp_done:
                    feedback_request = manipulation_api_pb2.ManipulationApiFeedbackRequest(
                        manipulation_cmd_id=cmd_response.manipulation_cmd_id)

                    # Send a request for feedback
                    response = manipulation_api_client.manipulation_api_feedback_command(
                        manipulation_api_feedback_request=feedback_request)

                    current_state = response.current_state
                    current_time = time.time() - time_start
                    print(
                        'Current state ({time:.1f} sec): {state}'.format(
                            time=current_time,
                            state=manipulation_api_pb2.ManipulationFeedbackState.Name(
                                current_state)), end='                \r')
                    sys.stdout.flush()

                    failed_states = [
                        manipulation_api_pb2.MANIP_STATE_GRASP_FAILED,
                        manipulation_api_pb2.MANIP_STATE_GRASP_PLANNING_NO_SOLUTION,
                        manipulation_api_pb2.MANIP_STATE_GRASP_FAILED_TO_RAYCAST_INTO_MAP,
                        manipulation_api_pb2.MANIP_STATE_GRASP_PLANNING_WAITING_DATA_AT_EDGE
                    ]

                    failed = current_state in failed_states
                    grasp_done = current_state == manipulation_api_pb2.MANIP_STATE_GRASP_SUCCEEDED or failed

                    time.sleep(0.1)

                holding_toy = not failed

            # Move the arm to a carry position.
            print('')
            print('Grasp finished, search for a person...')
            carry_cmd = RobotCommandBuilder.arm_carry_command()
            command_client.robot_command(carry_cmd)

            # Wait for the carry command to finish
            time.sleep(0.75)

            person = None
            while person is None:
                # Find a person to deliver the toy to
                person, image, vision_tform_person = get_obj_and_img(
                    network_compute_client, options.ml_service, options.person_model,
                    options.confidence_person, kImageSources, 'person')

            # We now have found a person to drop the toy off near.
            drop_position_rt_vision, heading_rt_vision = compute_stand_location_and_yaw(
                vision_tform_person, robot_state_client, distance_margin=2.0)

            wait_position_rt_vision, wait_heading_rt_vision = compute_stand_location_and_yaw(
                vision_tform_person, robot_state_client, distance_margin=3.0)

            # Tell the robot to go there

            # Limit the speed so we don't charge at the person.
            se2_pose = geometry_pb2.SE2Pose(
                position=geometry_pb2.Vec2(x=drop_position_rt_vision[0],
                                           y=drop_position_rt_vision[1]), angle=heading_rt_vision)
            move_cmd = RobotCommandBuilder.synchro_se2_trajectory_command(
                se2_pose, frame_name=frame_helpers.VISION_FRAME_NAME,
                params=get_walking_params(0.5, 0.5))
            end_time = 5.0
            cmd_id = command_client.robot_command(command=move_cmd,
                                                  end_time_secs=time.time() + end_time)

            # Wait until the robot reports that it is at the goal.
            block_for_trajectory_cmd(command_client, cmd_id, timeout_sec=5)

            print('Arrived at goal, dropping object...')

            # Do an arm-move to gently put the object down.
            # Build a position to move the arm to (in meters, relative to and expressed in the gravity aligned body frame).
            x = 0.75
            y = 0
            z = -0.25
            hand_ewrt_flat_body = geometry_pb2.Vec3(x=x, y=y, z=z)

            # Point the hand straight down with a quaternion.
            qw = 0.707
            qx = 0
            qy = 0.707
            qz = 0
            flat_body_Q_hand = geometry_pb2.Quaternion(w=qw, x=qx, y=qy, z=qz)

            flat_body_tform_hand = geometry_pb2.SE3Pose(position=hand_ewrt_flat_body,
                                                        rotation=flat_body_Q_hand)

            robot_state = robot_state_client.get_robot_state()
            vision_tform_flat_body = frame_helpers.get_a_tform_b(
                robot_state.kinematic_state.transforms_snapshot, frame_helpers.VISION_FRAME_NAME,
                frame_helpers.GRAV_ALIGNED_BODY_FRAME_NAME)

            vision_tform_hand_at_drop = vision_tform_flat_body * math_helpers.SE3Pose.from_proto(
                flat_body_tform_hand)

            # duration in seconds
            seconds = 1

            arm_command = RobotCommandBuilder.arm_pose_command(
                vision_tform_hand_at_drop.x, vision_tform_hand_at_drop.y,
                vision_tform_hand_at_drop.z, vision_tform_hand_at_drop.rot.w,
                vision_tform_hand_at_drop.rot.x, vision_tform_hand_at_drop.rot.y,
                vision_tform_hand_at_drop.rot.z, frame_helpers.VISION_FRAME_NAME, seconds)

            # Keep the gripper closed.
            gripper_command = RobotCommandBuilder.claw_gripper_open_fraction_command(0.0)

            # Combine the arm and gripper commands into one RobotCommand
            command = RobotCommandBuilder.build_synchro_command(gripper_command, arm_command)

            # Send the request
            cmd_id = command_client.robot_command(command)

            # Wait until the arm arrives at the goal.
            block_until_arm_arrives(command_client, cmd_id)

            # Open the gripper
            gripper_command = RobotCommandBuilder.claw_gripper_open_fraction_command(1.0)
            command = RobotCommandBuilder.build_synchro_command(gripper_command)
            cmd_id = command_client.robot_command(command)

            # Wait for the dogtoy to fall out
            time.sleep(1.5)

            # Stow the arm.
            stow_cmd = RobotCommandBuilder.arm_stow_command()
            command_client.robot_command(stow_cmd)

            time.sleep(1)

            print('Backing up and waiting...')

            # Back up one meter and wait for the person to throw the object again.
            se2_pose = geometry_pb2.SE2Pose(
                position=geometry_pb2.Vec2(x=wait_position_rt_vision[0],
                                           y=wait_position_rt_vision[1]),
                angle=wait_heading_rt_vision)
            move_cmd = RobotCommandBuilder.synchro_se2_trajectory_command(
                se2_pose, frame_name=frame_helpers.VISION_FRAME_NAME,
                params=get_walking_params(0.5, 0.5))
            end_time = 5.0
            cmd_id = command_client.robot_command(command=move_cmd,
                                                  end_time_secs=time.time() + end_time)

            # Wait until the robot reports that it is at the goal.
            block_for_trajectory_cmd(command_client, cmd_id, timeout_sec=5)


def compute_stand_location_and_yaw(vision_tform_target, robot_state_client, distance_margin):
    # Compute drop-off location:
    #   Draw a line from Spot to the person
    #   Back up 2.0 meters on that line
    vision_tform_robot = frame_helpers.get_a_tform_b(
        robot_state_client.get_robot_state().kinematic_state.transforms_snapshot,
        frame_helpers.VISION_FRAME_NAME, frame_helpers.GRAV_ALIGNED_BODY_FRAME_NAME)

    # Compute vector between robot and person
    robot_rt_person_ewrt_vision = [
        vision_tform_robot.x - vision_tform_target.x, vision_tform_robot.y - vision_tform_target.y,
        vision_tform_robot.z - vision_tform_target.z
    ]

    # Compute the unit vector.
    if np.linalg.norm(robot_rt_person_ewrt_vision) < 0.01:
        robot_rt_person_ewrt_vision_hat = vision_tform_robot.transform_point(1, 0, 0)
    else:
        robot_rt_person_ewrt_vision_hat = robot_rt_person_ewrt_vision / np.linalg.norm(
            robot_rt_person_ewrt_vision)

    # Starting at the person, back up meters along the unit vector.
    drop_position_rt_vision = [
        vision_tform_target.x + robot_rt_person_ewrt_vision_hat[0] * distance_margin,
        vision_tform_target.y + robot_rt_person_ewrt_vision_hat[1] * distance_margin,
        vision_tform_target.z + robot_rt_person_ewrt_vision_hat[2] * distance_margin
    ]

    # We also want to compute a rotation (yaw) so that we will face the person when dropping.
    # We'll do this by computing a rotation matrix with X along
    #   -robot_rt_person_ewrt_vision_hat (pointing from the robot to the person) and Z straight up:
    xhat = -robot_rt_person_ewrt_vision_hat
    zhat = [0.0, 0.0, 1.0]
    yhat = np.cross(zhat, xhat)
    mat = np.matrix([xhat, yhat, zhat]).transpose()
    heading_rt_vision = math_helpers.Quat.from_matrix(mat).to_yaw()

    return drop_position_rt_vision, heading_rt_vision


def pose_dist(pose1, pose2):
    diff_vec = [pose1.x - pose2.x, pose1.y - pose2.y, pose1.z - pose2.z]
    return np.linalg.norm(diff_vec)


def get_walking_params(max_linear_vel, max_rotation_vel):
    max_vel_linear = geometry_pb2.Vec2(x=max_linear_vel, y=max_linear_vel)
    max_vel_se2 = geometry_pb2.SE2Velocity(linear=max_vel_linear, angular=max_rotation_vel)
    vel_limit = geometry_pb2.SE2VelocityLimit(max_vel=max_vel_se2)
    params = RobotCommandBuilder.mobility_params()
    params.vel_limit.CopyFrom(vel_limit)
    return params


if __name__ == '__main__':
    if not main(sys.argv[1:]):
        sys.exit(1)