Log Annotation¶
Client for the log-annotation service (DEPRECATED).
The log-annotation service is deprecated and will be removed in a later release. Instead, please use the data_buffer service going forward.
-
exception
bosdyn.client.log_annotation.
InvalidArgument
[source]¶ Bases:
bosdyn.client.exceptions.Error
A given argument could not be used.
-
class
bosdyn.client.log_annotation.
LogAnnotationClient
(*args, **kwargs)[source]¶ Bases:
bosdyn.client.common.BaseClient
A client for adding annotations to robot logs.
-
default_service_name
= 'log-annotation'¶
-
service_type
= 'bosdyn.api.LogAnnotationService'¶
-
add_text_messages
(text_messages, **kwargs)[source]¶ Log text messages to the robot.
- Parameters
text_messages – Sequence of LogAnnotationTextMessage protos.
- Raises
RpcError – Problem communicating with the robot.
-
add_operator_comment
(msg, robot_timestamp=None, **kwargs)[source]¶ Add an operator comment to the robot log.
- Parameters
msg – Text of user comment to log.
robot_timestamp – Time (google.protobuf.Timestamp) of messages, in robot time. If not set, timestamp will be when the robot receives the message.
- Raises
RpcError – Problem communicating with the robot.
-
add_operator_comment_async
(msg, robot_timestamp=None, **kwargs)[source]¶ Async version of add_operator_comment.
-
add_log_blob
(data, type_id, channel=None, robot_timestamp=None, **kwargs)[source]¶ Log blob messages to the robot.
- Parameters
data – Binary data of one blob.
type_id – Type of binary data of blob.
robot_timestamp – Time (google.protobuf.Timestamp) of messages, in robot time. If not set, timestamp will be when the robot receives the message.
- Raises
RpcError – Problem communicating with the robot.
-
-
class
bosdyn.client.log_annotation.
LogAnnotationHandler
(*args, **kwargs)[source]¶ Bases:
logging.Handler
A logging system Handler that will publish text to a bosdyn.api.LogAnnotationService.
- Parameters
service – Name of the service. See LogAnnotationTextMessage.
log_client – API client that will send log messages.
level – Python logging level. Defaults to NOTSET.
time_sync_endpoint – A TimeSyncEndpoint, already synchronized to the remote clock.
rpc_timeout – Timeout on RPCs made by log_client.
msg_num_limit – If number of messages reaches this number, send data with log_client.
msg_age_limit – If messages have been sitting locally for this many seconds, send data with log_client.
- Raises
log_annotation.InvalidArgument – The TimeSyncEndpoint is not valid.
-
emit
(record)[source]¶ Do whatever it takes to actually log the specified logging record.
This version is intended to be implemented by subclasses and so raises a NotImplementedError.
-
flush
()[source]¶ Ensure all logging output has been flushed.
This version does nothing and is intended to be implemented by subclasses.
-
close
()[source]¶ Tidy up any resources used by the handler.
This version removes the handler from an internal map of handlers, _handlers, which is used for handler lookup by name. Subclasses should ensure that this gets called from overridden close() methods.