API Example - World Object Service with Image Coordinates

These examples demonstrate how to use the world object service to inform Spot and store pixel coordinates on an image without any frame information.

Setup Dependencies

These examples need to be run with python3, and have the SDK 2.0 installed. See the requirements.txt file for a list of dependencies which can be installed with pip using:

python -m pip install -r requirements.txt

Running the Example

To run the example:

python add_image_coordinates.py --username USER --password PASSWORD ROBOT_IP