Keepalive Service
The Keepalive service unifies and expands the comms-loss behaviors of Spot. It lets a client specify one or more Policies, each containing one or more actions. Each action will automatically occur if a client does not send a CheckInRequest within a configurable amount of time.
For example, you may send a ModifyPolicyRequest that adds the following Policy:
“If this robot does not receive a CheckIn for this Policy, take these actions: After 10 seconds, record an Event. After 15 seconds, begin AutoReturn. After 25 seconds, shut off motor power. After 60 seconds, turn off the robot.”
Clients may add or remove a Policy at any time, and the robot does not need any Policy to operate.
Policy
A Policy tells the robot what to do, when. Zero or more clients may have zero or more Policies on the robot at any time.
The Policy timer
When a Policy is added, the Keepalive service
provides the client with an ID for that Policy.
starts a timer associated with the ID.
The Policy’s timer is reset to 0 when the Policy is added or “checked into”. Each Policy has a separate timer. The timer increments along with the robot’s clock. When the timer increments past an action’s associated duration, the action will automatically happen.
Actions
The following actions are available in a Policy:
Record one or more Events, as if via the DataBufferService.
Begin AutoReturn, as if via the AutoReturnService.
Come to a controlled stop, then power motors off.
Immediately power the motors AND robot computers off.
Mark a Lease as stale.
Most actions can be configured by the client. For example, for the RecordEvent action, the client specifies the Events to be recorded.
Removing a Policy
There are two main ways of removing a Policy.
Explicitly, by adding the target Policy ID to the
policy_ids_to_removefield ofModifyPolicyRequest.Implicitly, by adding to the
associated_leaseson the Policy.
For example, if a client has acquired leaseA = [6] from the robot and adds that lease to the associated_leases field of Policy 1, the next time the robot gives out leaseB = [7], Policy 1 will automatically be removed.
Backwards compatibility
The Keepalive service shares some features with other services, namely
The E-Stop Service
The “staleness” feature of the Lease Service
These other services will still work as usual if the Keepalive service is not used, with a few exceptions:
It is now valid to have no E-Stop configuration.
If an E-Stop configuration with Endpoints is set, and one or more Endpoints time out, the error will reference the Keepalive service.
If you are using the Keepalive service, you may notice a few things:
Registering an E-Stop Endpoint automatically adds a Policy with a matching timeout.
Acquiring a Lease automatically adds a Policy with LeaseStale actions at the previously hardcoded timeout.
It is safe to remove those auto-generated Policies if you wish.