File Indexer
A FileIndexer is an object which keeps an index of series and blocks within series
- class bosdyn.bddf.file_indexer.FileIndexer[source]
Bases:
objectAn object which keeps an index of series and blocks within series.
It can write a block index at the end of a data file.
- property file_index
Get the FileIndex proto used which describes how to access data in the file.
- property descriptor_index
Get the Descriptor proto containing the FileIndex.
- property series_block_indexes
series_index -> SeriesBlockIndex.
- Type:
Returns the current list of SeriesBlockIndexes
- static series_identifier_to_hash(series_identifier)[source]
Given a SeriesIdentifier, return a 64-bit hash.
- add_series_descriptor(series_descriptor, series_block_file_offset)[source]
Add the given series_descriptor to the index, with the given file offset.
- Parameters:
index (series_descriptor SeriesDescriptor to add to the) –
written (series_block_file_offset Location in file where SeriesDescriptor will be) – was read from.
or – was read from.
- add_series(series_type, series_spec, message_type, pod_type, annotations, additional_index_names, writer)[source]
Register a new series for messages for a DataWriter.
- Parameters:
series_type – the kind of spec, corresponding to the set of keys expected in series_spec.
series_spec – dict of {key (string) -> value (string)} describing the series.
message_type – MessageTypeDescriptor (need EITHER this OR pod_type)
pod_type – PodTypeDescriptor (need EITHER this OR pod_type)
annotations – optional dict of key (string) -> value (string) pairs to associate with the message channel
additional_index_names – names of additional timestamps to store with each message (list of string).
writer – BlockWriter owned by the DataWriter.
Returns series id (int).
Raises SeriesNotUniqueError if a series matching series_spec is already added.
- index_data_block(series_index, timestamp_nsec, file_offset, nbytes, additional_indexes)[source]
Add an entry to the data block index of the series identified by series_index.