Metrics Logging
Clients for the metrics logging service.
- exception bosdyn.client.metrics_logging.MissingKeysError(response, error_message=None)[source]
- Bases: - ResponseError- Metrics requested from the metrics service did not exist. 
- exception bosdyn.client.metrics_logging.UnableToOptOutError(response, error_message=None)[source]
- Bases: - ResponseError- Unable to opt-out of metrics logging due to invalid license permissions. 
- class bosdyn.client.metrics_logging.MetricsLoggingClient[source]
- Bases: - BaseClient- A client for the metrics logging service on the robot. - default_service_name = 'metrics-logging'
 - service_type = 'bosdyn.api.metrics_logging.MetricsLoggingRobotService'
 - get_metrics(keys=None, include_events=False, **kwargs)[source]
- Get metrics from the robot. - Parameters:
- keys (List[strings]) – A list of strings representing the keys for metrics that should be returned. 
- include_events (bool) – Whether events should be included in the response. 
 
- Returns:
- The GetMetricsResponse response. 
- Raises:
- RpcError – Problem communicating with the robot. 
 
 - get_metrics_async(keys=None, include_events=False, **kwargs)[source]
- Async version of get_metrics(). 
 - get_store_sequence_range(**kwargs)[source]
- Determine the range of sequence numbers currently being used by the metrics system’s store. - Returns:
- A list where the first number represents the starting index (inclusive), and the second number represents the final index (inclusive) for the entries in the metrics store. 
- Raises:
- RpcError – Problem communicating with the robot. 
 
 - get_absolute_metric_snapshot(sequence_numbers, **kwargs)[source]
- Get absolute metric snapshots for specific sequence numbers’ entries. - Parameters:
- sequence_numbers (List(int)) – The list of sequence numbers whose entries should be returned as absolute metric snapshots. 
- Returns:
- A list of signed_proto_pb2.SignedProto(). Each signed proto will contain the serialized absolute_metric_pb2.AbsoluteMetricsSnapshot() for the requested sequence number’s timestamp. The robot will exclude snapshots if the sequence number does not exist, or the response will exceed the grpc limit. 
- Raises:
- RpcError – Problem communicating with the robot.