Protobuf Reader
A class for reading Protobuf data from a DataFile.
- class bosdyn.bddf.protobuf_reader.ProtobufReader(data_reader)[source]
Bases:
MessageReaderA class for reading Protobuf data from a DataFile.
Methods raise ParseError if there is a problem with the format of the file.
- get_message(series_index, protobuf_type, index_in_series)[source]
Return a deserialized protobuf from bytes stored in the file.
- Parameters:
series_index – index (int) from the series_index() call
protobuf_type – class of the protobuf we want to deserialize
index_in_series – the index of the message within the series
Returns: DataTypeDescriptor for channel, timestamp_nsec (int), deserialized protobuf object