Network Compute Bridge
The network compute bridge allows you to off-load computation to another computer on the network. For example, you might want to offload a deep neural-network call to a server in the cloud.
Examples:
tensorflow_server.py: Processes requests to run a Faster R-CNN TensorFlow model on Spot image data.Registers a Network Compute Bridge Worker with the Spot directory service
Handles Network Compute queries and executes the TensorFlow model on the image or image source input
Can be easily reconfigured to run other TensorFlow object detection models
identify_object.py: Requests identification on an image using a TensorFlow model.Client requests an image source, such as
frontleft_fisheye_imageRobot takes image, rotates it to align with the horizon and sends it to a server running
tensorflow_server.py.Results are returned to the client. If depth data is available inside the bounding box, the robot adds depth to the result.
Fire Extinguisher Server: Example of a network compute bridge server for detecting fire extinguishers that uses Keras Retinanet instead of TensorFlow.
simple_alert_server.py: Registers a Network Compute Bridge alert-generating worker server and triggers a Data Acquisition request to generate captures with the alert.
System Diagram

Installation
Server
These examples require the bosdyn API and client to be installed, and must be run using python3.
The tensorflow_server.py example requires TensorFlow to be installed. You can install its
dependencies via:
python3 -m pip install -r requirements_server.txt
TensorFlow can use the GPU for better performance but installation of NVIDIA drivers and CUDA is outside the scope of the document. There are many tutorials available such as this one.
Client
The client example (identify_object.py) does not require TensorFlow:
python3 -m pip install -r requirements_client.txt
Execution
To run this example, first launch the server and direct it to your Spot:
python3 tensorflow_server.py -d <MODEL DIRECTORY> <ROBOT ADDRESS>
USERNAMEandPASSWORDare your user credentials for your Spot.MODEL DIRECTORYis the path to the directory containing the TensorFlow model to be hosted.ROBOT ADDRESSis the IP address or hostname of your Spot.
An example model directory can be obtained here: https://github.com/tensorflow/models/blob/master/research/object_detection/g3doc/tf1_detection_zoo.md. As an example, use the frozen_inference_graph.pb file from the faster_rcnn_inception_v2_coco model to detect people in the camera images.
To associate numeric labels with names, the user may optionally provide a CSV file in the model directory with a matching file name, e.g. frozen_inference_graph.csv, with the following format:
apples,1
oranges,2
Where 1 and 2 are possible label outputs for detections from the TensorFlow model and apples and oranges are their respective semantic names. The tensorflow_server.py example output indicates if a CSV has been loaded to associate label values with names.
An example CSV file for the Faster R-CNN model described above is included in this directory as frozen_inference_graph.csv.
After launching tensorflow_server.py, the user may post requests to it using the identify_object.py client example. To run this example with the above example server and model, run:
python3 identify_object.py --service <SERVICE_NAME> --model <MODEL_NAME> <ROBOT_IP>
For example:
python3 identify_object.py --service tensorflow-server --confidence 0.5 --model frozen_inference_graph --image-source frontleft_fisheye_image <ROBOT_IP>
Note, the USERNAME and PASSWORD are your user credentials for your Spot.
Simple Alert Server Execution
To run the simple_alert_server.py example:
python3 simple_alert_server.py <ROBOT ADDRESS>
Optionally, pass -p <PORT> to the command above to specify the port used by the server. This command generates a zip file with the captures from an acquisition request. The zip file contains two copies of an image captured from the robot back camera, and a metadata.json file that contains alert_data:simple-alert-server_alert_model_alert_output key with the alert values.
Robot-independent Execution
To run this example without a robot in the pipeline, first launch the server with the “-r” flag:
python3 tensorflow_server.py -r -d <MODEL DIRECTORY>
After launching tensorflow_server.py, the user may post requests to it using the identify_object_without_robot.py client example. To run this example with the above example server and model, run:
python3 identify_object_without_robot.py --model <MODEL_NAME> --server <SERVER_IP:PORT> --confidence 0.5 --model frozen_inference_graph
For example:
python3 identify_object_without_robot.py --server localhost:50051 --confidence 0.5 --model frozen_inference_graph --input-image-dir ~/Download/images/ -v
Example output:
Got 2 objects.
name: "obj1_label_person"
image_properties {
coordinates {
vertexes {
x: 1146.0
y: 27.0
}
--- cut ---
Docker Execution
This example contains the configuration files to run the python scripts described above also in Docker containers. The docker containers accept the same arguments described above. For example, to run the server docker container and the client docker container, follow the steps below with the correct values for the <> variables:
Create a .env file that specifies username and password with the following variables.
BOSDYN_CLIENT_USERNAME={username}
BOSDYN_CLIENT_PASSWORD={password}
sudo docker build -t ncb_server -f Dockerfile.server .
sudo docker run -it --network=host --env-file .env -v <MODEL_DIRECTORY>:/model_dir/ ncb_server --model-dir /model_dir/ <ROBOT_IP>
sudo docker build -t ncb_client -f Dockerfile.client .
sudo docker run -it --network=host --env-file .env ncb_client --service tensorflow-server --confidence 0.5 --model frozen_inference_graph --image-source frontleft_fisheye_image <ROBOT_IP>
When running ncb_server on CORE I/O, or another compute payload with GPU, pass the flag --gpus all to the docker run command to take advantage of the GPU.
Troubleshooting
Ensure that your firewall is allowing traffic on the specified port (default: 50051).