Fire Extinguisher Detector Server¶
This is an example of a network compute bridge server. It is similar to tensorflow_server.py, but uses Keras Retinanet instead of TensorFlow. The provided model specifically detects fire extinguishers
Build and Export¶
This example can be run on a local machine directly, but is easier to use with Docker.
The Docker image can be built and exported with the following commands:
# builds the image
sudo docker build -t fire_ext_detector .
# exports the image, uses pigz
sudo docker save fire_ext_detector | pigz > fire_ext_detector.tar.gz
To build the image for CORE I/O:
# Prerequisites
# Install the pigz and qemu packages
sudo apt-get install qemu binfmt-support qemu-user-static pigz
# This step will execute the registering scripts
docker run --rm --privileged multiarch/qemu-user-static --reset -p yes
# Builds the image
sudo docker build -t fire_ext_detector:l4t -f Dockerfile.l4t .
# Exports the image, uses pigz
sudo docker save fire_ext_detector:l4t | pigz > fire_ext_detector.tar.gz
Execution¶
To run this example on a Spot CORE, run:
./start_server.sh
Otherwise, run:
sudo docker run -d --name retinanet_server --network host --env BOSDYN_CLIENT_USERNAME --env BOSDYN_CLIENT_PASSWORD --restart unless-stopped fire_ext_detector -d . --port $PORT $ROBOT_IP
$PORT
is the port to use for the server on the machine the server is running on$ROBOT_IP
is the IP address or hostname of your Spot.$USERNAME
is the username for the robot$PASSWORD
is the password for the robot
To run this example on a CORE I/O, run:
# Load the image
sudo docker load -i fire_ext_detector.tar.gz
# Run the container
sudo docker run -d \
--gpus all \
--name retinanet_server \
--network host \
--restart unless-stopped \
-v /opt/payload_credentials/payload_guid_and_secret:/opt/payload_credentials/payload_guid_and_secret \
fire_ext_detector:l4t \
-d . 192.168.50.3 --payload-credentials-file /opt/payload_credentials/payload_guid_and_secret
Spot Extension for CORE I/O¶
This example also provides a script for building the fire extinguisher detector into a Spot Extension.
This script requires the same prerequisites as listed above for building a docker image for CORE I/O.
Additionally, this script requires that the current user be added to the docker
user group.
If this is not the case, the script needs to be run with root privileges.
./create_extension.sh
The output file will be called fire_ext_detector.spx and can be uploaded to a CORE I/O.