Channel¶
-
class
bosdyn.client.channel.
RefreshingAccessTokenAuthMetadataPlugin
(token_cb, add_app_token)[source]¶ Bases:
grpc.AuthMetadataPlugin
Plugin to refresh access token.
- Parameters
token_cb – Callable that returns a tuple of (app_token, user_token)
add_app_token (bool) – Whether to include an app token in the metadata. This is necessary for compatibility with old robot software.
-
bosdyn.client.channel.
create_secure_channel_creds
(cert, token_cb, add_app_token)[source]¶ Returns credentials for establishing a secure channel. Uses previously set values on the linked Sdk and self.
-
bosdyn.client.channel.
create_secure_channel
(address, port, creds, authority, options=[])[source]¶ Create a secure channel to given host:port.
- Parameters
address – Connection host address.
port – Connection port.
creds – A ChannelCredentials instance.
authority – Authority option for the channel.
options – A list of additional parameters for the GRPC channel.
- Returns
A secure channel.
-
bosdyn.client.channel.
create_insecure_channel
(address, port, authority=None, options=[])[source]¶ Create an insecure channel to given host and port.
This method is only used for testing purposes. Applications must use secure channels to communicate with services running on Spot.
- Parameters
address – Connection host address.
port – Connection port.
authority – Authority option for the channel.
options – A list of additional parameters for the GRPC channel.
- Returns
An insecure channel.
-
bosdyn.client.channel.
translate_exception
(rpc_error)[source]¶ Translated a GRPC error into an SDK RpcError.
- Parameters
rpc_error – RPC error to translate.
- Returns
Specific sub-type of RpcError.
-
bosdyn.client.channel.
generate_channel_options
(max_send_message_length=None, max_receive_message_length=None)[source]¶ Generate the array of options to specify in the creation of a client channel or server.
The list contains the values for max allowed message length for both sending and receiving. If no values are provided, the default values of 100 MB are used.
- Parameters
max_send_message_length (int) – Max message length allowed for message to send.
max_receive_message_length (int) – Max message length allowed for message to receive.
- Returns
Array with values for channel options.