Anomalies in Orbit
This Orbit API example demonstrates how to retrieve and edit anomaly data with a Boston Dynamics Orbit API client.
Understanding Orbit Web API
Please begin with the Quickstart Guide to get your Python programming environment set up properly. Then, specifically for this example, look at the Orbit API Docs. For a complete list of resources and their methods, see the Orbit API Reference.
Setup Dependencies
See the requirements.txt file for a list of python dependencies which can be installed with pip using the command:
python3 -m pip install -r requirements.txt
Run the Example
To run the example to get anomalies stored on your Orbit instance, run the following command with verify set to False. When set to False, requests will skip server’s TLS certificate verifications which will make your application vulnerable. For production software, we recommend you set verify to True or a path to CA bundle.
python3 get_anomalies.py --hostname ORBIT_IP --verify False
To close multiple anomaly alerts at once obtain their elementIds from the get_anomalies.py example and use them as arguments in the following command:
python3 patch_anomalies.py --hostname ORBIT_IP --bulk-close-element-ids ELEMENT_ID_1 ELEMENT_ID_2 ELEMENT_ID_3 --verify False
To edit an anomaly alert, obtain the anomaly uuid from the get_anomalies.py example and use it as an argument in the following command, and set the status flag to open or closed and patch the anomaly:
python3 patch_anomalies.py --hostname ORBIT_IP --anomaly-uuid ANOMALY_UUID_1 --status STATUS --verify False
Command to open a specific anomaly:
python3 patch_anomalies.py --hostname ORBIT_IP --anomaly-uuid ANOMALY_UUID_1 --status open --verify False
Command to close a specific anomaly:
python3 patch_anomalies.py --hostname ORBIT_IP --anomaly-uuid ANOMALY_UUID_1 --status closed --verify False
The above command prompts you to provide the API token obtained from the Orbit admin settings page. Alternatively, you can set the environment variable BOSDYN_ORBIT_CLIENT_API_TOKEN
to the API token obtained from Orbit admin settings page.