Docking
A client for the docking service.
- class bosdyn.client.docking.DockingClient[source]
Bases:
BaseClientA client for the docking service to help issue DockingCommand and get state. Clients are expected to issue a single DockingCommand and then periodically check the status of its execution. This service requires ownership over the robot, in the form of a lease and timesync.
- default_service_name = 'docking'
- service_type = 'bosdyn.api.docking.DockingService'
- docking_command(station_id, clock_identifier, end_time, prep_pose_behavior=None, lease=None, **kwargs)[source]
Issue a DockingCommandRequest to the robot.
- Parameters:
station_id – The ID of the docking station to dock at.
clock_identifier – Identifier provided by the time sync service.
end_time – Expiry time of the command in robot time.
prep_pose_behavior – [optional] How and if to use the pre-dock pose.
lease – [optional] Leave empty to have the lease filled in by the LeaseWallet
- Returns:
DockingCommand ID
- Raises:
ResponseError – The command was unable to be completed. See error for details.
- docking_command_async(station_id, clock_identifier, end_time, prep_pose_behavior=None, lease=None, **kwargs)[source]
Async version of docking_command().
- docking_command_full(station_id, clock_identifier, end_time, prep_pose_behavior=None, lease=None, require_fiducial=False, **kwargs)[source]
Identical to docking_command(), except will return the full DockingCommandResponse.
- docking_command_full_async(station_id, clock_identifier, end_time, prep_pose_behavior=None, lease=None, require_fiducial=False, **kwargs)[source]
Identical to docking_command_async(), except will return the full DockingCommandResponse.
- docking_command_feedback_full(command_id, end_time=None, **kwargs)[source]
Check the status of a previously issued docking command.
- Parameters:
command_id – The ID returned from a previous docking_command call.
- Raises:
RpcError – problem communicating with the robot
- Returns:
DockingCommandFeedbackResponse
- docking_command_feedback_full_async(command_id, end_time=None, **kwargs)[source]
Async version of docking_command_feedback_full().
- docking_command_feedback(command_id, **kwargs)[source]
Check the status of a previously issued docking command.
- Parameters:
command_id – The ID returned from a previous docking_command call.
- Returns:
Status of type DockingCommandFeedbackResponse.Status
Deprecated since version 3.0.0: This function can raise LeaseErrors when the feedback was successfully retrieved. Use docking_command_feedback_full instead.
- docking_command_feedback_async(command_id, **kwargs)[source]
Async version of docking_command_feedback().
Deprecated since version 3.0.0: This function can raise LeaseErrors when the feedback was successfully retrieved. Use docking_command_feedback_full_async instead.
- get_docking_config(**kwargs)[source]
Get the docking config stored on the robot.
- Returns:
List of docking configs of type ConfigRange
- bosdyn.client.docking.blocking_dock_robot(robot, dock_id, num_retries=4, timeout=30)[source]
Blocking helper that takes control of the robot and docks it.
- Parameters:
robot – The instance of the robot to control.
dock_id – The ID of the dock to dock at.
num_retries – Optional, number of attempts.
- Returns:
The number of retries required
- Raises:
CommandFailedError – The robot was unable to be docked. See error for details.
- bosdyn.client.docking.blocking_go_to_prep_pose(robot, dock_id, timeout=20)[source]
Blocking helper that takes control of the robot and takes it to the prep pose only.
- Parameters:
robot – The instance of the robot to control.
dock_id – The ID of the dock to use.
- Returns:
None
- Raises:
CommandFailedError – The robot was unable to go to the prep pose. See error for details.
- bosdyn.client.docking.blocking_undock(robot, timeout=20)[source]
Blocking helper that undocks the robot from the currently docked dock.
- Parameters:
robot – The instance of the robot to control.
- Returns:
None
- Raises:
CommandFailedError – The robot was unable to undock. See error for details.