Animation File To Proto
A tool to convert animation files into protobuf messages which can be uploaded to the robot and used within choreography sequences.
- exception bosdyn.choreography.client.animation_file_to_proto.AnimationFileFormatError[source]
Bases:
Exception
Specific Exception raised when we identify an issue with an animation (.cha) file.
- class bosdyn.choreography.client.animation_file_to_proto.Animation[source]
Bases:
object
Helper class to track values read from the animation file that are important to choreographer and necessary when uploading animated moves.
- bosdyn.choreography.client.animation_file_to_proto.set_proto(proto_object, attribute_name, attribute_value)[source]
Helper function to set a field to a specific value in the protobuf message.
- Parameters:
proto_object (Protobuf message) – Any generic protobuf message.
attribute_name (String) – The field name within the protobuf message.
attribute_value – A value with type matching the field type defined in the protobuf message definition. This will be saved in the attribute_name field.
- Returns:
Nothing. Mutates the input proto_object to update the specified field name to the provided value.
- bosdyn.choreography.client.animation_file_to_proto.handle_nested_double_value_params(proto_object, name, attribute_value)[source]
Helper function to set a field to a DoubleValue protobuf in a protobuf message.
- Parameters:
proto_object (Protobuf message) – Any generic protobuf message.
name (String) – The field name within the protobuf message. This name should be both the field name and sub-field name separated by a period. For example, for the Vec3 velocity field, the name would be ‘velocity.x’.
attribute_value – A value with type matching the field type defined in the protobuf message definition. This will be saved in the attribute_name field.
- Returns:
Nothing. Mutates the input proto_object to update the specified field name to the provided value.
- bosdyn.choreography.client.animation_file_to_proto.read_animation_params(animation)[source]
Parses the set of lines that are the parameters section of the file.
Reads the parameter lines into the min/max/default values in the Animation proto.
- Parameters:
animation (Animation) – The animation class structure containing the parameter lines.
- Returns:
The mutated animation class, which now contains populated params fields in the animation’s protobuf.
- bosdyn.choreography.client.animation_file_to_proto.read_and_find_animation_params(animate_move_params_file, filepath_input=True)[source]
Create a mapping of the parameter name to the default parameter values.
- Parameters:
animate_move_params_file (string) – filepath to the default parameters file, or a string representing the contents of the parameters file.
filepath_input (boolean) – With filepath_input set to True, the animate_move_params_file argument will be interpreted as a file path to the default parameters file. When set to False, the animate_move_params_file argument will be read as the information in the default parameters file passed as a string.
- Returns:
A dictionary containing the parameter name as the key, and the full parameter line from the file as the value.
- bosdyn.choreography.client.animation_file_to_proto.convert_animation_file_to_proto(animated_file, animate_move_params_file='')[source]
Parses a file into the animation proto that will be uploaded to the robot.
- Parameters:
animated_file (string) – The filepath to the animation text file.
animate_move_params_file (string) – [Required if needing default param values. Otherwise optional] The filepath to a default set of move parameters or move parameters as a string.
- Returns:
The Animation class, which contains the animation proto to be uploaded to the robot, as well as additional information to be used by Choreographer.
- bosdyn.choreography.client.animation_file_to_proto.write_animation_to_dest(animation, destination)[source]
Write the new animation proto to a .cap file.
- Parameters:
animation (Animation class) – The animation class object generated by the cha file conversion helpers to save the protobuf from.
destination (string) – The full filepath to the location to save the animation protobuf message.