Data Acquisition Helpers¶
-
bosdyn.client.data_acquisition_helpers.
issue_acquire_data_request
(data_acq_client, acquisition_requests, group_name, action_name, metadata=None)[source]¶ Sends the data acquisition request without blocking until the acquisition completes.
- Parameters
data_acq_client – DataAcquisition client for send the acquisition requests.
acquisition_requests – Acquisition requests to include in request message.
group_name – Group name for the acquisitions.
action_name – Action name for the acquisitions.
metadata – Metadata to include in the request message.
- Returns
The request id (int) and the action id (CaptureActionId). A request id set as None indicates the AcquireData rpc failed.
-
bosdyn.client.data_acquisition_helpers.
acquire_and_process_request
(data_acquisition_client, acquisition_requests, group_name, action_name, metadata=None, block_until_complete=True)[source]¶ Send acquisition request and optionally block until the acquisition completes.
If blocking, the GetStatus RPC is used to monitor the status of the acquisition request.
- Parameters
data_acquisition_client (DataAcquisitionClient) – The client for send the acquisition requests.
acquisition_requests (data_acquisition_pb2.AcquisitionRequestList) – Acquisition requests to include in request message.
group_name (string) – Group name for the acquisitions.
action_name (string) – Action name for the acquisitions.
metadata (data_acquisition_pb2.Metadata) – Metadata to include in the request message.
block_until_complete (Boolean) – If true, don’t return until the GetStatus completes.
- Returns
Boolean indicating if the acquisition completed successfully or not.
-
bosdyn.client.data_acquisition_helpers.
cancel_acquisition_request
(data_acq_client, request_id)[source]¶ Cancels an acquisition request based on the request id
- Parameters
data_acq_client – DataAcquisition client for send the acquisition requests.
request_id – The id number for the AcquireData request to cancel.
- Returns
None.
-
bosdyn.client.data_acquisition_helpers.
clean_filename
(filename)[source]¶ Removes bad characters in a filename.
- Parameters
filename (string) – Original filename to clean.
- Returns
*?<>|
- Return type
Valid filename with removed characters
-
bosdyn.client.data_acquisition_helpers.
make_time_query_params
(start_time_secs, end_time_secs, robot)[source]¶ Create time-based query params for the download request.
- Parameters
start_time_secs (float) – The start time for the download data range.
end_time_secs (float) – The end time for the download range.
robot (Robot) – The robot object, used to acquire timesync and convert the times to robot time.
- Returns
The query params (data_acquisition_store_pb2.DataQueryParams) for the time-range download.
-
bosdyn.client.data_acquisition_helpers.
make_time_query_params_from_group_name
(group_name, data_store_client)[source]¶ Create time-based query params for the download request using the group name.
- Parameters
group_name (string) – The group name for the data to be downloaded.
data_store_client (DataAcquisitionStoreClient) – The data store client, used to get the action ids for the group name.
- Returns
The query params (data_acquisition_store_pb2.DataQueryParams) for the time-range download.
-
bosdyn.client.data_acquisition_helpers.
download_data_REST
(query_params, hostname, token, destination_folder='.', additional_params=None)[source]¶ Retrieve all data for a query from the DataBuffer REST API and write it to files.
- Parameters
query_params (bosdyn.api.DataQueryParams) – Query parameters to use to retrieve metadata from the DataStore service. Must be time-based query parameters only.
hostname (string) – Hostname to specify in URL where the DataBuffer service is running.
token (string) – User token to specify in https GET request for authentication.
destination_folder (string) – Folder where to download the data.
additional_params (dict) – Additional GET parameters to append to the URL.
- Returns
Boolean indicating if the data was downloaded successfully or not.