Server Util¶
Helper functions and classes for creating and running a gRPC service.
-
class
bosdyn.client.server_util.
ResponseContext
(response, request, rpc_logger=None, channel_prefix=None)[source]¶ Bases:
object
Helper to log gRPC request and response message to the data buffer for a service.
It should be called using a “with” statement each time an RPC is received such that the request and response proto messages can be passed in. It will automatically log the request and response to the data buffer, and mutates the headers to add additional information before logging.
- Parameters
response (protobuf) – any gRPC response message with a bosdyn.api.ResponseHeader proto.
request (protobuf) – any gRPC request message with a bosdyn.api.RequestHeader proto.
rpc_logger (DataBufferClient) – Optional data buffer client to log the messages; if not provided, only the headers will be mutated and nothing will be logged.
channel_prefix (string) – the prefix you want this req / resp pair logged under.
-
class
bosdyn.client.server_util.
GrpcServiceRunner
(service_servicer, add_servicer_to_server_fn, port=0, max_workers=4, max_send_message_length=None, max_receive_message_length=None, timeout_secs=3, force_sigint_capture=True, logger=None)[source]¶ Bases:
object
A runner to start a gRPC server on a background thread and allow easy cleanup.
- Parameters
service_servicer (custom servicer class derived from ServiceServicer) – Servicer that defines server behavior.
add_servicer_to_server_fn (function) – Function generated by gRPC compilation that attaches the servicer to the gRPC server.
port (int) – The port number the service can be accessed through on the host system. Defaults to 0, which will assign an ephemeral port.
max_send_message_length (int) – Max message length (bytes) allowed for messages sent.
max_receive_message_length (int) – Max message length (bytes) allowed for messages received.
timeout_secs (int) – Number of seconds to wait for a clean server shutdown.
force_sigint_capture (bool) – Re-assign the SIGINT handler to default in order to prevent other scripts from blocking a clean exit. Defaults to True.
logger (logging.Logger) – Logger to log with.
-
bosdyn.client.server_util.
populate_response_header
(response, request, error_code=1, error_msg=None)[source]¶ Sets the ResponseHeader header in the response. :param response: The GRPC response message to be populated. :type response: bosdyn.api Response message :param request: The header from the request is added to the response. :type request: bosdyn.api Request message :param error_code: The status for the RPC response. :type error_code: header_pb2.CommonError :param error_msg: An optional error message describing a bad header status failure. :type error_msg: str
- Returns
Mutates the response message’s header to be fully populated.
-
bosdyn.client.server_util.
strip_large_bytes_fields
(proto_message)[source]¶ Removes any large bytes fields from a protobuf message depending on the proto type.
-
bosdyn.client.server_util.
get_bytes_field_allowlist
()[source]¶ Creates set of protos which will have bytes fields removed.
-
bosdyn.client.server_util.
strip_image_response
(proto_message)[source]¶ Removes bytes from the image_pb2.ImageResponse proto.
-
bosdyn.client.server_util.
strip_get_image_response
(proto_message)[source]¶ Removes bytes from the image_pb2.GetImageResponse proto.
-
bosdyn.client.server_util.
strip_local_grid_responses
(proto_message)[source]¶ Removes bytes from the local_grid_pb2.GetLocalGridsResponse proto.
-
bosdyn.client.server_util.
strip_store_image_request
(proto_message)[source]¶ Removes bytes from the data_acquisition_store_pb2.StoreImageRequest proto.
-
bosdyn.client.server_util.
strip_store_data_request
(proto_message)[source]¶ Removes bytes from the data_acquisition_store_pb2.StoreDataRequest proto.
-
bosdyn.client.server_util.
strip_record_signal_tick
(proto_message)[source]¶ Removes bytes from the data_buffer_pb2.RecordSignalTicksRequest proto.