Retrieving Mission state¶
This example program demonstrates how to retrieve information about the state of the currently-running mission.
Setup Dependencies¶
See the requirements.txt file for a list of python dependencies which can be installed with pip using the command:
python3 -m pip install -r requirements.txt
Running the Example¶
To run the example:
python3 get_mission_state.py --username USER --password PASSWORD ROBOT_IP