Comms image service¶
This service creates a virtual camera device that can be selected on the controller and displays a map of wifi signal strength. This example will register itself as a payload, which will need to be authorized in the robot’s admin console. The payload dimensions, location, and weight are small values.
How to use¶
Running locally:¶
pip install -r docker-requirements.txt
python3 comms_image_service.py [options] --host-ip <computer IP> <robotIP>
When using a Docker image on CORE:¶
Build using included Dockerfile then save to a .tar
Upload image tarfile using Portainer on CORE and create a new container from the image
Under “Network ports configuration”, expose a port number (e.g. 7223)
Set the restart policy to “Always Unless Stopped”
In the “Advanced container settings”, put
--port {PORT_NUM}
From the command line (alternate method):¶
sudo docker run -it -p {PORT_NUM}:{PORT_NUM} {comms_image_service} --port {PORT_NUM}