Stitch Front Spot Images Together¶
This programming example shows how to take two fisheye front images from a Spot ImageResponse and stitch them together. Note that due to its graphics-intensive nature, this operation is not performed on robot. This example is adapted from the Spot Tablet solution.
Required Items¶
none
Installation Steps¶
Install Packages on PC¶
Navigate via the CLI on your PC to the stitch_front_images directory and review the requirements.txt file. Several python packages are described and can be installed using the following command line:
python3 -m pip install -r requirements.txt
To execute¶
python3 stitch_front_images.py