Arm JointMove Command¶
An example of commanding a JointMove with Spot’s arm. The example initializes the SDK to talk to robot and then requests Spot to stand before executing the JointMove trajectory.
Understanding Spot Programming¶
For your best learning experience, please use the Quickstart Guide found in the SDK’s docs/python directory. That will help you get your Python programming environment set up properly.
Common Problems¶
Remember, you will need to launch a software e-stop separately. The E-Stop programming example is here.
Make sure the Motor Enable button on the Spot rear panel is depressed.
Make sure Spot is sitting upright, with the battery compartment on the side closest the floor.
Setup Dependencies¶
This example requires the bosdyn API and client to be installed, and must be run using python3. Using pip, these dependencies can be installed using:
python3 -m pip install -r requirements.txt
Run the Example¶
To run the example:
python3 arm_joint_move.py --username USER --password PASSWORD ROBOT_IP