Controlling the Robot with an Xbox Controller¶
Xbox Controller example allows users to control a Spot robot through an Xbox controller. The example was tested with an Xbox 360 wired controller. The button mapping is:
Button Combination | Functionality |
---|---|
A | Walk |
B | Stand |
X | Sit |
Y | Stairs |
LB + : | |
- D-pad up/down | Walk height |
- D-pad left | Battery-Change Pose |
- D-pad right | Self right |
- Y | Jog |
- A | Amble |
- B | Crawl |
- X | Hop |
If Stand Mode | |
- Left Stick | |
-- X | Rotate body in roll axis |
-- Y | Control height |
- Right Stick | |
-- X | Turn body in yaw axis |
-- Y | Turn body in pitch axis |
Else | |
- Left Stick | Move |
- Right Stick | Turn |
LB + RB + B | E-Stop |
Start | Motor power & Control |
Back | Exit |
User Guide¶
Installation¶
For your best learning experience, please use the Quickstart Guide found in the SDK’s docs/python directory. That will help you get your Python programming environment setup properly.
OS-Specific Dependencies¶
This example has external dependencies to communicate with an XBox controller, and those dependencies are OS-specific.
Ubuntu: On Ubuntu 18.04, the example uses the xboxdrv
driver to communicate with the controller, so please install the driver by executing:
sudo apt-get install xboxdrv
The xboxdrv
driver supports only Xbox360 controllers. Newer controllers are not supported.
Windows: On Windows, the example uses XInput-Python
package, which is automatically installed with the pip command below. The XInput
package officially supports Xbox360 controllers, but newer controllers also work with this example on Windows.
MacOS: This example is not supported on MacOS.
Installation Instructions¶
To install this example on Ubuntu 18.04 and Windows, follow these instructions:
Create virtual environment as described in this Quickstart Guide virtualenv section
Install dependencies:
python3 -m pip install -r requirements.txt
Run the example using instructions in the next section
To exit the virtual environment, run
deactivate
Execution¶
This example follows the common pattern for expected arguments. It needs the common arguments used to configure the SDK and connect to a Spot:
hostname passed as the last argument
username and password should be set in the environment variables
BOSDYN_CLIENT_USERNAME
andBOSDYN_CLIENT_PASSWORD
.
1) The example needs to be run as sudo. To run a python program as sudo within a virtual environment, you need to specify the python executable in the virtualenv folder:
sudo venv/bin/python xbox_controller.py --user USER --password PASSWORD ROBOT_IP
2) After the controller is connected, the example prints a status window:
E-Stop Control Motors On Mode
3) Next, press the key combination Left Button + Right Button + B
to turn E-Stop on:
E-Stop Control Motors On Mode
X
4) Next, press the Guide
button to acquire a lease with this Spot:
E-Stop Control Motors On Mode
X X
5) Next, press the Start
button to turn the motors on:
E-Stop Control Motors On Mode
X X X
6) Spot is now ready to be controlled.
7) To E-Stop Spot at any time, press the E-Stop button combination (LB + RB + B)
8) To exit and power off Spot, press the Back
button.