World Object Mutations¶
These examples demonstrate how to use the world object service to add, change, and delete world objects.
Setup Dependencies¶
These examples need to be run with python3, and have the Spot SDK installed. See the requirements.txt file for a list of dependencies which can be installed with pip.
python3 -m pip install -r requirements.txt
Running the Example¶
To run the example:
python3 mutate_world_objects.py --username USER --password PASSWORD ROBOT_IP