Sdk
Sdk is a repository for settings typically common to a single developer and/or robot fleet.
- exception bosdyn.client.sdk.SdkError[source]
Bases:
ErrorGeneral class of errors to handle non-response non-rpc errors.
- exception bosdyn.client.sdk.UnableToLoadAppTokenError[source]
Bases:
SdkErrorCannot load the provided app token path.
- bosdyn.client.sdk.generate_client_name(prefix='')[source]
Returns a descriptive client name for API clients with an optional prefix.
- bosdyn.client.sdk.create_standard_sdk(client_name_prefix, service_clients=None, cert_resource_glob=None)[source]
Return an Sdk with the most common configuration.
- Parameters:
client_name_prefix – prefix to pass to generate_client_name()
service_clients – List of service client classes to register in addition to the defaults.
cert_resource_glob – Glob expression matching robot certificate(s). Default None to use distributed certificate.
- Raises:
IOError – Robot cert could not be loaded.
- class bosdyn.client.sdk.Sdk(name=None)[source]
Bases:
objectRepository for settings typically common to a single developer and/or robot fleet. See also Robot for robot-specific settings.
- Parameters:
name – Name to identify the client when communicating with the robot.
- create_robot(address, name=None)[source]
Get a Robot initialized with this Sdk, creating it if it does not yet exist.
- Parameters:
address – Network-resolvable address of the robot, e.g. ‘192.168.80.3’
name – A unique identifier for the robot, e.g. ‘My First Robot’. Default None to use the address as the name.
- Returns:
A Robot initialized with the current Sdk settings.
- set_max_message_length(max_message_length)[source]
Updates the send and receive max message length values in all the clients/channels created from this point on.
- Parameters:
max_message_length (int) – Max message length value to use for sending and receiving messages.
- Returns:
None.
- register_service_client(creation_func, service_type=None, service_name=None)[source]
Tell the Sdk how to create a specific type of service client.
- Parameters:
creation_func – Callable that returns a client. Typically just the class.
service_type – Type of the service. If None (default), will try to get the name from creation_func.
service_name – Name of the service. If None (default), will try to get the name from creation_func.
- load_robot_cert(resource_path_glob=None)[source]
Load the SSL certificate for the robot.
- Parameters:
resource_path_glob – Optional path to certificate resource(s). If None, will load the certificate in the ‘resources’ package. Otherwise, should be a glob expression to match certificates. Defaults to None.
- Raises:
IOError – Robot cert could not be loaded.
- bosdyn.client.sdk.decode_token(token)[source]
Decodes a JWT token without verification.
- Parameters:
token – A string representing a token.
- Returns:
Dictionary containing information about the token. Empty dictionary if failed to load token.
- Raises:
UnableToLoadAppTokenError – If the token cannot be read.
Deprecated since version 3.0.1: Decoding tokens is no longer supported in the sdk. Use pyjwt directly instead.
- bosdyn.client.sdk.log_token_time_remaining(token)[source]
Log the time remaining until app token expires.
- Parameters:
token – A jwt token
- Raises:
UnableToLoadAppTokenError – If the token expiration information cannot be retrieved.
Deprecated since version 3.0.1: Decoding tokens is no longer supported in the sdk. Use pyjwt directly instead.