Stream Data Reader
Data reader which reads the file format from a stream, without seeking.
- class bosdyn.bddf.stream_data_reader.StreamDataReader(outfile)[source]
Bases:
BaseDataReaderData reader which reads the file format from a stream, without seeking.
- property read_checksum
64-bit checksum read from the end of the file, or None if not yet read.
- property stream_file_index
Return the file index as parsed from the stream.
- series_descriptor(series_index)[source]
Return SeriesDescriptor for given series index.
Returns KeyError if no such series exists.
- read_data_block()[source]
Read and return next data block.
Returns: DataDescriptor, SeriesDescriptor, data (bytes)
- Raises ParseError if there is a problem with the format of the file,
EOFError if the end of the file is reached.
- read_next_block()[source]
Read and return next block.
Returns: True, DataDescriptor, data (bytes) for data block Returns: False, DescriptorBlock, None for descriptor block
- Raises ParseError if there is a problem with the format of the file,
EOFError if the end of the file is reached.
- property series_block_indexes
series_index -> SeriesBlockIndex.
- Type:
Returns the current list of SeriesBlockIndexes
- series_block_index(series_index)[source]
Returns the SeriesBlockIndexes for the given series_index.
- property eof
Returns True if all blocks in the file have been read.