Hello Orbit

This example program is the introductory programming example for the Orbit client, which uses the Orbit v0 web API via OrbitClient. It demonstrates how to initialize the Orbit client, authenticate with an API token, and finally list the names of the robots connected to Orbit.

For an equivalent walkthrough against the new v1 API (introduced in Orbit v5.2), see the orbit_v1_api example, which uses raw HTTP because OrbitClient targets v0.

Understanding Orbit Web API

Please begin with the Quickstart Guide to get your Python programming environment set up properly. Then, specifically for this example, look at the Orbit API Docs.

Setup Dependencies

See the requirements.txt file for a list of python dependencies which can be installed with pip using the command:

python3 -m pip install -r requirements.txt

Run the Example

To run the example for local development and testing, run the following command with verify set to False. When set to False, requests will skip server’s TLS certificate verifications which will make your application vulnerable. For production software, we recommend you set verify to True or a path to CA bundle.

python3 hello_orbit.py --hostname ORBIT_IP --verify False

The above command prompts you to provide the API token obtained from the Orbit admin settings page. Alternatively, you can set the environment variable BOSDYN_ORBIT_CLIENT_API_TOKEN to the API token obtained from Orbit admin settings page.