GraphNav Point Cloud Extractor¶
This is an example program for opening and parsing a GraphNav map and extracting a globally consistent point cloud from it. This requires the map to have been run through Anchoring Optimization first (see the graph_nav_anchoring_optimization example. Note that if the map was recorded using Autowalk, it will automatically meet the prerequisites). The data is expected to be in XYZ32F format.
Setup Dependencies¶
This example requires Numpy, and requires python 3. Using pip, these dependencies can be installed using:
python3 -m pip install -r requirements.txt
Running the Example¶
Record a map using AutoWalk or the Command Line interface. (If using Autowalk, transfer the map from Documents/bosdyn/autowalk/your_map.walk to your local machine using a USB cable). The map should be a directory of the form:
- /your_map.walk
+ graph
- waypoint_snapshots
- edge_snapshots
Run the point cloud extractor
python3 -m extract_point_cloud --path <path_to_your_map_directory> --output <output PLY file>
Understanding the Point Cloud Extractor¶
This example
Loads a Graph Nav Map from a directory.
Extracts the data from each waypoint.
Transforms the data into the seed frame using the anchoring of each waypoint.
Saves the data to a .PLY file.
To view the data, use a 3D model viewer (such as MeshLab or CloudCompare).
What is actually in the point cloud?¶
For base platform robots, the data in the point cloud will be visual feature data. It will be sparse, and correspond to 3D points with high contrast near the robot. For robots with LIDAR, the data will be a combination of visual feature data and LIDAR data. LIDAR data is downsampled to a 10cm resolution, and some horizontal surfaces (e.g. the floor or ceiling) are intentionally filtered out.
These data are used for localization purposes and shouldn’t be used as, for example, a “digital twin”.