API Example - Visualize Depth in Visual Image
This example demonstrates how to use the depth_in_visual_frame image sources to visualize depth in a visual image.
Setup Dependencies
This example requires the bosdyn API and client to be installed, and must be run using python3. Using pip, these dependencies can be installed using:
python3 -m pip install -r requirements.txt
Running the Example
To run the example:
python3 get_depth_plus_visual_image.py ROBOT_IP
Example output