Using the Robot Data Service¶
The data service tracks data logged to the robot via the API. This includes:
Text messages: Info/Warning/Error/Debug messages, typically logged by API services.
Comments: Short messages, typically added by operators about the robot behavior.
Events: Messages documenting a robot or client event, with a timestamp and possibly a duration.
Message blobs: Arbitrary binary message blobs.
These, and other, messages are stored in data “pages” on the robot. A page is a discrete unit of storage tracked by the data service.
These example programs demonstrate how to query the robot data service for information about the robot’s data pages and their contents.
Setup Dependencies¶
This example requires the bosdyn API and client to be installed, and must be run using python3. Using pip, these dependencies can be installed using:
python3 -m pip install -r requirements.txt
Running the Examples¶
Each example requires that you specify a username and password to authenticate with the robot.
get_comments.py¶
Get operator comments logged via API.
python3 get_comments.py --username USER --password PASSWORD ROBOT_IP
get_events.py¶
Get events logged on the robot.
python3 get_events.py --username USER --password PASSWORD ROBOT_IP
get_index.py¶
Get lists of pages that contain blobs, text-message, events, or operator comments. COMMAND may be one of blob, text, event, or comment.
python3 get_index.py --username USER --password PASSWORD ROBOT_IP COMMAND
get_pages.py¶
Get a list of data pages currently on the robot.
python3 get_pages.py --username USER --password PASSWORD ROBOT_IP
You may optionally specify a time range of pages to return.
For example:
python3 get_pages.py --username USER --password PASSWORD \
--timespan 20201030-20201031 ROBOT_IP
See the description of time range specifications below.
delete_pages.py¶
Delete data pages from the robot. Running this without a time range will delete all data pages on the robot.
python3 delete_pages.py --username USER --password PASSWORD ROBOT_IP
You may optionally specify a time range of pages to delete. For example:
python3 delete_pages.py --username USER --password PASSWORD \
--timespan 20201031_115000-20201031_115950 --robot-time ROBOT_IP
You may specify only one start or only end time if preferred.
Time ranges¶
Times in the command-line arguments are of the format _val_or val-val where val has one of these formats:
yyyymmdd_hhmmss (e.g.,
20200120_120000
)yyyymmdd (e.g.,
20200120
)nd n days ago
nh n hours ago
nm n minutes ago
ns n seconds ago
nnnnnnnnnn[.nn] (e.g.,
1581869515.256
) Seconds since epochnnnnnnnnnnnnnnnnnnnn Nanoseconds since epoch
So:
5m
means from 5 minutes ago until now.20201107-20201108
means all of 2020/11/07.
Adding --robot-time
indicates that the specified time range is in the robot clock, so the specified value should not be converted from client time to robot time.