Grpc Reader
A class for reading GRPC data from a DataFile.
- class bosdyn.bddf.grpc_reader.GrpcReader(data_reader, protobuf_classes)[source]
- Bases: - object- A class for reading GRPC data from a DataFile. - Methods raise ParseError if there is a problem with the format of the file. - property data_reader
- Return underlying DataReader this object is using. 
 - get_proto_reader(proto_name)[source]
- Return the GrpcProtoReader for protobuf messages with the specified type name. 
 - get_message(series_index, index_in_series)[source]
- Return a deserialized protobuf from bytes stored in the file. - Parameters:
- series_index – index (int) from the series_index() call 
- index_in_series – the index of the message within the series 
 
 - Returns: timestamp_nsec (int), deserialized protobuf object