Performing Asynchronous State Queries on Spot¶
This example program demonstrates how to query the robot state service using wait-until-done, block-until-done, and callback-when-done. Please look at the code to see how each asynchronous query is accomplished.
Setup Dependencies¶
This example requires the bosdyn API and client to be installed, and must be run using python3. Using pip, these dependencies can be installed using:
python3 -m pip install -r requirements.txt
Running the Example¶
To run the example:
python3 get_robot_state_async.py --username USER --password PASSWORD ROBOT_IP