Network Compute Bridge Client
For clients to the network compute bridge service.
- exception bosdyn.client.network_compute_bridge_client.ExternalServiceNotFoundError(response, error_message=None)[source]
Bases:
ResponseErrorThe requested service for external computation was not found in the directory.
- exception bosdyn.client.network_compute_bridge_client.ExternalServerError(response, error_message=None)[source]
Bases:
ResponseErrorThe call to the external server did not complete successfully.
- exception bosdyn.client.network_compute_bridge_client.NetworkComputeRotationError(response, error_message=None)[source]
Bases:
ResponseErrorThe robot failed to rotate the image as requested.
- exception bosdyn.client.network_compute_bridge_client.NetworkComputeAnalysisFailedError(response, error_message=None)[source]
Bases:
ResponseErrorThe model failed to analyze the set of input images, but a retry might work.
- class bosdyn.client.network_compute_bridge_client.NetworkComputeBridgeClient[source]
Bases:
BaseClientClient to either the NetworkComputeBridgeService or the NetworkComputeBridgeWorkerService.
- default_service_name = 'network-compute-bridge'
- service_type = 'bosdyn.api.NetworkComputeBridge'
- list_available_models(service_name, **kwargs)[source]
List all available models that the service knows.
- Parameters:
service_name (str) – The service to query for models.
- Returns:
The full ListAvailableModelsResponse, which contains any models the service or worker service advertise.
- Raises:
RpcError – Problem communicating with the robot.
ExternalServiceNotFoundError – The network compute bridge worker service was not found in the robot’s directory.
ExternalServerError – Either the service or worker service threw an error when responding with the set of all models.
- list_available_models_async(service_name, **kwargs)[source]
Async version of list_available_models().
- list_available_models_command(list_request, **kwargs)[source]
List all available models that the service knows.
- Parameters:
list_request (ListAvailableModelsRequest) – The request to list all models.
- Returns:
The full ListAvailableModelsResponse, which contains any models the service or worker service advertise.
- Raises:
RpcError – Problem communicating with the robot.
ExternalServiceNotFoundError – The network compute bridge worker service was not found in the robot’s directory.
ExternalServerError – Either the service or worker service threw an error when responding with the set of all models.
- list_available_models_command_async(list_request, **kwargs)[source]
Async version of list_available_models_command().
- network_compute_bridge_command(network_compute_request, **kwargs)[source]
Issue the main network compute bridge request to run a model on specific, requested data.
- Parameters:
network_compute_request (NetworkComputeRequest) – The request which contains what type of data should be processed, and which model the server should run.
- Returns:
The full NetworkComputeResponse, which contains the processed data.
- Raises:
RpcError – Problem communicating with the robot.
ExternalServiceNotFoundError – The network compute bridge worker service was not found in the robot’s directory.
ExternalServerError – Either the service or worker service threw an error when responding with the set of all models.
NetworkComputeRotationError – For processed image data, the robot was unable to rotate the image as requested.