Adjusting Robot Stance In Place¶
This example will exercise the stance function to reposition the robot’s feet.
Setup Dependencies¶
These examples need to be run with python3, and have the Spot SDK installed. See the requirements.txt file for a list of dependencies which can be installed with pip.
python3 -m pip install -r requirements.txt
Setup Robot¶
To properly setup for this example:
Have the robot in an area with ~1m space all around
Have the robot powered off
Use an external E-Stop endpoint from an api client or tablet
Running the Example¶
When run, this script will
Leave the tablet with cut motor power authority.
Power on and stand up the robot.
Once standing, you will see the robot reposition its feet at the current body location to the foot offsets specified in the script.
python3 stance_in_place.py --username USER --password PASSWORD ROBOT_IP
Use Ctrl-C to exit the script and sit the robot.
Change Offset¶
Pass values to arguments –x-offset and –y-offset to adjust the change in stance.