Streamquality¶
For clients to the Spot CAM StreamQuality service.
- class bosdyn.client.spot_cam.streamquality.StreamQualityClient[source]¶
Bases:
BaseClient
A client calling Spot CAM StreamQuality service.
- default_service_name = 'spot-cam-stream-quality'¶
- service_type = 'bosdyn.api.spot_cam.StreamQualityService'¶
- set_stream_params(target_bitrate=None, refresh_interval=None, idr_interval=None, awb_mode=None, auto_exposure=None, sync_auto_exposure=None, manual_exposure=None, **kwargs)[source]¶
Change image compression and postprocessing.
At most one of auto_exposure, sync_auto_exposure, and manual_exposure can be specified. The others should be set to None if one is specified. Otherwise, they should all be None.
- Parameters
target_bitrate (int) – The compression level in target BPS
refreshinterval (int) – How often the entire feed should be refreshed (in frames)
idrinterval (int) – How often an IDR message should get sent (in frames)
awb_mode (AwbModeEnum) – Options for automatic white balancing mode
auto_exposure (AutoExposure) – Runs exposure independently on each of the ring cameras
sync_auto_exposure (SyncAutoExposure) – Runs a single autoexposure algorithm that takes into account data from all ring cameras
manual_exposure (ManualExposure) – Manual exposure sets an exposure for all ring cameras