Creating an E-Stop endpoint
This example is an E-Stop controller for a Spot robot. The example registers as an E-Stop endpoint with a Spot robot, and it provides an easy-to-use interface for users to trigger the E-Stop in the robot. Please refer to the main SDK documentation for information on how the E-Stop functionality works.
Setup Dependencies
See the requirements.txt file for a list of python dependencies which can be installed with pip using the command:
python3 -m pip install -r requirements.txt
Run the Example
To run the example as a GUI:
python3 estop_gui.py ROBOT_IP
To run the example without a GUI:
python3 estop_nogui.py ROBOT_IP
GUI Version
The GUI version of the example has two buttons. The red STOP button
engages the robot’s E-Stop system, which cuts off power to all the motors. This operation also
changes the E-Stop status to ESTOP_LEVEL_CUT. To release the E-Stop and transition the robot to
an operational state, press the green Release button.
Command-line version without a GUI
Similar to the usage of the GUI version, the non-GUI version of the example uses Space for
engaging the E-Stop system and r for releasing it.
Troubleshooting
The following error may appear when the example as a GUI is run on linux:
qt.qpa.plugin: Could not load the Qt platform plugin "xcb" in "" even though it was found.
This application failed to start because no Qt platform plugin could be initialized. Reinstalling the application may fix this problem.
Available platform plugins are: eglfs, linuxfb, minimal, minimalegl, offscreen, vnc, wayland-egl, wayland, wayland-xcomposite-egl, wayland-xcomposite-glx, webgl, xcb.
Aborted (core dumped)
If so, execute the following command:
sudo apt-get install python3-pyqt6