Constrained Manipulation¶
The examples here demonstrate how to use constrained manipulation through the API. This feature is used to manipulate objects that are constrained by the environment, and move in a low-dimensional space. Examples include ball valves, switches, cabinets and drawers.
Setup Dependencies¶
These examples need to be run with python3, and have the Spot SDK installed.
Constrained Manipulation Example¶
Before running this example, we need to set up the grasp of the object. Once the object is successfully grasped, we can run the constrained manipulation example.
Setup Robot and grasp and object¶
To properly setup for this example:
Use an external E-Stop endpoint from an api client or tablet
Power the robot on
Use the API or the tablet to drive the robot close to the object of interest, for e.g. a ball valve, cabinet, etc.
Grasp the object using the API scripts or the tablet
Run the run_constrained_manipulation.py script to manipulate constrained object.
Running the Example¶
When run, this script will take over the lease and perform manipulation for the task specified in the script for a fixed duration of time.
You can construct your task type of interest by calling one of the functions in constrained_manipulation_helper.py for e.g. construct_crank_task(velocity_normalized) in the run_constrained_manipulation.py script.
You can specify the task type, the velocity along the task and the force or torque limits as arguments. Note that for all tasks besides the knob task type, the velocity is a normalized velocity in the range [-1, 1]. Please look in the file constrained_manipulation_helper.py for more details on how the velocity is scaled with the force limit.
python3 run_constrained_manipulation.py ROBOT_IP --task-type crank --task-velocity 0.5 --force-limit 40