Network

For clients to the Spot CAM Network service.

class bosdyn.client.spot_cam.network.NetworkClient[source]

Bases: BaseClient

A client calling Spot CAM Network services such as ICE Candidates, SSL certs / Keys etc.

Note: Interactive Connectivity Establishment (ICE) is a protocol which lets two devices use an intermediary to exchange offers and answers even if the two devices are separated by Network Address Translation (NAT).

default_service_name = 'spot-cam-network'
service_type = 'bosdyn.api.spot_cam.NetworkService'
get_ice_configuration(**kwargs)[source]

Get ICE configuration from Spot CAM.

get_ice_configuration_async(**kwargs)[source]

Async version of get_ice_configuration()

set_ice_configuration(ice_servers, **kwargs)[source]

Set ICE configuration on Spot CAM.

This overrides all existing configured servers

set_ice_configuration_async(ice_servers, **kwargs)[source]

Async version of set_ice_configuration()