Common
Contains elements common to all service clients.
- bosdyn.client.common.common_header_errors(response)[source]
Return an exception based on common response header.
None if no error.
- bosdyn.client.common.streaming_common_header_errors(response_iterator)[source]
Return an exception based on common response header for a streaming response iterator.
None if no error.
- bosdyn.client.common.common_lease_errors(response)[source]
Return an exception based on lease use result.
None if no error.
- bosdyn.client.common.streaming_common_lease_errors(response_iterator)[source]
Return an exception based on lease use result for a streaming response iterator.
None if no error.
- bosdyn.client.common.custom_params_error(response, status_value=None, status_field_name='status', error_field_name='custom_param_error', total_response=None)[source]
Return an exception based on having a custom parameter status and message.
None if no error.
- bosdyn.client.common.error_pair(error_message)[source]
Creates a pair of an error class and the associated docstring as the error message which can be used by the error_factory.
- Parameters:
error_message – A class that inherits from the python Error class.
- Returns:
The tuple of the error class and it’s associated docstring.
- bosdyn.client.common.error_factory(response, status, status_to_string, status_to_error)[source]
Return an error based on the status field of the given response.
Since most callers of this function are “response to error” callbacks, any exceptions raised by this function are a considered a serious problem. Strongly consider using collections.defaultdict for the status_to_error mapping, and/or wrapping calls to this function in try/except blocks.
- Parameters:
response – Protobuf message to examine or an iterator of protobuf responses.
status – Status from the protobuf message.
status_to_string – Function that converts numeric status value to string. May raise ValueError, in which case just the numeric code is included in a default error message.
status_to_error – mapping of status -> (error_constructor, error_message) error_constructor must take arguments “response” and “error_message”. (and ideally will subclass from ResponseError.)
- Returns:
None if status_to_error[status] maps to (None, _). Otherwise, an instance of an error determined by status_to_error.
- bosdyn.client.common.handle_unset_status_error(unset, field='status', statustype=None)[source]
Decorate “error from response” functions to handle unset status field errors.
- bosdyn.client.common.handle_common_header_errors(func)[source]
Decorate “error from response” functions to handle typical header errors.
- bosdyn.client.common.handle_lease_use_result_errors(func)[source]
Decorate “error from response” functions to handle typical lease errors.
- bosdyn.client.common.handle_custom_params_errors(*args, status_value=None, status_field_name='status', error_field_name='custom_param_error')[source]
Decorate “error from response” functions to handle custom param errors.
- bosdyn.client.common.handle_license_errors(func)[source]
Decorate “error from response” functions to handle typical license errors.
- bosdyn.client.common.handle_license_errors_if_present(func)[source]
Decorate “error from response” functions to handle typical license errors.
Does not raise an error for STATUS_UNKNOWN. Use for responses that may only sometimes fill out the license status.
- bosdyn.client.common.print_response(func)[source]
Decorate “error from response” functions to print for debugging specific messages.
- class bosdyn.client.common.BaseClient(stub_creation_func, name=None)[source]
Bases:
objectHelper base class for all clients to Boston Dynamics services.
- static request_trim_for_log(req)[source]
Deprecated since version 3.3.0: Forces serialization even if the logging is not happening. Do not use.
- static response_trim_for_log(resp)[source]
Deprecated since version 3.3.0: Forces serialization even if the logging is not happening. Do not use.
- property channel
- update_request_iterator(request_iterator, logger, rpc_method, is_blocking, copy_request=True)[source]
- call(rpc_method, request, value_from_response=None, error_from_response=None, assemble_type=None, copy_request=True, **kwargs)[source]
Returns result of calling rpc_method(request, kwargs) after running processors.
value_from_response and error_from_response should not raise their own exceptions! Additionally, value_from_response and error_from_response that are not common handlers must accept streaming responses if it is a grpc streaming response.
- call_async(rpc_method, request, value_from_response=None, error_from_response=None, copy_request=True, **kwargs)[source]
Returns a Future for rpc_method(request, kwargs) after running processors.
value_from_response and error_from_response should not raise their own exceptions!
call_async does not accept streaming rpcs, see ‘call_async_streaming’.
- call_async_streaming(rpc_method, request, value_from_response=None, error_from_response=None, assemble_type=None, copy_request=False, **kwargs)[source]
Returns a Future for rpc_method(request, kwargs) after running processors.
value_from_response and error_from_response should not raise their own exceptions.
A version of ‘call_async’ for streaming rpcs. True async streaming calls are not supported by python grpc. Instead, this call creates a thread that runs the synchronous ‘call’ function.
- chunk_message(data_chunk_byte_size: int)
Take a message, and split it into data chunks.
- Parameters:
data_chunk_byte_size – max size of each streamed message
Deprecated since version 3.3.0: This has been moved to bosdyn.client.data_chunk. Please use bosdyn.client.data_chunk.chunk_message instead.
- class bosdyn.client.common.FutureWrapper(future, value_from_response, error_from_response, is_streaming=False)[source]
Bases:
objectWraps a Future to aid more complicated clients’ async calls.