Manipulating Spot Service Configurations in Directory¶
These examples demonstrate how to use Spot’s Directory Client to list, register, update, and remove information about API services.
Setup Dependencies¶
This example needs to be run with python3. See the requirements.txt file for a list of dependencies which can be installed with pip using:
python3 -m pip install -r requirements.txt
Running the Example¶
To run the example:
python3 directory_modification.py --username USER --password PASSWORD ROBOT_IP