Auto Return Example¶
This example starts AutoReturn functionality manually with a force-acquired lease.
Setup Dependencies¶
These examples need to be run with python3, and have the Spot SDK installed. See the requirements.txt file for a list of dependencies which can be installed with pip.
$ python3 -m pip install -r requirements.txt
Run the Example¶
To run the example:
python3 force_start_auto_return.py ROBOT_IP