Reset Safety Stop Command with the Python SDK
This example provides basic Python scripts to reset the primary and redundant safety stops on a robot configured for Safety-Related Stopping Function (SRSF). Robots equipped with this feature will be listed as Safety-Related Stopping Function (SRSF) “Enabled” under the hardware information section found in the “About” page on the robot’s admin console.
Setup Dependencies
See the requirements.txt file for a list of python dependencies which can be installed with pip using the command:
python3 -m pip install -r requirements.txt
Using the Reset Safety Stop Command
All reset safety stop commands request the robot to reset the safety stop bit on a SRSF configured robot (either primary or redundant). The command requires the client to own the body lease to take effect.
All reset safety stop commands return header information, lease information, and a status. A reset safety stop command should return one of three immediate statuses:
STATUS_OK: Indicates that the robot accepted the reset safety stop command and executed it
STATUS_INCOMPATIBLE_HARDWARE_ERROR: Indicates that at the time the command was received, the robot was not configured for SRSF.
STATUS_FAILED: Indicates that the command was run and executed with an error.
STATUS_UNKNOWN_STOP_TYPE: Indicates that the command failed due to an unknown stop type in the request.
Running The Reset Safety Stop Examples
General Reset Safety Stop Usage
Using the reset safety stop commands in Python begins with the establishment of a Power Client, generally through something like
power_client = robot.ensure_client(PowerClient.default_service_name)
Once this is established, one can use power_client.reset_safety_stop(safety_stop_type=power_pb2.ResetSafetyStopRequest.SAFETY_STOP_REDUNDANT, lease=None) to issue a reset redundant safety stop command or power_client.reset_primary_safety_stop(safety_stop_type=power_pb2.ResetSafetyStopRequest.SAFETY_STOP_PRIMARY, lease=None) to issue a reset primary safety stop command, where the lease can be passed through context such as a LeaseKeepAlive.
Reset Primary Safety Stop Example
To run the Reset primary safety stop example, run:
python3 reset_primary_safety_stop.py ROBOT_IP
Out of the box, this example issues a command that resets the primary safety stop bit on a SRSF configured robot.
Reset Redundant Safety Stop Example
To run the reset redundant safety stop example, run:
python3 reset_redundant_safety_stop.py ROBOT_IP
Out of the box, this example issues a command that resets the redundant safety stop bit on a SRSF configured robot.