Understanding Spot Programming
This guide will help you understand the programming principles that drive Spot and the Spot Python SDK.
Understanding How to Setup and Command Spot to Move _ Create the SDK object _ Create a Robot object _ Retrieve the Robot ID _ Blocking vs. Asynchronous Spot Python SDK functions _ Inspecting robot state _ Services and Authentication _ Retrieving Robot State _ Robot State was a Message, Messages are defined by Protobufs _ Capture and View Camera images _ Configuring “Motor Power Authority” (software E-Stop) _ Create and register an E-Stop Endpoint _ Clear the E-Stop _ Taking ownership of Spot (Leases) _ Powering on the robot _ Establishing timesync _ Commanding the robot * Powering off the robot
Fundamental Robot Services
Understanding the “id” command
The “id” command is one of the simplest Spot commands, so it’s useful to understand how it works, since every command to Spot performs many of the same basic functions.
Specify the verbose flag with --verbose , and you’ll get a lot of information! We’ll explain the pieces…
$ python -m bosdyn.client --verbose 192.168.80.3 id
2020-03-26 17:30:27,571 - DEBUG - Creating standard Sdk, cert glob: "None"
2020-03-26 17:30:27,610 - DEBUG - Created client for robot-id
2020-03-26 17:30:27,615 - DEBUG - Created channel to 192.168.80.3 at port 443 with authority id.spot.robot
...
The first output line creates a Spot SDK object. All Spot API programs start this way.
Note that the output text itself demonstrates Spot’s use of Python’s logging facility, we recommend you perform your logging with the same.
The third line creates a client of Spot’s robot-id service. The Spot API exposes on-robot capabilities via a set of network-accessible services - similar to a microservice architecture.
The final line of output above shows the command initiating a gRPC channel to Spot. All communication to the robot is over a secure HTTPS connection. Spot API uses gRPC as its underlying RPC (Remote Procedure Call) transport. gRPC is a high-performance networking connection for services which supports a wide variety of programming environments. gRPC uses Protocol Buffers as the messaging format, which has a compact over-the-wire representation and supports backwards and forwards compatibility.
2020-03-26 17:30:27,616 - DEBUG - blocking request: b'/bosdyn.api.RobotIdService/GetRobotId'
header {
request_timestamp {
seconds: 1585258227
nanos: 616570624
}
client_name: "BosdynClientbblank02:__main__.py-28906"
}
In the above output, a blocking GetRobotId RPC can be seen being made to the bosdyn.api.RobotIdService.
Finally, the RobotIdService responds to the GetRobotId RPC with a response including information about the robot.
2020-03-26 17:30:27,650 - DEBUG - response: b'/bosdyn.api.RobotIdService/GetRobotId'
header {
request_header {
request_timestamp {
seconds: 1585258227
nanos: 616570624
}
client_name: "BosdynClientbblank02:__main__.py-28906"
}
request_received_timestamp {
seconds: 1585258226
nanos: 224952738
}
response_timestamp {
seconds: 1585258226
nanos: 224990830
}
error {
code: CODE_OK
}
request {
type_url: "type.googleapis.com/bosdyn.api.RobotIdRequest"
value: "\n6\n\014\010\363\275\364\363\005\020\200\276\200\246\002\022&BosdynClientbblank02:__main__.py-28906"
}
}
robot_id {
serial_number: "beta-BD-90490007"
species: "spot"
version: "V3"
software_release {
version {
major_version: 2
}
changeset_date {
seconds: 1583941992
}
changeset: "b11205d698e"
install_date {
seconds: 1583953617
}
}
nickname: "beta29"
computer_serial_number: "02-19904-9903"
}
Listing services
The following command lists all of the services available on the robot. Note the robot-id service is listed, which we just used in the previous section. Services are what you communicate with on Spot, use them to issue commands, retrieve information, etc.
$ python -m bosdyn.client --user user --password password 192.168.80.3 dir list
name type authority tokens
------------------------------------------------------------------------------------------------------------------------------------
auth bosdyn.api.AuthService auth.spot.robot
directory bosdyn.api.DirectoryService api.spot.robot user
directory-registration bosdyn.api.DirectoryRegistrationService api.spot.robot user
estop bosdyn.api.EstopService estop.spot.robot user
graph-nav-service bosdyn.api.graph_nav.GraphNavService graph-nav.spot.robot user
image bosdyn.api.ImageService api.spot.robot user
lease bosdyn.api.LeaseService api.spot.robot user
...
See the Concept documents for more details about Spot’s API Architecture.
How to Setup and Command Spot to Move
It is useful to run Spot from the command line to understand the basics for commanding Spot.
Start up a python interpreter and import the bosdyn.client package - this should work assuming you’ve successfully completed our Spot Python SDK Quickstart.
$ python
Python 3.6.8 (default, Jan 14 2019, 11:02:34)
[GCC 8.0.1 20180414 (experimental) [trunk revision 259383]] on linux
Type "help", "copyright", "credits" or "license" for more information.
>>> import bosdyn.client
Create the SDK object
All Boston Dynamics API programs start by creating an SDK object with a client name argument. The client name is used to help with debugging, and does not have any semantic information - so use whatever string is helpful for you.
>>> sdk = bosdyn.client.create_standard_sdk('understanding-spot')
Create a robot object
To retrieve the robot id like we did in Spot Python SDK Quickstart we’ll first need to create a robot object, using its network address as an argument. In this example, we only create one robot object, but it is possible to create and control multiple robots in the same program with the Boston Dynamics API.
>>> robot = sdk.create_robot('192.168.80.3')
Retrieve the Robot ID
As discussed earlier, Spot exposes its capability via a number of services. The Boston Dynamics Python API has a corresponding set of clients for each service, which are created off of the robot object.
Let’s create a RobotIdClient of the robot-id service, and then retrieve id information:
>>> id_client = robot.ensure_client('robot-id')
>>> id_client.get_id()
serial_number: "beta-BD-90490007"
species: "spot"
...
Blocking vs. Asynchronous Spot Python SDK functions
The get_id() call above is blocking - it will not complete until after the RPC completes. It is possible to tweak parameters for the call, such as a timeout for how long to wait. The following example sets a too short timeout and fails…
>>> id_client.get_id(timeout=0.0001)
Traceback (most recent call last):
File "/mnt/c/spot_v2_0/bblank_spot_v2_0_env/lib/python3.6/site-packages/bosdyn/client/common.py", line 290, in call
response = rpc_method(request, **kwargs)
File "/mnt/c/spot_v2_0/bblank_spot_v2_0_env/lib/python3.6/site-packages/grpc/_channel.py", line 826, in __call__
return _end_unary_response_blocking(state, call, False, None)
File "/mnt/c/spot_v2_0/bblank_spot_v2_0_env/lib/python3.6/site-packages/grpc/_channel.py", line 729, in _end_unary_response_blocking
raise _InactiveRpcError(state)
grpc._channel._InactiveRpcError: <_InactiveRpcError of RPC that terminated with:
status = StatusCode.DEADLINE_EXCEEDED
details = "Deadline Exceeded"
debug_error_string = "{"created":"@1585323526.280242100","description":"Error received from peer ipv4:192.168.80.3:443","file":"src/core/lib/surface/call.cc","file_line":1056,"grpc_message":"Deadline Exceeded","grpc_status":4}"
>
In addition to blocking calls, clients support non-blocking asynchronous calls. This can be useful in high performance applications where a thread of execution can not stall waiting for an RPC to complete. Python’s futures architecture is used as the underpinning of asynchronous communication. See the get_robot_state_async programming example for how to use these functions.
Let’s make an asynchronous call for the robot id and wait for the result from the returned future object:
>>> fut = id_client.get_id_async()
>>> fut.result()
serial_number: "beta-BD-90490007"
species: "spot"
...
Inspecting robot state
The robot-state service contains dynamic information about the robot such as location, battery status, etc.
Services and Authentication
Before robot state can be retrieved, you need to authenticate to the robot. The majority of services require the user to be authenticated - this prevents random network attackers from being able to control the robot or intercept information which might be sensitive.
Assuming that the username is user and the password is password, issue the following command.
>>> robot.authenticate('user', 'password')
If you provided the wrong credentials, an exception will be raised.
Retrieving robot state
Now we can create a RobotStateClient for the robot-state service, and obtain information about Spot:
>>> state_client = robot.ensure_client('robot-state')
>>> state_client.get_robot_state()
power_state {
timestamp {
seconds: 1585324337
nanos: 644209920
}
... a whole lot more
Robot State was a message, messages are defined by protobufs
The structure of the robot state message retrieved above is defined by its protobuf definition. This is the language the robot speaks. Spot SDK completely exposes the protobuf, so to really understand Spot programming you want to look at and understand the protobufs. Take a look, they are right here in your distribution! ../../protos/bosdyn/api/robot_state.proto
Spot’s Frames
Often, it is useful to know about the position of Spot and how it relates to the world around it. To express this information, Spot uses frames to represent objects and locations (e.g. the “body” frame) and 3D transformations to describe the relationship between two frames using a translation vector and a rotation quaternion. See the Geometry and Frames documentation for much more detail on frames and transformations, the math possible with 3D transformations, and the different frame’s Spot knows about.
Capture and View Camera Images
Spot has 5 “fisheye” cameras in addition to 5 depth cameras. Images can be captured from the these image sources. The ‘list_image_sources’ RPC returns valid camera source names.
>>> from bosdyn.client.image import ImageClient
>>> image_client = robot.ensure_client(ImageClient.default_service_name)
>>> sources = image_client.list_image_sources()
>>> [source.name for source in sources]
['back_depth', 'back_depth_in_visual_frame', 'back_fisheye_image', 'frontleft_depth', 'frontleft_depth_in_visual_frame', 'frontleft_fisheye_image', 'frontright_depth', 'frontright_depth_in_visual_frame', 'frontright_fisheye_image', 'left_depth', 'left_depth_in_visual_frame', 'left_fisheye_image', 'right_depth', 'right_depth_in_visual_frame', 'right_fisheye_image']
Using the source names listed above, we can capture an image from one or more image sources. These images can be captured in RAW format or JPG format (with specified quality). Multiple images requested in a single RPC will be hardware time-synced with one another. Let’s retrieve the left_fisheye_image and display it (unless you are on MacOS or WSL)…
>>> image_response = image_client.get_image_from_sources(["left_fisheye_image"])[0]
>>> from PIL import Image
>>> import io
>>> image = Image.open(io.BytesIO(image_response.shot.image.data))
>>> image.show()
Taking ownership of Spot (Leases)
There’s one more step before powering on Spot’s motors, and that’s to acquire ownership of the robot. The robot can have multiple clients but only one can control the robot even as other clients may be requesting data or acting as E-Stop endpoints.
To gain control of the robot, a client needs to acquire a Lease. A valid lease must be presented with every mobility command to the robot. Leases can be returned when the client no longer wants to control the robot.
Like the E-Stop, lease-holders need to periodically check in with Spot to indicate that they are still actively controlling the robot. If it has been too long since a check-in, the robot will commence a Comms Loss Procedure - sitting down if it can, and then powering off.
Let’s make a LeaseClient for the lease service and list the current leases:
>>> lease_client = robot.ensure_client('lease')
>>> lease_client.list_leases()
[resource: "all-leases"
lease {
resource: "all-leases"
epoch: "ZBEwqFkjbTznJRxU"
sequence: 1
client_names: "root"
}
lease_owner {
}
, resource: "body"
lease {
resource: "body"
epoch: "ZBEwqFkjbTznJRxU"
sequence: 1
client_names: "root"
}
lease_owner {
}
, resource: "mobility"
lease {
resource: "mobility"
epoch: "ZBEwqFkjbTznJRxU"
sequence: 1
client_names: "root"
}
lease_owner {
}
]
The lease-able resources are listed: “body”, “mobility”, (”full-arm”, “gripper”, “arm” for robots with an arm). The “body” resource covers all of the motors on Spot and for most use-cases it is sufficient to issue all commands just using the “body” lease since services on Spot will break apart the lease to use the minimal set of resources necessary.
NOTE: the lease_owner field is empty since no one has acquired the body lease.
When taking lease control of Spot, the lease should first be acquired, and then the “keepalive” should be created to retain ownership of the lease resource. Let’s acquire a lease, create the keepalive, and again list:
>>> lease = lease_client.acquire()
>>> lease_keep_alive = bosdyn.client.lease.LeaseKeepAlive(lease_client)
>>> lease_client.list_leases()
[resource: "all-leases"
lease {
resource: "all-leases"
epoch: "ZBEwqFkjbTznJRxU"
sequence: 2
client_names: "root"
}
lease_owner {
client_name: "HelloSpotClientlaptop-kbrandes01:hello_spot.py-32049"
}
, resource: "body"
lease {
resource: "body"
epoch: "ZBEwqFkjbTznJRxU"
sequence: 2
client_names: "root"
}
lease_owner {
client_name: "HelloSpotClientlaptop-kbrandes01:hello_spot.py-32049"
}
, resource: "mobility"
lease {
resource: "mobility"
epoch: "ZBEwqFkjbTznJRxU"
sequence: 2
client_names: "root"
}
lease_owner {
client_name: "HelloSpotClientlaptop-kbrandes01:hello_spot.py-32049"
}
]
After acquiring the “body” lease, you take ownership of the sub-resource “mobility”. For a robot with an arm, you will also take ownership of the sub-resources “full-arm”, “arm”, and “gripper” when acquiring the “body” lease.
NOTE: the lease keepalive object must remain in scope for the entire duration of the program that is using the lease for commands.
Powering on the robot
Now that you’ve authenticated to Spot, created an E-Stop endpoint, and acquired a lease, it’s time to power on the robot.
Make sure that the robot is in a safe spot, in a seated position, with a charged battery, and not connected to shore power.
The power_on helper function first issues a lower level power command to the robot and then waits for power command feedback. This command returns once the robot is powered on or throws an error if the power command fails for any reason. It typically takes several seconds to complete.
>>> robot.power_on(timeout_sec=20)
The robot object provides a method to check the power status of the robot. This just uses the RobotStateService to check the PowerState:
>>> robot.is_powered_on()
True
Establishing timesync
Timesync is required to coordinate clock skew between your device and Spot. From a safety perspective, this allows users to define a period of time for which a command will be valid. The robot class maintains a timesync thread. The wait_for_sync call below will start a timesync thread, and block until sync is established. After timesync is established, this thread will make periodic calls to maintain timesync. Each client is issued a clock identifier which is used to validate that the client has performed timesync, for services that require this functionality. The client library is written such that most implementation details of timesync are taken care of in the background.
>>> robot.time_sync.wait_for_sync()
Commanding the robot
The RobotCommandService is the primary interface for commanding mobility. Mobility and mobility-related commands include stand, sit, selfright, safe_power_off, velocity, and trajectory. For this tutorial, we will just issue stand and safe power off commands.
The API provides a helper function to stand Spot. This command wraps several RobotCommand RPC calls. First a stand command is issued. The robot checks some basic pre-conditions (powered on, not faulted, not E-Stopped) and returns a command id. This command id can then be passed to the robot command feedback RPC. This call returns both high level feedback (”is the robot still processing the command?”) as well as command specific feedback (in the case of stand, “is the robot standing?”).
>>> from bosdyn.client.robot_command import RobotCommandClient, blocking_stand
>>> command_client = robot.ensure_client(RobotCommandClient.default_service_name)
>>> blocking_stand(command_client, timeout_sec=10)
The robot should now be standing. In addition, the stand command can be modified to control the height of the body as well as the orientation of the body with respect to the footprint frame. The footprint frame is a gravity aligned frame with its origin located at the geometric center of the feet. The Z axis up, and the X axis is forward.
The commands proto can be quite expressive, and therefore, if going beyond default parameters, non-trivial. To increase simplicity, Spot API provides several helper functions that combine Spot API RPC commands into single line functions.
We encourage you to experiment with these various parameters, referencing the robot_command proto parent class for general Boston Dynamics robots and the robot command proto Spot subclass.
# Command Spot to rotate about the Z axis.
>>> from bosdyn.geometry import EulerZXY
>>> footprint_R_body = EulerZXY(yaw=0.4, roll=0.0, pitch=0.0)
>>> from bosdyn.client.robot_command import RobotCommandBuilder
>>> cmd = RobotCommandBuilder.synchro_stand_command(footprint_R_body=footprint_R_body)
>>> command_client.robot_command(cmd)
# Command Spot to raise up.
>>> cmd = RobotCommandBuilder.synchro_stand_command(body_height=0.1)
>>> command_client.robot_command(cmd)
Powering off the robot
Power off the robot using the power_off command. Note the preferred method is with cut_immediately=False where Spot will come to a stop and sit down gently before powering off. The other power off option cuts motor power immediately, which causes the robot to collapse.
>>> robot.power_off(cut_immediately=False)