Source code for bosdyn.client.keepalive

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

"""Client implementation of the Keepalive service."""

from __future__ import print_function

import collections
import logging
import threading
import time
from typing import Callable, List, Union

import bosdyn.client.lease
import bosdyn.util
from bosdyn.api import lease_pb2
from bosdyn.api.keepalive import keepalive_pb2, keepalive_service_pb2_grpc
from bosdyn.client.common import (
    BaseClient,
    common_header_errors,
    error_factory,
    error_pair,
    handle_common_header_errors,
    handle_unset_status_error,
)
from bosdyn.client.error_callback_result import ErrorCallbackResult
from bosdyn.client.exceptions import ResponseError, RetryableRpcError
from bosdyn.util import now_sec


[docs]class KeepaliveResponseError(ResponseError): """Error in Keepalive RPC."""
[docs]class InvalidLeaseError(KeepaliveResponseError): """A policy's associated lease was not the same, super, or sub lease of the active lease."""
[docs]class InvalidPolicyError(KeepaliveResponseError): """The specified policy ID was not valid."""
[docs]class Policy(): """Helper class for API Policy.""" def __init__(self, proto: Union[None, 'keepalive_pb2.Policy'] = None): """Constructor.""" self.policy_proto = proto or keepalive_pb2.Policy() @property def name(self) -> str: """Get or set the name of the Policy.""" return self.policy_proto.name @name.setter def name(self, _name: str): self.policy_proto.name = _name
[docs] def add_associated_lease(self, lease: Union['bosdyn.client.lease.Lease', 'lease_pb2.Lease']): if isinstance(lease, bosdyn.client.lease.Lease): self.policy_proto.associated_leases.append(lease.lease_proto) else: self.policy_proto.associated_leases.append(lease)
[docs] def add_controlled_motors_off_action(self, after: float): """Add a 'controlled motors off' action that triggers after specified time (seconds).""" self._configure_action(after, lambda action: action.controlled_motors_off.SetInParent())
[docs] def add_immediate_robot_off_action(self, after: float): """Add an 'immediate robot off' action that triggers after specified time (seconds).""" self._configure_action(after, lambda action: action.immediate_robot_off.SetInParent())
[docs] def add_record_event_action(self, events: List['bosdyn.api.Event'], after: float): """Add a 'record event' action that triggers after specified time (seconds).""" def copy_events(action): for event in events: action.record_event.events.add().CopyFrom(event) self._configure_action(after, copy_events)
[docs] def add_auto_return_action(self, leases: List['bosdyn.client.lease.Lease'], params: 'bosdyn.api.auto_return.Params', after: float): """Add an 'auto return' action that triggers after specified time (seconds).""" def copy_params_and_leases(action): action.auto_return.leases.extend(lease.lease_proto for lease in leases) action.auto_return.params.CopyFrom(params) self._configure_action(after, copy_params_and_leases)
[docs] def add_lease_stale_action(self, leases: List['bosdyn.client.lease.Lease'], after: float): """Add a 'mark lease stale' action that triggers after specified time (seconds).""" def copy_leases(action): action.lease_stale.leases.extend(lease.lease_proto for lease in leases) self._configure_action(after, copy_leases)
[docs] def shortest_action_delay(self) -> Union[None, float]: """Get the shortest delay on an action, or None if no actions are set. For example: pol = Policy() pol.add_controlled_motors_off_action(2.5) pol.add_immediate_robot_off_action(1.2) assert pol.shortest_action_delay() == 1.2 """ delay = None for actionafter in self.policy_proto.actions: tmp = bosdyn.util.duration_to_seconds(actionafter.after) if delay is None or tmp < delay: delay = tmp return delay
def _configure_action(self, after: float, set_action: Callable[['keepalive_pb2.ActionAfter'], None]): """Helper function to reduce boilerplate of adding an action.""" action = self.policy_proto.actions.add() action.after.CopyFrom(bosdyn.util.seconds_to_duration(after)) set_action(action)
[docs]class KeepaliveClient(BaseClient): """A client for the Keepalive service. This client is in BETA and may undergo changes in future releases. """ default_service_name = 'keepalive' service_type = 'bosdyn.api.keepalive.KeepaliveService' def __init__(self): super().__init__(keepalive_service_pb2_grpc.KeepaliveServiceStub) self._timesync_endpoint = None
[docs] def modify_policy(self, to_add: Union['Policy', 'keepalive_pb2.Policy'] = None, policy_ids_to_remove: List[int] = None, **kwargs): """Add given policy and remove policies with given ids.""" request = self._modify_policy_request(to_add, policy_ids_to_remove) return self.call(self._stub.ModifyPolicy, request, None, modify_policy_error, **kwargs)
[docs] def modify_policy_async(self, to_add: Union['Policy', 'keepalive_pb2.Policy'] = None, policy_ids_to_remove: List[int] = None, **kwargs): """Async version of the modify_policy() RPC.""" request = self._modify_policy_request(to_add, policy_ids_to_remove) return self.call_async(self._stub.ModifyPolicy, request, None, modify_policy_error, **kwargs)
[docs] def check_in(self, policy_id: int, **kwargs): """Check in for given policy_id, refreshing that policy's timer.""" request = self._check_in_request(policy_id) return self.call(self._stub.CheckIn, request, None, check_in_error, **kwargs)
[docs] def check_in_async(self, policy_id: int, **kwargs): """Async version of the check_in() RPC.""" request = self._check_in_request(policy_id) return self.call_async(self._stub.CheckIn, request, None, check_in_error, **kwargs)
[docs] def get_status(self, **kwargs): """Get status on all policies.""" request = keepalive_pb2.GetStatusRequest() return self.call(self._stub.GetStatus, request, None, common_header_errors, **kwargs)
[docs] def get_status_async(self, **kwargs): """Async version of the get_status() RPC.""" request = keepalive_pb2.GetStatusRequest() return self.call_async(self._stub.GetStatus, request, None, common_header_errors, **kwargs)
@staticmethod def _modify_policy_request(to_add: Union['Policy', 'keepalive_pb2.Policy'], policy_ids_to_remove): if isinstance(to_add, Policy): request = keepalive_pb2.ModifyPolicyRequest(to_add=to_add.policy_proto, policy_ids_to_remove=policy_ids_to_remove) else: request = keepalive_pb2.ModifyPolicyRequest(to_add=to_add, policy_ids_to_remove=policy_ids_to_remove) return request @staticmethod def _check_in_request(policy_id): request = keepalive_pb2.CheckInRequest(policy_id=policy_id) return request
_MODIFY_POLICY_STATUS_TO_ERROR = collections.defaultdict(lambda: (None, None)) _MODIFY_POLICY_STATUS_TO_ERROR.update({ keepalive_pb2.ModifyPolicyResponse.STATUS_INVALID_LEASE: error_pair(InvalidLeaseError), keepalive_pb2.ModifyPolicyResponse.STATUS_INVALID_POLICY_ID: error_pair(InvalidPolicyError) }) _CHECK_IN_STATUS_TO_ERROR = collections.defaultdict(lambda: (None, None)) _CHECK_IN_STATUS_TO_ERROR.update( {keepalive_pb2.CheckInResponse.STATUS_INVALID_POLICY_ID: error_pair(InvalidPolicyError)})
[docs]@handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def modify_policy_error(response): """ModifyPolicy response to exception.""" return error_factory(response, response.status, status_to_string=keepalive_pb2.ModifyPolicyResponse.Status.Name, status_to_error=_MODIFY_POLICY_STATUS_TO_ERROR)
[docs]@handle_common_header_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def check_in_error(response): """CheckIn response to exception.""" return error_factory(response, response.status, status_to_string=keepalive_pb2.CheckInResponse.Status.Name, status_to_error=_CHECK_IN_STATUS_TO_ERROR)
#pylint: disable=too-many-instance-attributes
[docs]class PolicyKeepalive(): """Specify a keepalive Policy that should be held to. Meant to be used as a context manager. For example: client = robot.ensure_client(KeepaliveClient.default_service_name) pol = Policy() # After 30 seconds of not hearing from this process, turn the robot motors off. pol.add_controlled_motors_off_action(30) with PolicyKeepalive(client, pol, rpc_interval_seconds=3) as policy_keepalive: # A thread will attempt a CheckIn every 3 seconds. run_my_code() """ #pylint: disable=too-many-arguments def __init__(self, client: KeepaliveClient, policy: Policy, rpc_timeout_seconds: float = None, rpc_interval_seconds: float = None, logger: 'logging.Logger' = None, remove_policy_on_exit: bool = False, initial_retry_seconds: float = 1.0): self.logger = logger or logging.getLogger() self.remove_policy_on_exit = remove_policy_on_exit self._client = client self._policy = policy self._policy_id = None # If the interval isn't specified manually, try to get the interval from the policy, # assuming the user wants to check in a few times before the earliest action. # This will raise an exception if there's no action at all. self._rpc_interval_seconds = rpc_interval_seconds or policy.shortest_action_delay() / 3 self._rpc_timeout_seconds = rpc_timeout_seconds self._initial_retry_seconds = initial_retry_seconds #: Callable[[Exception], ErrorCallbackResult] | None: Optional callback to be called when #: an error occurs in the keepalive thread. self.keepalive_error_callback = None self._end_check_in_signal = threading.Event() self._thread = threading.Thread(target=self._periodic_check_in) self._thread.daemon = True def __enter__(self): """Add this instance's policy and begin checking in.""" self._policy_id = self._client.modify_policy(to_add=self._policy).added_policy.policy_id self.start() return self def __exit__(self, exc_type, exc_val, exc_tb): """Stop checking in, and optionally remove the policy.""" self.shutdown() if self.remove_policy_on_exit: self.remove_policy()
[docs] def remove_policy(self): """Remove this instance's policy, if it did manage to add one.""" if self._policy_id: self._client.modify_policy(policy_ids_to_remove=[self._policy_id]) self._policy_id = None
[docs] def start(self): """Start the checkin thread.""" self._thread.start()
[docs] def shutdown(self): """Stop the checkin thread and block until it ends.""" self._end_periodic_check_in() self._thread.join()
def _check_in(self): self._client.check_in(self._policy_id, timeout=self._rpc_timeout_seconds) def _end_periodic_check_in(self): self._end_check_in_signal.set() def _periodic_check_in(self): retry_interval = self._initial_retry_seconds wait_time = self._rpc_interval_seconds # Block and wait for the stop signal. If we receive it within the check-in period, # leave the loop. Under normal conditions, wait up to self._check_in_period seconds, minus # the RPC processing time. (values < 0 are OK and unblock immediately) while not self._end_check_in_signal.wait(wait_time): exec_start = now_sec() action = ErrorCallbackResult.RESUME_NORMAL_OPERATION try: self._check_in() except RetryableRpcError as exc: self.logger.warning('exception during check-in:\n%s\n', exc) self.logger.info('continuing check-in') except Exception as exc: # pylint: disable=broad-except if self.keepalive_error_callback is not None: action = ErrorCallbackResult.DEFAULT_ACTION try: action = self.keepalive_error_callback(exc) except Exception: # pylint: disable=broad-except self.logger.exception( 'Exception thrown in the provided keepalive error callback') else: raise # How long did the RPC and processing of said RPC take? exec_seconds = now_sec() - exec_start if action == ErrorCallbackResult.ABORT: self.logger.warning('Callback directed the keepalive thread to exit.') break elif action == ErrorCallbackResult.RETRY_IMMEDIATELY: wait_time = 0 continue elif action == ErrorCallbackResult.RETRY_WITH_EXPONENTIAL_BACK_OFF: wait_time = retry_interval - exec_seconds retry_interval = min(2 * retry_interval, self._rpc_interval_seconds) else: # Success path, or default action (resume normal operation) wait_time = self._rpc_interval_seconds - exec_seconds retry_interval = self._initial_retry_seconds self.logger.info('Policy check-in stopped')
[docs]def remove_all_policies(keepalive_client, attempts=1): """Remove all policies on the robot. Optionally do this over a few attempts, in case other things are also removing policies. """ last_exc = None for i in range(attempts): if last_exc: time.sleep(0.5) last_exc = None all_policy_ids = [p.policy_id for p in keepalive_client.get_status().status] if all_policy_ids: try: keepalive_client.modify_policy(policy_ids_to_remove=all_policy_ids) except InvalidPolicyError as exc: last_exc = exc else: break else: break if last_exc: raise last_exc