Source code for bosdyn.client.math_helpers

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

import math
import numbers

import numpy
from deprecated.sphinx import deprecated

from bosdyn.api import geometry_pb2


[docs]def recenter_value_mod(value, center, amplitude): new_value = (value - center) % amplitude + center if new_value >= (center + 0.5 * amplitude): new_value -= amplitude elif new_value < (center - 0.5 * amplitude): new_value += amplitude return new_value
[docs]def recenter_angle_mod(theta, center): return recenter_value_mod(theta, center, 2 * math.pi)
[docs]def angle_diff(a1, a2): return recenter_angle_mod(a1 - a2, 0.0)
[docs]def angle_diff_degrees(a1, a2): return recenter_value_mod(a1 - a2, 0.0, 360.0)
[docs]class Vec2(object): """Class representing a two-dimensional vector.""" def __init__(self, x, y): self.x = x self.y = y def __str__(self): return 'X: %0.3f Y: %0.3f' % (self.x, self.y) def __neg__(self): return Vec2(-self.x, -self.y) def __mul__(self, other): if not isinstance(other, numbers.Number): raise TypeError("Can't multiply types %s and %s." % (type(self), type(other))) return Vec2(self.x * other, self.y * other) def __rmul__(self, lhs): return self * lhs def __truediv__(self, other): if not isinstance(other, numbers.Number): raise TypeError("Can't divide types %s and %s." % (type(self), type(other))) return Vec2(self.x / other, self.y / other) # Included for python 2 compatibility def __div__(self, other): return self.__truediv__(other) def __add__(self, other): if not isinstance(other, Vec2): raise TypeError("Can't add types %s and %s." % (type(self), type(other))) return Vec2(self.x + other.x, self.y + other.y) def __sub__(self, other): return self + (-other) def __setitem__(self, idx, data): # pylint: disable=no-else-return if idx == 0: self.x = data return elif idx == 1: self.y = data return raise IndexError("Invalid index {}".format(idx)) def __getitem__(self, idx): # pylint: disable=no-else-return if idx == 0: return self.x elif idx == 1: return self.y raise IndexError("Invalid index {}".format(idx))
[docs] def length(self): return math.sqrt(self.x * self.x + self.y * self.y)
[docs] def to_proto(self): """Converts the math_helpers.Vec2 into an output of the protobuf geometry_pb2.Vec2.""" return geometry_pb2.Vec2(x=self.x, y=self.y)
[docs] def dot(self, other): if not isinstance(other, Vec2): raise TypeError("Can't dot types %s and %s." % (type(self), type(other))) return self.x * other.x + self.y * other.y
[docs] def cross(self, other): if not isinstance(other, Vec2): raise TypeError("Can't cross types %s and %s." % (type(self), type(other))) return self.x * other.y - other.x * self.y
[docs] @staticmethod def from_proto(proto): """Create a math_helpers.Vec2 from a geometry_pb2.Vec2 proto.""" return Vec2(proto.x, proto.y)
[docs]class Vec3(object): """Class representing a three-dimensional vector.""" def __init__(self, x, y, z): self.x = x self.y = y self.z = z def __str__(self): return 'X: %0.3f Y: %0.3f Z: %0.3f' % (self.x, self.y, self.z) def __neg__(self): return Vec3(-self.x, -self.y, -self.z) def __mul__(self, other): if not isinstance(other, numbers.Number): raise TypeError("Can't multiply types %s and %s." % (type(self), type(other))) return Vec3(self.x * other, self.y * other, self.z * other) def __rmul__(self, lhs): return self * lhs def __truediv__(self, other): if not isinstance(other, numbers.Number): raise TypeError("Can't divide types %s and %s." % (type(self), type(other))) return Vec3(self.x / other, self.y / other, self.z / other) # Included for python 2 compatibility def __div__(self, other): return self.__truediv__(other) def __add__(self, other): if not isinstance(other, Vec3): raise TypeError("Can't add types %s and %s." % (type(self), type(other))) return Vec3(self.x + other.x, self.y + other.y, self.z + other.z) def __sub__(self, other): return self + (-other) def __setitem__(self, idx, data): # pylint: disable=no-else-return if idx == 0: self.x = data return elif idx == 1: self.y = data return elif idx == 2: self.z = data return raise IndexError("Invalid index {}".format(idx)) def __getitem__(self, idx): # pylint: disable=no-else-return if idx == 0: return self.x elif idx == 1: return self.y elif idx == 2: return self.z raise IndexError("Invalid index {}".format(idx))
[docs] def length(self): return math.sqrt(self.x * self.x + self.y * self.y + self.z * self.z)
[docs] def to_proto(self): """Converts the math_helpers.Vec3 into an output of the protobuf geometry_pb2.Vec3.""" return geometry_pb2.Vec3(x=self.x, y=self.y, z=self.z)
[docs] def to_numpy(self): """Converts the math_helpers.Vec3 into an output of numpy format.""" return numpy.array([self.x, self.y, self.z])
[docs] def dot(self, other): if not isinstance(other, Vec3): raise TypeError("Can't dot types %s and %s." % (type(self), type(other))) return self.x * other.x + self.y * other.y + self.z * other.z
[docs] def cross(self, other): if not isinstance(other, Vec3): raise TypeError("Can't cross types %s and %s." % (type(self), type(other))) return Vec3(self.y * other.z - self.z * other.y, self.z * other.x - self.x * other.z, self.x * other.y - self.y * other.x)
[docs] @staticmethod def from_proto(proto): """Create a math_helpers.Vec3 from a geometry_pb2.Vec3 proto.""" return Vec3(proto.x, proto.y, proto.z)
[docs] @staticmethod def from_numpy(array): """Create a math_helpers.Vec3 from a numpy array.""" return Vec3(array[0], array[1], array[2])
[docs]class SE2Pose(object): """Class representing an SE2Pose with position and angle.""" def __init__(self, x, y, angle): self.x = x self.y = y self.angle = angle def __str__(self): return 'position -- X: %0.3f Y: %0.3f Yaw: %0.1f deg' % (self.x, self.y, math.degrees(self.angle))
[docs] @staticmethod def flatten(se3pose): """ Flatten a given SE3Pose to an SE2Pose. This will lose height information if the se3pose provided is not gravity aligned. The common gravity aligned frames are odom, vision, and flat_body. Inputs: se3pose (math_helpers.SE3Pose) Returns: math_helpers.SE2Pose representing the flattened se3pose. """ x = se3pose.x y = se3pose.y angle = se3pose.rot.to_yaw() return SE2Pose(x, y, angle)
[docs] def to_obj(self, proto): """Adds the math_helpers.SE2Pose properties into the geometry_pb2.SE2Pose 'proto'.""" proto.position.x = self.x proto.position.y = self.y proto.angle = self.angle
[docs] def to_proto(self): """Converts the math_helpers.SE2Pose into an output of the protobuf geometry_pb2.SE2Pose.""" return geometry_pb2.SE2Pose(position=geometry_pb2.Vec2(x=self.x, y=self.y), angle=self.angle)
[docs] def inverse(self): """ Compute the inverse of the math_helpers.SE2Pose. For example, if the SE(2) pose represented a_tform_b, then the inverse pose is b_tform_a. Returns: math_helpers.SE2Pose representing the inverse of the current SE(2) Pose. """ c = math.cos(self.angle) s = math.sin(self.angle) return SE2Pose(-self.x * c - self.y * s, self.x * s - self.y * c, -self.angle)
[docs] def mult(self, se2pose): """ Computes the multiplication between the current math_helpers.SE2Pose and the input se2pose. For example, if the 'self' SE2Pose represents a_tform_b and the input se2pose represents b_tform_c, then the output will represent the transform a_tform_c. Inputs: se2pose (math_helpers.se2pose) Returns: math_helpers.se2pose representing the multiplication of two SE(2) poses. """ rotation_matrix = self.to_rot_matrix() rotated_pos = rotation_matrix.dot((se2pose.x, se2pose.y)) return SE2Pose(self.x + rotated_pos[0], self.y + rotated_pos[1], recenter_angle_mod(self.angle + se2pose.angle, 0.0))
def __mul__(self, other): """Overrides the '*' symbol to compute the multiplication between two SE(2) poses, or between an SE(2) pose and a Vec2""" if isinstance(other, Vec2): rotation_matrix = self.to_rot_matrix() rotated_pos = rotation_matrix.dot((other.x, other.y)) return Vec2(self.x + rotated_pos[0], self.y + rotated_pos[1]) if isinstance(other, SE2Pose): rotation_matrix = self.to_rot_matrix() rotated_pos = rotation_matrix.dot((other.x, other.y)) return SE2Pose(self.x + rotated_pos[0], self.y + rotated_pos[1], recenter_angle_mod(self.angle + other.angle, 0.0)) else: raise TypeError("Can't multiply types %s and %s." % (type(self), type(other)))
[docs] def to_rot_matrix(self): """Returns the rotation matrix generate from the angle of the current SE(2) Pose.""" c = math.cos(self.angle) s = math.sin(self.angle) return numpy.array([[c, -s], [s, c]])
[docs] def to_matrix(self): """Returns the 3x3 matrix to transform a 2D point (in generalized coordinates).""" c = math.cos(self.angle) s = math.sin(self.angle) return numpy.array([[c, -s, self.x], [s, c, self.y], [0, 0, 1]])
[docs] def to_adjoint_matrix(self): """This creates the adjoint matrix for the current SE2Pose. The adjoint matrix can be used to change reference frames for a SE(2) velocity vector. For example, if you have math_helpers.SE2Velocity velocity_in_frame_b, then the adjoint matrix for the math_helpers.SE2Pose (representing a_tform_b) can be used as follows to transform the velocity: velocity_in_frame_a = a_tform_b.to_adjoint_matrix() * velocity_in_frame_b Returns: a_adjoint_b (Numpy 3x3 matrix) representing the adjoint matrix for the SE2Pose. """ a_R_b = self.to_rot_matrix() position_skew_mat = skew_matrix_2d(self.position) a_adjoint_b = numpy.block([[a_R_b, position_skew_mat.T], [0, 0, 1]]) return a_adjoint_b
@property def position(self): """Property to allow attribute access of the protobuf message field 'position' similar to the geometry_pb2.SE2Pose for the math_helper.SE2Pose.""" return geometry_pb2.Vec2(x=self.x, y=self.y)
[docs] @staticmethod def from_matrix(mat): """Extract SE2Pose from a 3x3 matrix""" # Extract separately to get float type, instead of single-element matrix type. x = mat[0, 2] y = mat[1, 2] angle = math.atan2(mat[1, 0], mat[0, 0]) print(x, y, angle) return SE2Pose(x, y, angle)
[docs] @staticmethod @deprecated(reason='Use from_proto instead.', version='3.1.0') def from_obj(tform): return SE2Pose.from_proto(tform)
[docs] @staticmethod def from_proto(tform): """Create a math_helpers.SE2Pose from a geometry_pb2.SE2Pose proto.""" return SE2Pose(tform.position.x, tform.position.y, tform.angle)
[docs] def get_closest_se3_transform(self, height_z=0.0): """Compute the closest math_helpers.SE3Pose from the current math_helpers.SE2Pose.""" # Note that if the SE(2) pose is a transform from a non-gravity-aligned frame, # then height information will be incorrect in the inflated SE(3) pose unless # the correct height is passed into the function as height_z. return SE3Pose(x=self.x, y=self.y, z=height_z, rot=Quat.from_yaw(self.angle))
[docs]class SE2Velocity(object): """Class representing an SE2Velocity with linear velocity and angular velocity.""" def __init__(self, x, y, angular): self.linear_velocity_x = float(x) self.linear_velocity_y = float(y) self.angular_velocity = float(angular) def __str__(self): return 'Linear velocity -- X: %0.3f Y: %0.3f Angular velocity -- %0.3f ' % ( self.linear_velocity_x, self.linear_velocity_y, self.angular_velocity)
[docs] def to_obj(self, proto): """Adds the math_helpers.SE2Velocity properties into the geometry_pb2.SE2Velocity 'proto'.""" proto.linear.x = self.linear_velocity_x proto.linear.y = self.linear_velocity_y proto.angular = self.angular_velocity
[docs] def to_proto(self): """Converts the math_helpers.SE2Velocity into an output of the protobuf geometry_pb2.SE2Velocity.""" return geometry_pb2.SE2Velocity( linear=geometry_pb2.Vec2(x=self.linear_velocity_x, y=self.linear_velocity_y), angular=self.angular_velocity)
[docs] def to_vector(self): """Creates a 3x1 velocity vector as a numpy array.""" # Create a 3x1 vector of [x_d, y_d, r_d] return numpy.array([self.linear_velocity_x, self.linear_velocity_y, self.angular_velocity]).reshape((3, 1))
[docs] @staticmethod def from_vector(se2_vel_vector): """Converts a 3x1 velocity vector (of either a numpy array or a list) into a math_helpers.SE2Velocity object.""" if isinstance(se2_vel_vector, list): if len(se2_vel_vector) != 3: # Must have 3 elements to be a complete SE2Velocity print("Velocity list must have 3 elements. The input has the wrong dimension of: " + str(len(se2_vel_vector))) return None else: return SE2Velocity(x=se2_vel_vector[0], y=se2_vel_vector[1], angular=se2_vel_vector[2]) if isinstance(se2_vel_vector, numpy.ndarray): if se2_vel_vector.shape[0] != 3: # Must have 3 elements to be a complete SE2Velocity print( "Velocity numpy array must have 3 elements. The input has the wrong dimension of: " + str(se2_vel_vector.shape[0])) return None else: if (isinstance(se2_vel_vector[0], numpy.ndarray)): return SE2Velocity(x=se2_vel_vector[0][0], y=se2_vel_vector[1][0], angular=se2_vel_vector[2][0]) return SE2Velocity(x=se2_vel_vector[0], y=se2_vel_vector[1], angular=se2_vel_vector[2])
@property def linear(self): """Property to allow attribute access of the protobuf message field 'linear' similar to the geometry_pb2.SE2Velocity for the math_helper.SE2Velocity.""" return geometry_pb2.Vec2(x=self.linear_velocity_x, y=self.linear_velocity_y) @property def angular(self): """Property to allow attribute access of the protobuf message field 'angular' similar to the geometry_pb2.SE2Velocity for the math_helper.SE2Velocity.""" return self.angular_velocity
[docs] @staticmethod @deprecated(reason='Use from_proto instead.', version='3.1.0') def from_obj(vel): return SE2Velocity.from_proto(vel)
[docs] @staticmethod def from_proto(vel): """Create a math_helpers.SE2Velocity from a geometry_pb2.SE2Velocity proto.""" return SE2Velocity(x=vel.linear.x, y=vel.linear.y, angular=vel.angular)
[docs]class SE3Velocity(object): """Class representing an SE3Velocity with linear velocity and angular velocity.""" def __init__(self, lin_x, lin_y, lin_z, ang_x, ang_y, ang_z): self.linear_velocity_x = float(lin_x) self.linear_velocity_y = float(lin_y) self.linear_velocity_z = float(lin_z) self.angular_velocity_x = float(ang_x) self.angular_velocity_y = float(ang_y) self.angular_velocity_z = float(ang_z) def __str__(self): return 'Linear velocity -- X: %0.3f Y: %0.3f Z: %0.3f Angular velocity -- X: %0.3f Y: %0.3f Z: %0.3f' % ( self.linear_velocity_x, self.linear_velocity_y, self.linear_velocity_z, self.angular_velocity_x, self.angular_velocity_y, self.angular_velocity_z)
[docs] def to_obj(self, proto): """Adds the math_helpers.SE3Velocity properties into the geometry_pb2.SE3Velocity 'proto'.""" proto.linear.x = self.linear_velocity_x proto.linear.y = self.linear_velocity_y proto.linear.z = self.linear_velocity_z proto.angular.x = self.angular_velocity_x proto.angular.y = self.angular_velocity_y proto.angular.z = self.angular_velocity_z
[docs] def to_proto(self): """Converts the math_helpers.SE3Velocity into an output of the protobuf geometry_pb2.SE3Velocity.""" return geometry_pb2.SE3Velocity( linear=geometry_pb2.Vec3(x=self.linear_velocity_x, y=self.linear_velocity_y, z=self.linear_velocity_z), angular=geometry_pb2.Vec3(x=self.angular_velocity_x, y=self.angular_velocity_y, z=self.angular_velocity_z))
[docs] def to_vector(self): """Creates a 6x1 velocity vector as a numpy array.""" # Create a vector [x_d, y_d, z_d, r_x_d, r_y_d, r_z_d] of dimensions 6x1 return numpy.array([ self.linear_velocity_x, self.linear_velocity_y, self.linear_velocity_z, self.angular_velocity_x, self.angular_velocity_y, self.angular_velocity_z ]).reshape((6, 1))
@property def linear(self): """Property to allow attribute access of the protobuf message field 'linear' similar to the geometry_pb2.SE3Velocity for the math_helper.SE3Velocity.""" return geometry_pb2.Vec3(x=self.linear_velocity_x, y=self.linear_velocity_y, z=self.linear_velocity_z) @property def angular(self): """Property to allow attribute access of the protobuf message field 'angular' similar to the geometry_pb2.SE3Velocity for the math_helper.SE3Velocity.""" return geometry_pb2.Vec3(x=self.angular_velocity_x, y=self.angular_velocity_y, z=self.angular_velocity_z)
[docs] @staticmethod @deprecated(reason='Use from_proto instead.', version='3.1.0') def from_obj(vel): return SE3Velocity.from_proto(vel)
[docs] @staticmethod def from_proto(vel): """Create a math_helpers.SE3Velocity from a geometry_pb2.SE3Velocity proto.""" return SE3Velocity(lin_x=vel.linear.x, lin_y=vel.linear.y, lin_z=vel.linear.z, ang_x=vel.angular.x, ang_y=vel.angular.y, ang_z=vel.angular.z)
[docs] @staticmethod def from_vector(se3_vel_vector): """Converts a 6x1 velocity vector (of either a numpy array or a list) into a math_helpers.SE3Velocity object.""" if isinstance(se3_vel_vector, list): if len(se3_vel_vector) != 6: # Must have 6 elements to be a complete SE3Velocity print("Velocity list must have 6 elements. The input has the wrong dimension of: " + str(len(se3_vel_vector))) return None else: return SE3Velocity(lin_x=se3_vel_vector[0], lin_y=se3_vel_vector[1], lin_z=se3_vel_vector[2], ang_x=se3_vel_vector[3], ang_y=se3_vel_vector[4], ang_z=se3_vel_vector[5]) if isinstance(se3_vel_vector, numpy.ndarray): if se3_vel_vector.shape[0] != 6: # Must have 6 elements to be a complete SE3Velocity print( "Velocity numpy array must have 6 elements. The input has the wrong dimension of: " + str(se3_vel_vector.shape[0])) return None else: if (isinstance(se3_vel_vector[0], numpy.ndarray)): return SE3Velocity(lin_x=se3_vel_vector[0][0], lin_y=se3_vel_vector[1][0], lin_z=se3_vel_vector[2][0], ang_x=se3_vel_vector[3][0], ang_y=se3_vel_vector[4][0], ang_z=se3_vel_vector[5][0]) return SE3Velocity(lin_x=se3_vel_vector[0], lin_y=se3_vel_vector[1], lin_z=se3_vel_vector[2], ang_x=se3_vel_vector[3], ang_y=se3_vel_vector[4], ang_z=se3_vel_vector[5])
[docs]class SE3Pose(object): """Class representing an SE3Pose with position and rotation.""" def __init__(self, x, y, z, rot): self.x = x self.y = y self.z = z # Expect the declaration of math_helpers.SE3Pose to pass a math_helpers.Quat, however we will convert # a protobuf Quaternion into the math_helpers object as well. if isinstance(rot, geometry_pb2.Quaternion): rot = Quat.from_proto(rot) self.rot = rot def __str__(self): return 'position -- X: %0.3f Y: %0.3f Z: %0.3f rotation -- %s' % (self.x, self.y, self.z, str(self.rot)) def __iter__(self): return iter([self.x, self.y, self.z, self.rot.w, self.rot.x, self.rot.y, self.rot.z])
[docs] @staticmethod @deprecated(reason='Use from_proto instead.', version='3.1.0') def from_obj(tform): return SE3Pose.from_proto(tform)
[docs] @staticmethod def from_proto(tform): """Create a math_helpers.SE3Pose from a geometry_pb2.SE3Pose proto.""" if tform.HasField('rotation'): quat = Quat.from_proto(tform.rotation) else: # Create the identity quaternion if no rotation is provided in the SE(3) pose. quat = Quat() return SE3Pose(tform.position.x, tform.position.y, tform.position.z, quat)
[docs] @staticmethod def from_se2(tform, z=0): return SE3Pose(tform.x, tform.y, z, Quat.from_yaw(tform.angle))
[docs] def to_obj(self, proto): """Adds the math_helpers.SE3Pose properties into the geometry_pb2.SE3Pose 'proto'.""" proto.position.x = self.x proto.position.y = self.y proto.position.z = self.z self.rot.to_obj(proto.rotation)
[docs] def to_proto(self): """Converts the math_helpers.SE3Pose into an output of the protobuf geometry_pb2.SE3Pose.""" return geometry_pb2.SE3Pose( position=geometry_pb2.Vec3(x=self.x, y=self.y, z=self.z), rotation=geometry_pb2.Quaternion(w=self.rot.w, x=self.rot.x, y=self.rot.y, z=self.rot.z))
[docs] def inverse(self): """ Compute the inverse of the math_helpers.SE3Pose. For example, if the SE(3) pose represented a_tform_b, then the inverse pose is b_tform_a. Returns: math_helpers.SE3Pose representing the inverse of the current SE(3) Pose. """ inv_rot = self.rot.inverse() (x, y, z) = inv_rot.transform_point(self.x, self.y, self.z) return SE3Pose(-x, -y, -z, inv_rot)
[docs] def transform_point(self, x, y, z): """ Compute the transformation (translation and rotation) of a (x,y,z) vector using the current SE(3) pose. Returns: tuple (size 3) representing the transformed coordinate. """ (out_x, out_y, out_z) = self.rot.transform_point(x, y, z) return (out_x + self.x, out_y + self.y, out_z + self.z)
[docs] def transform_vec3(self, vec3): """ Compute the transformation (translation and rotation) of a (x,y,z) vector using the current SE(3) pose. Returns: Vec3 representing the transformed coordinate. """ (out_x, out_y, out_z) = self.rot.transform_point(vec3.x, vec3.y, vec3.z) return geometry_pb2.Vec3(x=out_x + self.x, y=out_y + self.y, z=out_z + self.z)
[docs] def transform_cloud(self, points): """ Compute the transformation (translation and rotation) of multiple vector/points using the current math_helpers.SE3Pose. Inputs: points (Nx3 numpy matrix) representing a set of (x,y,z) points to be transformed Returns: Nx3 numpy matrix of the points after they are transformed with the current math_helpers.SE3Pose. """ return SE3Pose.transform_cloud_from_matrix(self.to_matrix(), points)
[docs] @staticmethod def transform_cloud_from_matrix(transform, points): """ Compute the transformation (translation and rotation) of multiple vector/points using the input SE(3) pose. Inputs: transform (4x4 numpy matrix) representing the SE3Pose to be used to transform. points (Nx3 numpy matrix) representing a set of (x,y,z) points to be transformed Returns: Nx3 numpy matrix of the points after they are transformed. """ rot = transform[0:3, 0:3] trans = transform[0:3, 3] return (numpy.dot(points, rot.T) + trans)
[docs] def to_matrix(self): """Returns the 4x4 matrix to transform a 3D point (in generalized coordinates).""" ret = numpy.eye(4) ret[0:3, 0:3] = self.rot.to_matrix() ret[0:3, 3] = [self.x, self.y, self.z] return ret
[docs] def mult(self, se3pose): """ Computes the multiplication between the current math_helpers.SE3Pose and the input se3pose. For example, if the 'self' SE3Pose represents a_tform_b and the input se3pose represents b_tform_c, then the output will represent the transform a_tform_c. Inputs: se3pose (math_helpers.SE3Pose) Returns: math_helpers.SE3Pose representing the multiplication of two SE(3) poses. """ (x, y, z) = self.rot.transform_point(se3pose.x, se3pose.y, se3pose.z) return SE3Pose(self.x + x, self.y + y, self.z + z, self.rot.mult(se3pose.rot))
def __mul__(self, other): """Overrides the '*' symbol to compute the multiplication between two SE(3) poses, or between an SE(3) pose and a Vec3.""" if isinstance(other, Vec3): (x, y, z) = self.transform_point(other.x, other.y, other.z) return Vec3(x, y, z) if isinstance(other, SE3Pose): (x, y, z) = self.rot.transform_point(other.x, other.y, other.z) return SE3Pose(self.x + x, self.y + y, self.z + z, self.rot.mult(other.rot)) else: raise TypeError("Can't multiply types %s and %s." % (type(self), type(other))) @property def position(self): """Property to allow attribute access of the protobuf message field 'position' similar to the geometry_pb2.SE3Pose for the math_helper.SE3Pose.""" return geometry_pb2.Vec3(x=self.x, y=self.y, z=self.z) @property def rotation(self): """Property to allow attribute access of the protobuf message field 'rotation' similar to the geometry_pb2.SE3Pose for the math_helper.SE3Pose.""" return self.rot
[docs] @staticmethod def from_matrix(mat): """Extract math_helpers.SE3Pose from a 4x4 matrix.""" x, y, z = mat[0:3, 3] rot = Quat.from_matrix(mat[0:3, 0:3]) return SE3Pose(x, y, z, rot)
[docs] @staticmethod def from_identity(): """Create a math_helpers.SE3Pose representing the identity SE(3) pose.""" return SE3Pose(0, 0, 0, Quat())
[docs] def get_translation(self): """Returns a 3x1 numpy array representing the translation only of the current SE3Pose.""" return numpy.array([self.x, self.y, self.z])
[docs] def to_adjoint_matrix(self): """This creates the adjoint matrix for the current SE3Pose. The adjoint matrix can be used to change reference frames for a SE(3) velocity vector. For example, if you have math_helpers.SE3Velocity velocity_in_frame_b, then the adjoint matrix for the math_helpers.SE3Pose (representing a_tform_b) can be used as follows to transform the velocity: velocity_in_frame_a = a_tform_b.to_adjoint_matrix() * velocity_in_frame_b Returns: a_adjoint_b (Numpy 6x6 matrix) representing the adjoint matrix for the SE3Pose. """ a_R_b = self.rot.to_matrix() position_skew_mat = skew_matrix_3d(self.position) mat = numpy.matmul(position_skew_mat, a_R_b) a_adjoint_b = numpy.block([[a_R_b, mat], [numpy.zeros((3, 3)), a_R_b]]) return a_adjoint_b
[docs] def get_closest_se2_transform(self): """Compute the closest math_helpers.SE2Pose from the current math_helpers.SE3Pose.""" # For a transform a_T_b, the pose_frame_name represents "frame A". This must be a gravity # aligned frame, either "vision", "odom", or "flat_body" to be safely converted from # an SE3Pose to an SE2Pose with minimal loss of height information. return SE2Pose.flatten(self)
[docs] @staticmethod def interp(a, b, fraction): """ Performs a blend of two SE3Poses. Out = a * (1 - fraction) + b * fraction Args: a(SE3Pose): Lower blend input. b(SE3Pose): Upper blend input. fraction(float): The blending factor. Should be inside [0, 1] Returns: SE3Pose """ x = a.x * (1.0 - fraction) + b.x * fraction y = a.y * (1.0 - fraction) + b.y * fraction z = a.z * (1.0 - fraction) + b.z * fraction rot = Quat.slerp(a.rot, b.rot, fraction) return SE3Pose(x, y, z, rot)
[docs]class Quat(object): """Class representing a Quaternion.""" def __init__(self, w=1, x=0, y=0, z=0): self.w = w self.x = x self.y = y self.z = z def __repr__(self): return 'W: %0.4f X: %0.4f Y: %0.4f Z: %0.4f' % (self.w, self.x, self.y, self.z)
[docs] def inverse(self): """Computes the inverse of the current math_helpers.Quat.""" return Quat(self.w, -self.x, -self.y, -self.z)
[docs] def transform_point(self, x, y, z): """Computes the transformation (rotation by the quaternion) of a single (x,y,z) point using the current math_helpers.Quat.""" inv = self.inverse() q = Quat(0, x, y, z) q = q.mult(inv) q = self.mult(q) return (q.x, q.y, q.z)
[docs] def transform_vec3(self, vec3): """Computes the transformation (rotation by the quaternion) of a Vec3 point using the current math_helpers.Quat.""" x, y, z = self.transform_point(vec3.x, vec3.y, vec3.z) return geometry_pb2.Vec3(x=x, y=y, z=z)
[docs] def to_matrix(self): """Creates the 3x3 numpy rotation matrix from the current math_helpers.Quat""" ret = numpy.eye(3) ret[0, 0] = 1.0 - 2.0 * self.y * self.y - 2.0 * self.z * self.z ret[0, 1] = 2.0 * self.x * self.y - 2.0 * self.z * self.w ret[0, 2] = 2.0 * self.x * self.z + 2.0 * self.y * self.w ret[1, 0] = 2.0 * self.x * self.y + 2.0 * self.z * self.w ret[1, 1] = 1.0 - 2.0 * self.x * self.x - 2.0 * self.z * self.z ret[1, 2] = 2.0 * self.y * self.z - 2.0 * self.x * self.w ret[2, 0] = 2.0 * self.x * self.z - 2.0 * self.y * self.w ret[2, 1] = 2.0 * self.y * self.z + 2.0 * self.x * self.w ret[2, 2] = 1.0 - 2.0 * self.x * self.x - 2.0 * self.y * self.y return ret
[docs] @staticmethod def from_matrix(rot): """Creates a math_helpers.Quat from a numpy 3x3 matrix representing rotation.""" wt = 1 + rot[0, 0] + rot[1, 1] + rot[2, 2] # do this most often so we get consistently signed quaternions if wt > 0.1: return Quat._from_matrix_w(rot) xt = 1 + rot[0, 0] - rot[1, 1] - rot[2, 2] yt = 1 - rot[0, 0] + rot[1, 1] - rot[2, 2] zt = 1 - rot[0, 0] - rot[1, 1] + rot[2, 2] # This is a list of (function that divides by the square root of val, val) # The idea is to find the largest of wt, xt, yt, zt and then use the corresponding # function to do the conversion. This will do the best thing numerically. t = [(Quat._from_matrix_w, wt), (Quat._from_matrix_x, xt), (Quat._from_matrix_y, yt), (Quat._from_matrix_z, zt)] from_matrix_coord, val = max(t, key=lambda entry: entry[1]) if val < 1e-6: # This shouldn't actually be theoretically possible. raise ArithmeticError( 'Matrix cannot be converged to quaternion. Are you sure this is a valid' ' rotation matrix?\n' + str(rot)) return from_matrix_coord(rot)
@staticmethod def _from_matrix_w(rot): """Computes the value of the quaternion for the w-axis from a numpy 3x3 rotation matrix.""" w = math.sqrt(1 + rot[0, 0] + rot[1, 1] + rot[2, 2]) * 0.5 return Quat(w=w, x=(rot[2, 1] - rot[1, 2]) / (4.0 * w), y=(rot[0, 2] - rot[2, 0]) / (4.0 * w), z=(rot[1, 0] - rot[0, 1]) / (4.0 * w)) @staticmethod def _from_matrix_x(rot): """Computes the value of the quaternion for the x-axis from a numpy 3x3 rotation matrix.""" x = math.sqrt(1 + rot[0, 0] - rot[1, 1] - rot[2, 2]) * 0.5 return Quat(w=(rot[2, 1] - rot[1, 2]) / (4.0 * x), x=x, y=(rot[0, 1] + rot[1, 0]) / (4.0 * x), z=(rot[0, 2] + rot[2, 0]) / (4.0 * x)) @staticmethod def _from_matrix_y(rot): """Computes the value of the quaternion for the y-axis from a numpy 3x3 rotation matrix.""" y = math.sqrt(1 - rot[0, 0] + rot[1, 1] - rot[2, 2]) * 0.5 return Quat(w=(rot[0, 2] - rot[2, 0]) / (4.0 * y), x=(rot[0, 1] + rot[1, 0]) / (4.0 * y), y=y, z=(rot[1, 2] + rot[2, 1]) / (4.0 * y)) @staticmethod def _from_matrix_z(rot): """Computes the value of the quaternion for the z-axis from a numpy 3x3 rotation matrix.""" z = math.sqrt(1 - rot[0, 0] - rot[1, 1] + rot[2, 2]) * 0.5 return Quat(w=(rot[1, 0] - rot[0, 1]) / (4.0 * z), x=(rot[0, 2] + rot[2, 0]) / (4.0 * z), y=(rot[1, 2] + rot[2, 1]) / (4.0 * z), z=z)
[docs] @staticmethod def from_roll(angle): """Computes a representative math_helpers.Quat from the Euler angle for roll.""" return Quat(w=math.cos(angle / 2.0), x=math.sin(angle / 2.0))
[docs] @staticmethod def from_pitch(angle): """Computes a representative math_helpers.Quat from the Euler angle for pitch.""" return Quat(w=math.cos(angle / 2.0), y=math.sin(angle / 2.0))
[docs] @staticmethod def from_yaw(angle): """Computes a representative math_helpers.Quat from the Euler angle for yaw.""" return Quat(w=math.cos(angle / 2.0), z=math.sin(angle / 2.0))
[docs] def to_roll(self): """Computes the Euler angle roll from the current math_helpers.Quat""" if (self.w * self.w + self.x * self.x + self.y * self.y + self.z * self.z == 0.0): return 0.0 t0 = 2.0 * (self.w * self.x + self.y * self.z) t1 = 1.0 - 2.0 * (self.x * self.x + self.y * self.y) return math.atan2(t0, t1)
[docs] def to_pitch(self): """Computes the Euler angle pitch from the current math_helpers.Quat""" if (self.w * self.w + self.x * self.x + self.y * self.y + self.z * self.z == 0.0): return 0.0 t2 = 2.0 * (self.w * self.y - self.z * self.x) if t2 < -1.0: t2 = -1.0 if t2 > 1.0: t2 = 1.0 return math.asin(t2)
[docs] def to_yaw(self): """Computes the Euler angle yaw from the current math_helpers.Quat""" yaw_only_quat = self.closest_yaw_only_quaternion() return recenter_angle_mod(2 * math.atan2(yaw_only_quat.z, yaw_only_quat.w), 0.0)
[docs] def to_axis_angle(self): """Computes the angle and the respective axis from the math_helpers.Quat""" if (self.w * self.w + self.x * self.x + self.y * self.y + self.z * self.z == 0.0): return (0.0, [0, 0, 1]) mag = 1.0 - (self.w * self.w) if mag <= 1e-12: return (0.0, [0, 0, 1]) denom = math.sqrt(mag) if denom < 1e-12: return (0.0, [0, 0, 1]) angle = 2.0 * math.acos(self.w) axis = [self.x / denom, self.y / denom, self.z / denom] return (angle, axis)
[docs] @staticmethod @deprecated(reason='Use from_proto instead.', version='3.1.0') def from_obj(proto): return Quat.from_proto(proto)
[docs] @staticmethod def from_proto(proto): """Create a math_helpers.Quat from a geometry_pb2.Quaternion proto.""" return Quat(proto.w, proto.x, proto.y, proto.z)
[docs] def to_obj(self, proto): """Adds the math_helpers.Quat properties into the geometry_pb2.Quaternion 'proto'.""" proto.w = self.w proto.x = self.x proto.y = self.y proto.z = self.z
[docs] def to_proto(self): """Converts the math_helpers.Quat into an output of the protobuf geometry_pb2.Quaternion.""" return geometry_pb2.Quaternion(w=self.w, x=self.x, y=self.y, z=self.z)
[docs] def mult(self, other_quat): """Computes the multiplication of two math_helpers.Quats.""" return Quat( self.w * other_quat.w - self.x * other_quat.x - self.y * other_quat.y - self.z * other_quat.z, self.w * other_quat.x + self.x * other_quat.w + self.y * other_quat.z - self.z * other_quat.y, self.w * other_quat.y - self.x * other_quat.z + self.y * other_quat.w + self.z * other_quat.x, self.w * other_quat.z + self.x * other_quat.y - self.y * other_quat.x + self.z * other_quat.w)
def __mul__(self, other): """Overrides the '*' symbol to compute the multiplication between two math_helpers.Quats or between a Quat and a Vec3.""" if isinstance(other, Vec3): (x, y, z) = self.transform_point(other.x, other.y, other.z) return Vec3(x, y, z) if isinstance(other, Quat): return self.mult(other) raise TypeError("Can't multiply types %s and %s." % (type(self), type(other)))
[docs] def normalize(self): """Normalizes the quaternion.""" q = numpy.array([self.w, self.x, self.y, self.z]) len = numpy.sqrt(numpy.dot(q.transpose(), q)) if (len < 1e-15): q = [1.0, 0.0, 0.0, 0.0] else: q /= len self.w = q[0] self.x = q[1] self.y = q[2] self.z = q[3] return self
[docs] def closest_yaw_only_quaternion(self): """Computes a yaw-only math_helpers.Quat from the current roll/pitch/yaw math_helpers.Quat""" mag = math.sqrt(self.w * self.w + self.z * self.z) if mag > 0: return Quat(w=self.w / mag, x=0, y=0, z=self.z / mag) else: # If the problem is ill posed (i.e. z-axis of quaternion is [0, 0, -1]), then preserve old # behavior and always rotate 180 degrees around the y-axis. return Quat(w=0, x=0, y=1, z=0) * self
[docs] @staticmethod def slerp(a, b, fraction): v0 = numpy.array([a.w, a.x, a.y, a.z]) v1 = numpy.array([b.w, b.x, b.y, b.z]) dot = numpy.dot(v0.transpose(), v1) # If the dot product is negative, slerp will not take # the shorter path. Note that v1 and -v1 are equivalent when # the negation is applied to all four components. Fix by # reversing one quaternion. if dot < 0.0: v0 *= -1.0 dot = -dot DOT_THRESHOLD = 1.0 - 1e-4 if dot > DOT_THRESHOLD: # If the inputs are too close for comfort, linearly interpolate # and normalize the result. result = v0 + fraction * (v1 - v0) result /= numpy.sqrt(numpy.dot(result.transpose(), result)) else: # Since dot is in range [0, DOT_THRESHOLD], acos is safe theta_0 = math.acos(dot) # theta_0 = angle between input vectors theta = theta_0 * fraction # theta = angle between v0 and result sin_theta = math.sin(theta) # compute this value only once sin_theta_0 = math.sin(theta_0) # compute this value only once s0 = math.cos( theta) - dot * sin_theta / sin_theta_0 # == sin(theta_0 - theta) / sin(theta_0) s1 = sin_theta / sin_theta_0 result = (s0 * v0) + (s1 * v1) return Quat(result[0], result[1], result[2], result[3])
[docs] @staticmethod def from_two_vectors(u_in: Vec3, v_in: Vec3): """ Returns a quaternion representing the rotation from u to v.""" # Normalizing by max avoids all sorts of underflow and overflow issues when we multiply # terms together, including any issues in calculating the norm itself. max_u = max([math.fabs(u_in[0]), math.fabs(u_in[1]), math.fabs(u_in[2])]) max_v = max([math.fabs(v_in[0]), math.fabs(v_in[1]), math.fabs(v_in[2])]) if max_u == 0 or max_v == 0: # Undefined; return identity return Quat(1, 0, 0, 0) u = u_in * (1 / max_u) v = v_in * (1 / max_v) u_dot_v = u.dot(v) u_dot_u = u.dot(u) v_dot_v = v.dot(v) norm_u_norm_v = math.sqrt(u_dot_u * v_dot_v) if u_dot_v < 0: #When this is the case, things get annoying because the |u||v| + u.v (see u_dot_v >= 0 #case below) has cancellation; this leads us to a different formula that is sensitive to #the magnitude of c. If the vectors are close to antipodal, the cross product itself can #be ill conditioned. Algebraically, u x (u + v) is equal to u x v, but, the result is #much more likely to be orthogonal to u and v for extreme cases. c = u.cross(u + v) max_c = max([math.fabs(c[0]), math.fabs(c[1]), math.fabs(c[2])]) if max_c == 0: # We pick an orthogonal axis, avoiding the smallest one if abs(u[0]) > abs(u[1]): if abs(u[1]) > abs(u[2]): q = Quat(0, -u[1], u[0], 0) return q.normalize() else: q = Quat(0, u[2], 0, -u[0]) return q.normalize() elif abs(u[0]) > abs(u[2]): q = Quat(0, -u[1], u[0], 0) return q.normalize() else: q = Quat(0, 0, -u[2], u[1]) return q.normalize() c_scl = (1 / max_c) * c norm2_c_scl = c_scl.dot(c_scl) tmp = (norm_u_norm_v - u_dot_v) * c_scl q = Quat(norm2_c_scl * max_c, tmp[0], tmp[1], tmp[2]) return q.normalize() else: c = u.cross(v) q = Quat(norm_u_norm_v + u_dot_v, c[0], c[1], c[2]) return q.normalize()
[docs] def conj(self): return Quat(self.w, -self.x, -self.y, -self.z)
[docs]def pose_to_xyz_yaw(A_tform_B): """Gets the x,y,z yaw of B in A from the SE3Pose protobuf message.""" yaw = Quat.from_proto(A_tform_B.rotation).to_yaw() x = A_tform_B.position.x y = A_tform_B.position.y z = A_tform_B.position.z return (x, y, z, yaw)
[docs]def is_within_threshold(pose_3d, max_translation_meters, max_yaw_degrees): """Determines whether the given SE3 pose is small enough in X, Y, and theta.""" delta = SE2Pose.flatten(SE3Pose.from_proto(pose_3d)) dist_2d = math.sqrt(delta.x * delta.x + delta.y * delta.y) angle_deg = math.degrees(abs(delta.angle)) return (dist_2d < max_translation_meters) and (angle_deg < max_yaw_degrees)
[docs]@deprecated(reason='Use recenter_angle_mod or recenter_value_mod instead.', version='3.2.0') def recenter_angle(q, lower_limit, upper_limit): recenter_range = upper_limit - lower_limit while q >= upper_limit: q -= recenter_range while q < lower_limit: q += recenter_range return q
[docs]def skew_matrix_3d(vec3_proto): """Creates a 3x3 numpy matrix representing the skew symmetric matrix for a vec3. These are used to create the adjoint matrices for SE3Pose's, among other things.""" return numpy.array([[0, -vec3_proto.z, vec3_proto.y], [vec3_proto.z, 0, -vec3_proto.x], [-vec3_proto.y, vec3_proto.x, 0]])
[docs]def skew_matrix_2d(vec2_proto): """Creates a 2x1 numpy matrix representing the skew symmetric matrix for a vec2. These are used to create the adjoint matrices for SE2Pose's, among other things.""" return numpy.array([[vec2_proto.y, -vec2_proto.x]])
[docs]def matrix_from_proto(proto): """Converts a geometry_pb2.Matrix or geometry_pb2.Matrixf to a numpy array.""" return numpy.array(proto.values).reshape(proto.rows, proto.cols)
[docs]def transform_se2velocity(a_adjoint_b_matrix, se2_velocity_in_b): """ Changes the frame that the SE(2) Velocity is expressed in. More specifically, it converts the SE(2) Velocity in frame b to a SE(2) Velocity in frame c using the adjoint matrix a_adjoint_b. Inputs: a_adjoint_b_matrix (3x3 numpy matrix) se2_velocity_in_b (geometry_pb2.SE2Velocity OR math_helpers.SE2Velocity) described in frame B. Returns: math_helpers.SE2Velocity described in frame a. None if the input velocity is an unknown type. """ if isinstance(se2_velocity_in_b, geometry_pb2.SE2Velocity): se2_velocity_in_b_vector = (SE2Velocity.from_proto(se2_velocity_in_b)).to_vector() elif isinstance(se2_velocity_in_b, SE2Velocity): se2_velocity_in_b_vector = se2_velocity_in_b.to_vector() else: return None se2_velocity_in_a_vector = numpy.asarray( numpy.matmul(a_adjoint_b_matrix, se2_velocity_in_b_vector)) se2_velocity_in_a = SE2Velocity.from_vector(se2_velocity_in_a_vector) return se2_velocity_in_a
[docs]def transform_se3velocity(a_adjoint_b_matrix, se3_velocity_in_b): """ Changes the frame that the SE(3) Velocity is expressed in. More specifically, it converts the SE(3) Velocity in frame b to a SE(3) Velocity in frame c using the adjoint matrix a_adjoint_b. Inputs: a_adjoint_b_matrix (6x6 numpy matrix) se3_velocity_in_b (geometry_pb2.SE3Velocity OR math_helpers.SE3Velocity) described in frame B. Returns: math_helpers.SE3Velocity described in frame a. None if the input velocity is an unknown type. """ if isinstance(se3_velocity_in_b, geometry_pb2.SE3Velocity): se3_velocity_in_b_vec = (SE3Velocity.from_proto(se3_velocity_in_b)).to_vector() elif isinstance(se3_velocity_in_b, SE3Velocity): se3_velocity_in_b_vec = se3_velocity_in_b.to_vector() else: return None se3_velocity_in_a_vec = numpy.asarray(numpy.matmul(a_adjoint_b_matrix, se3_velocity_in_b_vec)) se3_velocity_in_a = SE3Velocity.from_vector(se3_velocity_in_a_vec) return se3_velocity_in_a
[docs]def quat_to_eulerZYX(q): """Convert a Quat object into Euler yaw, pitch, roll angles (radians).""" pitch = math.asin(-2 * (q.x * q.z - q.w * q.y)) if pitch > 0.9999: yaw = 2 * math.atan2(q.z, q.w) pitch = math.pi / 2 roll = 0 elif pitch < -0.9999: yaw = 2 * math.atan2(q.z, q.w) pitch = -math.pi / 2 roll = 0 else: yaw = math.atan2(2 * (q.x * q.y + q.w * q.z), q.w * q.w + q.x * q.x - q.y * q.y - q.z * q.z) roll = math.atan2(2 * (q.y * q.z + q.w * q.x), q.w * q.w - q.x * q.x - q.y * q.y + q.z * q.z) return yaw, pitch, roll