Source code for bosdyn.client.payload

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

"""Client for the payload service.

This allows client code to read from the robot payload registry.
"""

import logging

import bosdyn.api.payload_pb2 as payload_service_protos
import bosdyn.api.payload_service_pb2_grpc as payload_service

from .common import BaseClient, common_header_errors

LOGGER = logging.getLogger('payload_client')


def _get_entry_value(response):
    return response.payloads


[docs]class PayloadClient(BaseClient): """A client handling payload configs.""" default_service_name = 'payload' service_type = 'bosdyn.api.PayloadService' def __init__(self): super(PayloadClient, self).__init__(payload_service.PayloadServiceStub)
[docs] def list_payloads(self, **kw_args): """List all payloads registered on the robot. Args: kw_args: Extra arguments to pass to grpc call invocation. Returns: A list of the proto message definitions of all registered payloads Raises: RpcError: Problem communicating with the robot. """ request = payload_service_protos.ListPayloadsRequest() return self.call(self._stub.ListPayloads, request, value_from_response=_get_entry_value, error_from_response=common_header_errors, **kw_args)
[docs] def list_payloads_async(self, **kw_args): """List all payloads registered on the robot. Args: kw_args: Extra arguments to pass to grpc call invocation. Returns: A list of the proto message definitions of all registered payloads Raises: RpcError: Problem communicating with the robot. """ request = payload_service_protos.ListPayloadsRequest() return self.call_async(self._stub.ListPayloads, request, value_from_response=_get_entry_value, error_from_response=common_header_errors, **kw_args)