# Copyright (c) 2022 Boston Dynamics, Inc. All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).
"""Client implementation of the RayCast service."""
import collections
from bosdyn.client.common import BaseClient, error_pair, handle_unset_status_error
from bosdyn.client.common import error_factory, handle_common_header_errors
from bosdyn.client.exceptions import ResponseError
from bosdyn.api import geometry_pb2
from bosdyn.api import ray_cast_pb2
from bosdyn.api import ray_cast_service_pb2_grpc
[docs]class RayCastResponseError(ResponseError):
"""General class of errors for ray cast service."""
[docs]class InvalidRequestError(RayCastResponseError):
"""Request was invalid / malformed in some way."""
[docs]class InvalidIntersectionTypeError(RayCastResponseError):
"""Requested source not valid for current robot configuration."""
[docs]class UnknownFrameError(RayCastResponseError):
"""The frame_name for a command was not a known frame."""
# yapf: disable
# pylint: disable=line-too-long
_STATUS_TO_ERROR = collections.defaultdict(lambda: (ResponseError, None))
_STATUS_TO_ERROR.update({
ray_cast_pb2.RaycastResponse.STATUS_OK: (None, None),
ray_cast_pb2.RaycastResponse.STATUS_INVALID_REQUEST: error_pair(InvalidRequestError),
ray_cast_pb2.RaycastResponse.STATUS_INVALID_INTERSECTION_TYPE: error_pair(InvalidIntersectionTypeError),
ray_cast_pb2.RaycastResponse.STATUS_UNKNOWN_FRAME: error_pair(UnknownFrameError),
})
# pylint: enable=line-too-long
# yapf: enable
@handle_common_header_errors
@handle_unset_status_error(unset='STATUS_UNKNOWN')
def _error_from_response(response):
"""Return a custom exception, None if no error."""
return error_factory(response, response.status,
status_to_string=ray_cast_pb2.RaycastResponse.Status.Name,
status_to_error=_STATUS_TO_ERROR)
[docs]class RayCastClient(BaseClient):
"""A client that allows arbitrary rays to be queried against the robot."""
default_authority = 'ray-cast.spot.robot'
default_service_name = 'ray-cast'
service_type = 'bosdyn.api.RayCastService'
def __init__(self):
super(RayCastClient, self).__init__(ray_cast_service_pb2_grpc.RayCastServiceStub)
[docs] def raycast(self, ray_origin, ray_direction, raycast_types, min_distance=0, frame_name=None,
**kwargs):
"""Requests robot to intersect ray against the environment it built up.
Args:
ray_origin: (x, y, z) position of the ray in the specified frame.
ray_direction: (x, y, z) vector denoting the direction of the ray in the specified
frame.
raycast_types: array of 0 or more raycast types. 0 will cast into all sources.
min_distance: a positive real value denoting how far (meters) behind a ray an
intersection can occur.
frame_name: the frame the ray is in.
Returns:
RaycastResponse
"""
req = self._raycast_request(ray_origin, ray_direction, raycast_types, min_distance,
frame_name)
return self.call(self._stub.Raycast, req, None, _error_from_response, **kwargs)
[docs] def raycast_async(self, ray_origin, ray_direction, raycast_types, min_distance=0,
frame_name=None, **kwargs):
"""Async version of raycast()."""
req = self._raycast_request(ray_origin, ray_direction, raycast_types, min_distance,
frame_name)
return self.call_async(self._stub.Raycast, req, None, _error_from_response, **kwargs)
@staticmethod
def _raycast_request(ray_origin, ray_direction, raycast_types, min_distance, frame_name):
origin_proto = geometry_pb2.Vec3(x=ray_origin[0], y=ray_origin[1], z=ray_origin[2])
dir_proto = geometry_pb2.Vec3(x=ray_direction[0], y=ray_direction[1], z=ray_direction[2])
ray = geometry_pb2.Ray(origin=origin_proto, direction=dir_proto)
proto = ray_cast_pb2.RaycastRequest(ray=ray, min_intersection_distance=min_distance,
ray_frame_name=frame_name)
proto.intersection_types.extend(raycast_types)
return proto