# Copyright (c) 2023 Boston Dynamics, Inc. All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).
"""For clients to the robot id service.
RobotIdClient -- Wrapper around service stub.
"""
from deprecated.sphinx import deprecated
from bosdyn.api import robot_id_pb2, robot_id_service_pb2_grpc
from bosdyn.client.common import BaseClient, common_header_errors
def _get_entry_value(response):
return response.robot_id
[docs]class RobotIdClient(BaseClient):
"""Client to access robot info."""
# Typical name of the service in the robot's directory listing.
default_service_name = 'robot-id'
# gRPC service proto definition implemented by this service
service_type = 'bosdyn.api.RobotIdService'
def __init__(self):
super(RobotIdClient, self).__init__(robot_id_service_pb2_grpc.RobotIdServiceStub)
[docs] def get_id(self, **kwargs):
"""Get the robot's robot/id.proto."""
req = robot_id_pb2.RobotIdRequest()
return self.call(self._stub.GetRobotId, req, value_from_response=_get_entry_value,
error_from_response=common_header_errors, copy_request=False, **kwargs)
[docs] def get_id_async(self, **kwargs):
"""Return a future to results of "get_id".
See "get_id" for further docs.
"""
req = robot_id_pb2.RobotIdRequest()
return self.call_async(self._stub.GetRobotId, req, value_from_response=_get_entry_value,
error_from_response=common_header_errors, copy_request=False,
**kwargs)
[docs]def version_tuple(version):
"""Return the version as a tuple for easy comparisons."""
return version.major_version, version.minor_version, version.patch_level
[docs]@deprecated(reason='distutils is deprecated. Use version_tuple() instead.', version='4.0.0')
def create_strict_version(robot_id):
"""Create and return a StrictVersion object, from a robot_id, which can be compared easily."""
if robot_id is None:
return None
version_string = str(robot_id.software_release.version.major_version) + '.' + \
str(robot_id.software_release.version.minor_version) + '.' + \
str(robot_id.software_release.version.patch_level)
from distutils.version import StrictVersion
return StrictVersion(version_string)