Source code for bosdyn.client.token_manager

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

"""For clients to automate token refresh.

TokenManager -- Wrapper around token fresh policy.
"""

import datetime
import logging
import threading

from .auth import InvalidTokenError
from .error_callback_result import ErrorCallbackResult
from .exceptions import ResponseError, RpcError, TimedOutError
from .token_cache import WriteFailedError

_LOGGER = logging.getLogger(__name__)

USER_TOKEN_REFRESH_TIME_DELTA = datetime.timedelta(hours=1)
USER_TOKEN_RETRY_INTERVAL_START = datetime.timedelta(seconds=1)


[docs]class TokenManager: """Refreshes the user token in the robot object. The refresh policy assumes the token is minted and then the manager is launched. """ def __init__(self, robot, timestamp=None, refresh_interval=USER_TOKEN_REFRESH_TIME_DELTA, initial_retry_interval=USER_TOKEN_RETRY_INTERVAL_START): self.robot = robot self._last_timestamp = timestamp or datetime.datetime.now() self._refresh_interval = refresh_interval self._initial_retry_seconds = initial_retry_interval # Daemon threads can still run during shutdown after python has # started to clear out things in globals(). # Fixed in Python3: https://bugs.python.org/issue1856 # Do not use threading.Timer or sleep() because that will slow down # real time services. Use a thread instead. self._exit_thread = threading.Event() self._exit_thread.clear() self.th = threading.Thread(name='token_manager', target=self.update) self.th.daemon = True self.th.start()
[docs] def is_alive(self): return self.th.is_alive()
[docs] def stop(self): self._exit_thread.set()
[docs] def update(self): """Refresh the user token as needed.""" retry_interval = self._initial_retry_seconds wait_time = min(self._refresh_interval - (datetime.datetime.now() - self._last_timestamp), self._refresh_interval) while not self._exit_thread.wait(wait_time.total_seconds()): start_time = datetime.datetime.now() action = ErrorCallbackResult.RESUME_NORMAL_OPERATION try: self.robot.authenticate_with_token(self.robot.user_token) self._last_timestamp = datetime.datetime.now() except WriteFailedError: _LOGGER.exception( "Failed to save the token to the cache. Continuing without caching.") except (InvalidTokenError, ResponseError, RpcError) as exc: _LOGGER.exception("Error refreshing the token.") # Default course of action is to retry with a back-off, unless the application # supplied callback directs us to do otherwise. action = ErrorCallbackResult.RETRY_WITH_EXPONENTIAL_BACK_OFF # If the application provided a callback and the error was encountered while # refreshing the token, invoke the callback so that the application can take # appropriate action. if self.robot.token_refresh_error_callback is not None and not isinstance( exc, TimedOutError): try: action = self.robot.token_refresh_error_callback(exc) except Exception: #pylint: disable=broad-except _LOGGER.exception( "Exception thrown in the provided token refresh error callback") if action == ErrorCallbackResult.RESUME_NORMAL_OPERATION: _LOGGER.warning("Refreshing token in %s", self._refresh_interval) elapsed = datetime.datetime.now() - start_time if action == ErrorCallbackResult.ABORT: _LOGGER.warning( "Application-supplied callback directed the token refresh loop to exit.") break elif action == ErrorCallbackResult.RETRY_IMMEDIATELY: _LOGGER.warning("Retrying to refresh token immediately.") wait_time = datetime.timedelta(seconds=0) elif action == ErrorCallbackResult.RESUME_NORMAL_OPERATION: wait_time = self._refresh_interval - elapsed retry_interval = self._initial_retry_seconds else: # action doesn't match one of the enum values or is one of # RETRY_WITH_EXPONENTIAL_BACK_OFF or DEFAULT_ACTION _LOGGER.warning("Retrying token refresh in %s", retry_interval) wait_time = retry_interval - elapsed retry_interval = min(2 * retry_interval, self._refresh_interval) message = 'Shutting down monitoring of token belonging to robot {}'.format( self.robot.address) _LOGGER.debug(message)