Source code for bosdyn.client.docking

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

"""A client for the docking service."""

import collections
import time

from deprecated.sphinx import deprecated

from bosdyn.api.docking import docking_pb2, docking_service_pb2_grpc
from bosdyn.client import lease
from bosdyn.client.common import (
    BaseClient,
    common_header_errors,
    common_lease_errors,
    error_factory,
    handle_common_header_errors,
    handle_lease_use_result_errors,
    handle_unset_status_error,
    maybe_raise,
)
from bosdyn.client.exceptions import ResponseError
from bosdyn.client.robot_command import CommandFailedError
from bosdyn.util import now_sec, seconds_to_timestamp


[docs]class DockingClient(BaseClient): """A client for the docking service to help issue DockingCommand and get state. Clients are expected to issue a single DockingCommand and then periodically check the status of its execution. This service requires ownership over the robot, in the form of a lease and timesync. """ default_service_name = 'docking' service_type = 'bosdyn.api.docking.DockingService' def __init__(self): super(DockingClient, self).__init__(docking_service_pb2_grpc.DockingServiceStub)
[docs] def update_from(self, other): super(DockingClient, self).update_from(other) if self.lease_wallet: lease.add_lease_wallet_processors(self, self.lease_wallet)
[docs] def docking_command(self, station_id, clock_identifier, end_time, prep_pose_behavior=None, lease=None, **kwargs): """Issue a DockingCommandRequest to the robot. Args: station_id: The ID of the docking station to dock at. clock_identifier: Identifier provided by the time sync service. end_time: Expiry time of the command in robot time. prep_pose_behavior: [optional] How and if to use the pre-dock pose. lease: [optional] Leave empty to have the lease filled in by the LeaseWallet Returns: DockingCommand ID Raises: ResponseError: The command was unable to be completed. See error for details. """ req = self._docking_command_request(lease, station_id, clock_identifier, end_time, prep_pose_behavior) return self.call(self._stub.DockingCommand, req, self._docking_id_from_response, _docking_command_error_from_response, copy_request=False, **kwargs)
[docs] def docking_command_async(self, station_id, clock_identifier, end_time, prep_pose_behavior=None, lease=None, **kwargs): """Async version of docking_command().""" req = self._docking_command_request(lease, station_id, clock_identifier, end_time, prep_pose_behavior) return self.call_async(self._stub.DockingCommand, req, self._docking_id_from_response, _docking_command_error_from_response, copy_request=False, **kwargs)
[docs] def docking_command_full(self, station_id, clock_identifier, end_time, prep_pose_behavior=None, lease=None, require_fiducial=False, **kwargs): """Identical to docking_command(), except will return the full DockingCommandResponse.""" req = self._docking_command_request(lease, station_id, clock_identifier, end_time, prep_pose_behavior, require_fiducial) return self.call(self._stub.DockingCommand, req, error_from_response=_docking_command_error_from_response, copy_request=False, **kwargs)
[docs] def docking_command_full_async(self, station_id, clock_identifier, end_time, prep_pose_behavior=None, lease=None, require_fiducial=False, **kwargs): """Identical to docking_command_async(), except will return the full DockingCommandResponse.""" req = self._docking_command_request(lease, station_id, clock_identifier, end_time, prep_pose_behavior, require_fiducial) return self.call_async(self._stub.DockingCommand, req, error_from_response=_docking_command_error_from_response, copy_request=False, **kwargs)
[docs] def docking_command_feedback_full(self, command_id, end_time=None, **kwargs): """Check the status of a previously issued docking command. Args: command_id: The ID returned from a previous docking_command call. Raises: RpcError: problem communicating with the robot Returns: DockingCommandFeedbackResponse """ req = self._docking_command_feedback_request(command_id, end_time) return self.call(self._stub.DockingCommandFeedback, req, error_from_response=common_header_errors, copy_request=False, **kwargs)
[docs] def docking_command_feedback_full_async(self, command_id, end_time=None, **kwargs): """Async version of docking_command_feedback_full().""" req = self._docking_command_feedback_request(command_id, end_time) return self.call_async(self._stub.DockingCommandFeedback, req, error_from_response=common_header_errors, copy_request=False, **kwargs)
[docs] @deprecated( reason='This function can raise LeaseErrors when the feedback was successfully retrieved. ' 'Use docking_command_feedback_full instead.', version='3.0.0', action='always') def docking_command_feedback(self, command_id, **kwargs): """Check the status of a previously issued docking command. Args: command_id: The ID returned from a previous docking_command call. Returns: Status of type DockingCommandFeedbackResponse.Status """ req = self._docking_command_feedback_request(command_id) return self.call(self._stub.DockingCommandFeedback, req, self._docking_status_from_response, _docking_feedback_error_from_response, copy_request=False, **kwargs)
[docs] @deprecated( reason='This function can raise LeaseErrors when the feedback was successfully retrieved. ' 'Use docking_command_feedback_full_async instead.', version='3.0.0', action='always') def docking_command_feedback_async(self, command_id, **kwargs): """Async version of docking_command_feedback().""" req = self._docking_command_feedback_request(command_id) return self.call_async(self._stub.DockingCommandFeedback, req, self._docking_status_from_response, _docking_feedback_error_from_response, copy_request=False, **kwargs)
[docs] def get_docking_config(self, **kwargs): """Get the docking config stored on the robot. Returns: List of docking configs of type ConfigRange """ req = docking_pb2.GetDockingConfigRequest() return self.call(self._stub.GetDockingConfig, req, self._docking_config_from_response, _docking_get_config_error_from_response, copy_request=False, **kwargs)
[docs] def get_docking_config_async(self, **kwargs): """Async version of get_docking_config().""" req = docking_pb2.GetDockingConfigRequest() return self.call_async(self._stub.GetDockingConfig, req, self._docking_config_from_response, _docking_get_config_error_from_response, copy_request=False, **kwargs)
[docs] def get_docking_state(self, **kwargs): """Get docking state from the robot. Returns: Robot dock state of type DockState """ req = docking_pb2.GetDockingStateRequest() return self.call(self._stub.GetDockingState, req, self._docking_state_from_response, _docking_get_state_error_from_response, copy_request=False, **kwargs)
[docs] def get_docking_state_async(self, **kwargs): """Async version of get_docking_state().""" req = docking_pb2.GetDockingStateRequest() return self.call_async(self._stub.GetDockingState, req, self._docking_state_from_response, _docking_get_state_error_from_response, copy_request=False, **kwargs)
@staticmethod def _docking_command_request(lease, station_id, clock_identifier, end_time, prep_pose_behavior, require_fiducial=False): return docking_pb2.DockingCommandRequest( lease=lease, docking_station_id=station_id, clock_identifier=clock_identifier, end_time=end_time, prep_pose_behavior=prep_pose_behavior, require_fiducial=require_fiducial) @staticmethod def _docking_command_feedback_request(command_id, end_time=None): req = docking_pb2.DockingCommandFeedbackRequest(docking_command_id=command_id) if end_time is not None: req.update_docking_params.end_time.CopyFrom(end_time) return req @staticmethod def _docking_id_from_response(response): return response.docking_command_id @staticmethod def _docking_status_from_response(response): return response.status @staticmethod def _docking_config_from_response(response): return response.dock_configs @staticmethod def _docking_state_from_response(response): return response.dock_state
_DOCKING_COMMAND_STATUS_TO_ERROR = collections.defaultdict(lambda: (ResponseError, None)) _DOCKING_COMMAND_STATUS_TO_ERROR.update( {docking_pb2.DockingCommandResponse.STATUS_OK: (None, None)}) @handle_common_header_errors @handle_lease_use_result_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _docking_command_error_from_response(response): """Return an exception based on response from DockingCommand RPC, None if no error.""" return error_factory(response, response.status, status_to_string=docking_pb2.DockingCommandResponse.Status.Name, status_to_error=_DOCKING_COMMAND_STATUS_TO_ERROR) @handle_common_header_errors @handle_lease_use_result_errors @handle_unset_status_error(unset='STATUS_UNKNOWN') def _docking_feedback_error_from_response(response): """Return an exception based on response from DockingCommandFeedback RPC, None if no error.""" return None @handle_common_header_errors def _docking_get_config_error_from_response(response): """Return an exception based on response from GetDockingConfig RPC, None if no error.""" return None @handle_common_header_errors def _docking_get_state_error_from_response(response): """Return an exception based on response from GetDockingState RPC, None if no error.""" return None
[docs]def blocking_dock_robot(robot, dock_id, num_retries=4, timeout=30): """Blocking helper that takes control of the robot and docks it. Args: robot: The instance of the robot to control. dock_id: The ID of the dock to dock at. num_retries: Optional, number of attempts. Returns: The number of retries required Raises: CommandFailedError: The robot was unable to be docked. See error for details. """ docking_client = robot.ensure_client(DockingClient.default_service_name) attempt_number = 0 docking_success = False # Try to dock the robot while attempt_number < num_retries and not docking_success: attempt_number += 1 converter = robot.time_sync.get_robot_time_converter() start_time = converter.robot_seconds_from_local_seconds(now_sec()) cmd_end_time = start_time + timeout cmd_timeout = cmd_end_time + 10 # client side buffer prep_pose = (docking_pb2.PREP_POSE_USE_POSE if (attempt_number % 2) else docking_pb2.PREP_POSE_SKIP_POSE) cmd_id = docking_client.docking_command(dock_id, robot.time_sync.endpoint.clock_identifier, seconds_to_timestamp(cmd_end_time), prep_pose) while converter.robot_seconds_from_local_seconds(now_sec()) < cmd_timeout: feedback = docking_client.docking_command_feedback_full(cmd_id) maybe_raise(common_lease_errors(feedback)) status = feedback.status if status == docking_pb2.DockingCommandFeedbackResponse.STATUS_IN_PROGRESS: # keep waiting/trying time.sleep(1) elif status == docking_pb2.DockingCommandFeedbackResponse.STATUS_DOCKED: docking_success = True break elif (status in [ docking_pb2.DockingCommandFeedbackResponse.STATUS_MISALIGNED, docking_pb2.DockingCommandFeedbackResponse.STATUS_ERROR_COMMAND_TIMED_OUT, ]): # Retry break else: raise CommandFailedError( "Docking Failed, status: '%s'" % docking_pb2.DockingCommandFeedbackResponse.Status.Name(status)) if docking_success: return attempt_number - 1 # Try and put the robot in a safe position try: blocking_go_to_prep_pose(robot, dock_id) except CommandFailedError: pass # Raise error on original failure to dock raise CommandFailedError("Docking Failed, too many attempts")
[docs]def blocking_go_to_prep_pose(robot, dock_id, timeout=20): """Blocking helper that takes control of the robot and takes it to the prep pose only. Args: robot: The instance of the robot to control. dock_id: The ID of the dock to use. Returns: None Raises: CommandFailedError: The robot was unable to go to the prep pose. See error for details. """ docking_client = robot.ensure_client(DockingClient.default_service_name) converter = robot.time_sync.get_robot_time_converter() start_time = converter.robot_seconds_from_local_seconds(now_sec()) cmd_end_time = start_time + timeout cmd_timeout = cmd_end_time + 10 # client side buffer cmd_id = docking_client.docking_command(dock_id, robot.time_sync.endpoint.clock_identifier, seconds_to_timestamp(cmd_end_time), docking_pb2.PREP_POSE_ONLY_POSE) while converter.robot_seconds_from_local_seconds(now_sec()) < cmd_timeout: feedback = docking_client.docking_command_feedback_full(cmd_id) maybe_raise(common_lease_errors(feedback)) status = feedback.status if status == docking_pb2.DockingCommandFeedbackResponse.STATUS_IN_PROGRESS: # keep waiting/trying time.sleep(1) elif status == docking_pb2.DockingCommandFeedbackResponse.STATUS_AT_PREP_POSE: return else: raise CommandFailedError("Failed to go to the prep pose, status: '%s'" % docking_pb2.DockingCommandFeedbackResponse.Status.Name(status)) raise CommandFailedError("Error going to the prep pose, timeout exceeded.")
[docs]def blocking_undock(robot, timeout=20): """Blocking helper that undocks the robot from the currently docked dock. Args: robot: The instance of the robot to control. Returns: None Raises: CommandFailedError: The robot was unable to undock. See error for details. """ docking_client = robot.ensure_client(DockingClient.default_service_name) converter = robot.time_sync.get_robot_time_converter() start_time = converter.robot_seconds_from_local_seconds(now_sec()) cmd_end_time = start_time + timeout cmd_timeout = cmd_end_time + 10 # client side buffer cmd_id = docking_client.docking_command(0, robot.time_sync.endpoint.clock_identifier, seconds_to_timestamp(cmd_end_time), docking_pb2.PREP_POSE_UNDOCK) while converter.robot_seconds_from_local_seconds(now_sec()) < cmd_timeout: feedback = docking_client.docking_command_feedback_full(cmd_id) maybe_raise(common_lease_errors(feedback)) status = feedback.status if status == docking_pb2.DockingCommandFeedbackResponse.STATUS_IN_PROGRESS: # keep waiting/trying time.sleep(1) elif status == docking_pb2.DockingCommandFeedbackResponse.STATUS_AT_PREP_POSE: return else: raise CommandFailedError("Failed to undock the robot, status: '%s'" % docking_pb2.DockingCommandFeedbackResponse.Status.Name(status)) raise CommandFailedError("Error undocking the robot, timeout exceeded.")
[docs]def get_dock_id(robot): """Blocking helper to get dock ID that robot is currently docked at, None if not docked.""" docking_client = robot.ensure_client(DockingClient.default_service_name) dock_state = docking_client.get_docking_state() if dock_state.status == docking_pb2.DockState.DOCK_STATUS_DOCKED: return dock_state.dock_id return None