Source code for bosdyn.client.gps.ntrip_client

# Copyright (c) 2023 Boston Dynamics, Inc.  All rights reserved.
#
# Downloading, reproducing, distributing or otherwise using the SDK Software
# is subject to the terms and conditions of the Boston Dynamics Software
# Development Kit License (20191101-BDSDK-SL).

import base64
import socket
import ssl
import time
from threading import Thread

SERVER_RECONNECT_DELAY = 60  # seconds of delay before retry after server error
SOCKET_TIMEOUT = 10  # socket timeout in seconds
SOCKET_MAX_RECV_TIMEOUTS = 12  # number of timeouts before reconnecting

DEFAULT_NTRIP_SERVER = ""
DEFAULT_NTRIP_PORT = 2101
DEFAULT_NTRIP_TLS_PORT = 2102


[docs]class NtripClientParams: """ Class for storing parameters for connecting an NTRIP client to an NTRIP server. """ def __init__(self, server=DEFAULT_NTRIP_SERVER, port=DEFAULT_NTRIP_PORT, user="", password="", mountpoint="", tls=False, reconnect_secs=SERVER_RECONNECT_DELAY): """ Constructor. """ self.server = server self.port = port self.user = user self.password = password self.mountpoint = mountpoint self.tls = tls self.reconnect_secs = reconnect_secs
[docs]class NtripClient: """ Client used to connect to an NTRIP server to download GPS corrections. These corrections are then forwarded on to the GPS device using the given stream. """ def __init__(self, device, params: NtripClientParams, logger): """ Constructor. """ self.device = device self.host = params.server self.port = params.port self.user = params.user self.password = params.password self.mountpoint = params.mountpoint self.tls = params.tls self.reconnect_secs = params.reconnect_secs self.thread = None self.streaming = False self.sock = None self.logger = logger
[docs] def make_request(self): """ Make a connection request to an NTRIP server. """ auth_str = base64.b64encode(f"{self.user}:{self.password}".encode()).decode() request = (f"GET /{self.mountpoint} HTTP/1.1\r\n" f"Host: {self.host}:{self.port}\r\n" "User-Agent: NTRIP Python Client\r\n" "Accept: */*\r\n" f"Authorization: Basic {auth_str}\r\n" "Connection: close\r\n" "\r\n") return request.encode()
[docs] def start_stream(self): """ Start streaming data from an NTRIP server to a GPS receiver. """ if self.streaming: self.stop_stream() self.thread = Thread(target=self.stream_data_worker, daemon=True) self.thread.start()
[docs] def stop_stream(self): """ Stop streaming NTRIP data. """ self.streaming = False if self.thread: self.thread.join() self.thread = None
[docs] def is_streaming(self): """ Determine if we are streaming NTRIP data. """ return self.streaming
[docs] def send_gga(self, gga): """ Given a GPGGA message, send it to the NTRIP server. This helps the NTRIP server send corrections that are applicable to the area in which the receiver is operating. """ if self.sock: try: self.sock.send(gga.encode()) except OSError: self.logger.warning("Error sending GGA") return False return True return False
[docs] def create_icy_session(self): """ NTRIP Rev1 uses Shoutcast (ICY). Create an ICY session to stream RTCM data. """ try: # Create a socket connection to the host and port. sock = socket.socket(socket.AF_INET, socket.SOCK_STREAM) if self.tls: self.logger.info("Using secure connection") context = ssl.create_default_context() sock = context.wrap_socket(sock, server_hostname=self.host) sock.settimeout(SOCKET_TIMEOUT) self.logger.info("Connecting to NTRIP Server.") sock.connect((self.host, self.port)) self.logger.info("Connected to NTRIP Server.") # Send the request. self.logger.info("Sending NTRIP Request.") sock.send(self.make_request()) # Read a chunk of data, expecting to get the status line and headers. response = sock.recv(1024) response_lines = response.split(b"\r\n") if len(response_lines) < 2: self.logger.error("Invalid response from server: %s", response) return False status = response_lines[0].decode().split(" ") self.logger.info(response_lines[0].decode()) if status[1] != "200": self.logger.error("HTTP Error: %s, retrying in %d seconds", response_lines[0].decode(), self.reconnect_secs) sock.close() time.sleep(self.reconnect_secs) return False self.logger.info("NTRIP Request Response received.") for line in range(1, len(response_lines)): if response_lines[line] == b"": # Empty line, end of headers. # The rest of the response contains data. response = b"\r\n".join(response_lines[line + 1:]) break self.logger.info(response_lines[line]) if response: self.handle_ntrip_data(response) # Make the socket available for sending GGA. self.sock = sock return True except (socket.herror, socket.gaierror): self.logger.warning("Error connecting to server %s:%d", self.host, self.port) return False except (TimeoutError, socket.timeout): self.logger.warning("Connection timeout") return False
[docs] def stream_data(self): """ Stream NTRIP data from a connected server and send it to a GPS receiver. """ # NTRIP Rev1 uses Shoutcast (ICY), which looks a lot like HTTP but isn't quite the same. # Create an ICY session here to talk to an NTRIP Rev1 caster. ok = self.create_icy_session() if not ok: self.logger.error("Failed to create NTRIP Rev1 ICY session.") return timeouts = 0 has_data = False while self.streaming and timeouts < SOCKET_MAX_RECV_TIMEOUTS: try: response = self.sock.recv(2048) if response: timeouts = 0 self.handle_ntrip_data(response) if not has_data: self.logger.info("Received NTRIP data.") has_data = True else: self.logger.warning("Connection closed by server") break except (socket.herror, socket.gaierror): self.logger.warning("Error connecting to server %s:%d", self.host, self.port) except (TimeoutError, socket.timeout): self.logger.exception("Socket timeout.") timeouts += 1 self.logger.info("NTRIP stream closed. Closing socket.") # Close the socket. try: self.sock.close() except OSError: pass self.sock = None self.logger.info("NTRIP client finished.")
[docs] def stream_data_worker(self): """ NTRIP client worker thread function. """ self.streaming = True while self.streaming: self.stream_data() # stream_data blocks for the lifetime of a connection. If it returns while we are still # expecting to be streaming, it means the server disconnected from us. Wait for a delay # before attempting to reconnect to avoid spamming the server. if self.streaming: self.logger.info( f"Attempting to reconnect to NTRIP server in {self.reconnect_secs} seconds.") time.sleep(self.reconnect_secs)
[docs] def handle_ntrip_data(self, data): """ Callback for handling NTRIP data. """ # Send to receiver as is. self.device.write(data)
[docs] def handle_nmea_gga(self, sentence): """ Process an NMEA-GGA sentence passed in as a string. """ fields = sentence.split(",") if len(fields) < 7: return quality = int(fields[6] or 0) if quality not in (0, 6): # No fix or estimated. if not self.send_gga(sentence + "\r\n"): # Something went wrong, restart the stream. self.start_stream()